MSDSCSI_RequestSenseData_TypeDef Struct ReferenceKit Drivers > Msd
SCSI Request Sense response data typedef.
       Definition at line
       
        143
       
       of file
       
        msdscsi.h
       
       .
      
      
       #include <
       
     
        msdscsi.h
       
       >
      
         Data Fields | 
       |
| struct { | |
| uint8_t ResponseCode : 7 | |
| uint8_t Valid : 1 | |
| }; | |
| struct { | |
| uint8_t Eom : 1 | |
| uint8_t FileMark : 1 | |
| uint8_t Ili : 1 | |
| uint8_t Reserved : 1 | |
| uint8_t SenseKey : 4 | |
| }; | |
| struct { | |
| uint8_t SenseKeySpecific1 : 7 | |
| uint8_t Sksv : 1 | |
| }; | |
| uint8_t | AdditionalLength | 
| uint8_t | Asc | 
| uint8_t | Ascq | 
| uint32_t | CmdSpecificInfo | 
| uint8_t | Fruc | 
| uint32_t | Information | 
| uint8_t | Obsolete | 
| uint8_t | SenseKeySpecific2 | 
| uint8_t | SenseKeySpecific3 | 
Field Documentation
| uint8_t MSDSCSI_RequestSenseData_TypeDef::AdditionalLength | 
Number of additional sense bytes that follow.
        Definition at line
        
         157
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Asc | 
Additional sense code.
        Definition at line
        
         159
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Ascq | 
Additional sense code qualifier.
        Definition at line
        
         160
        
        of file
        
         msdscsi.h
        
        .
       
| uint32_t MSDSCSI_RequestSenseData_TypeDef::CmdSpecificInfo | 
Command specific information field.
        Definition at line
        
         158
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Eom | 
End of medium indicator.
        Definition at line
        
         153
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::FileMark | 
Filemark indicator.
        Definition at line
        
         154
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Fruc | 
Field replacable unit code.
        Definition at line
        
         161
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Ili | 
Incorrect length indicator.
        Definition at line
        
         152
        
        of file
        
         msdscsi.h
        
        .
       
| uint32_t MSDSCSI_RequestSenseData_TypeDef::Information | 
Information field.
        Definition at line
        
         156
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Obsolete | 
Obsolete, expect any value.
        Definition at line
        
         148
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Reserved | 
Reserved, expect 0.
        Definition at line
        
         151
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::ResponseCode | 
Response code, 0x70 = Current errors.
        Definition at line
        
         145
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKey | 
Generic error information.
        Definition at line
        
         150
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKeySpecific1 | 
Sense key specific field.
        Definition at line
        
         163
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKeySpecific2 | 
Sense key specific field.
        Definition at line
        
         166
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::SenseKeySpecific3 | 
Sense key specific field.
        Definition at line
        
         167
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Sksv | 
Sense key specific field qualifier.
        Definition at line
        
         164
        
        of file
        
         msdscsi.h
        
        .
       
| uint8_t MSDSCSI_RequestSenseData_TypeDef::Valid | 
Valid, qualifier for Information field.
        Definition at line
        
         146
        
        of file
        
         msdscsi.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/hardware/kit/common/drivers/
       
msdscsi.h