ACMP_TypeDef Struct ReferenceDevices > ACMP
ACMP Register Declaration
       Definition at line
       
        49
       
       of file
       
        efm32jg1b_acmp.h
       
       .
      
      
       #include <
       
     
        efm32jg1b_acmp.h
       
       >
      
         Data Fields | 
       |
| __IM uint32_t | APORTCONFLICT | 
| __IM uint32_t | APORTREQ | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | HYSTERESIS0 | 
| __IOM uint32_t | HYSTERESIS1 | 
| __IOM uint32_t | IEN | 
| __IM uint32_t | IF | 
| __IOM uint32_t | IFC | 
| __IOM uint32_t | IFS | 
| __IOM uint32_t | INPUTSEL | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [4] | 
| __IOM uint32_t | ROUTELOC0 | 
| __IOM uint32_t | ROUTEPEN | 
| __IM uint32_t | STATUS | 
Field Documentation
| __IM uint32_t ACMP_TypeDef::APORTCONFLICT | 
APORT Conflict Status Register
        Definition at line
        
         59
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
| __IM uint32_t ACMP_TypeDef::APORTREQ | 
APORT Request Status Register
        Definition at line
        
         58
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
| __IOM uint32_t ACMP_TypeDef::CTRL | 
Control Register
        Definition at line
        
         50
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() , ACMP_Disable() , ACMP_Enable() , ACMP_GPIOSetup() , ACMP_Init() , and ACMP_Reset() .
| __IOM uint32_t ACMP_TypeDef::HYSTERESIS0 | 
Hysteresis 0 Register
        Definition at line
        
         60
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() , ACMP_Reset() , ACMP_VASetup() , and ACMP_VBSetup() .
| __IOM uint32_t ACMP_TypeDef::HYSTERESIS1 | 
Hysteresis 1 Register
        Definition at line
        
         61
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_CapsenseInit() , ACMP_Reset() , ACMP_VASetup() , and ACMP_VBSetup() .
| __IOM uint32_t ACMP_TypeDef::IEN | 
Interrupt Enable Register
        Definition at line
        
         56
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_IntDisable() , ACMP_IntEnable() , ACMP_IntGetEnabled() , and ACMP_Reset() .
| __IM uint32_t ACMP_TypeDef::IF | 
Interrupt Flag Register
        Definition at line
        
         53
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_IntGet() , and ACMP_IntGetEnabled() .
| __IOM uint32_t ACMP_TypeDef::IFC | 
Interrupt Flag Clear Register
        Definition at line
        
         55
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_IntClear() , and ACMP_Reset() .
| __IOM uint32_t ACMP_TypeDef::IFS | 
Interrupt Flag Set Register
        Definition at line
        
         54
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_IntSet() .
| __IOM uint32_t ACMP_TypeDef::INPUTSEL | 
Input Selection Register
        Definition at line
        
         51
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_CapsenseChannelSet() , ACMP_CapsenseInit() , ACMP_ChannelSet() , ACMP_Init() , ACMP_Reset() , ACMP_VASetup() , and ACMP_VBSetup() .
| uint32_t ACMP_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         57
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
| uint32_t ACMP_TypeDef::RESERVED1[4] | 
Reserved for future use
        Definition at line
        
         63
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
| __IOM uint32_t ACMP_TypeDef::ROUTELOC0 | 
I/O Routing Location Register
        Definition at line
        
         65
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_GPIOSetup() .
| __IOM uint32_t ACMP_TypeDef::ROUTEPEN | 
I/O Routing Pine Enable Register
        Definition at line
        
         64
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
Referenced by ACMP_GPIOSetup() .
| __IM uint32_t ACMP_TypeDef::STATUS | 
Status Register
        Definition at line
        
         52
        
        of file
        
         efm32jg1b_acmp.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG1B/Include/
       
efm32jg1b_acmp.h