spidrv.c File Reference
SPIDRV API implementation.
- Version
 - 5.5.0
 
License
(C) Copyright 2015 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
       Definition in file
       
        spidrv.c
       
       .
      
       #include <string.h>
      
      
       #include "
       
        em_device.h
       
       "
      
      
       #include "
       
        em_gpio.h
       
       "
      
      
       #include "
       
        em_core.h
       
       "
      
      
       #include "
       
        em_usart.h
       
       "
      
      
       #include "
       
        dmadrv.h
       
       "
      
      
       #include "
       
        spidrv.h
       
       "
      
      
         Functions | 
       |
| Ecode_t | SPIDRV_AbortTransfer ( SPIDRV_Handle_t handle) | 
| 
         Abort an ongoing SPI transfer.
          | 
       |
| Ecode_t | SPIDRV_DeInit ( SPIDRV_Handle_t handle) | 
| 
         Deinitialize an SPI driver instance.
          | 
       |
| Ecode_t | SPIDRV_GetBitrate ( SPIDRV_Handle_t handle, uint32_t *bitRate) | 
| 
         Get current SPI bus bitrate.
          | 
       |
| Ecode_t | SPIDRV_GetFramelength ( SPIDRV_Handle_t handle, uint32_t *frameLength) | 
| 
         Get current SPI framelength.
          | 
       |
| Ecode_t | SPIDRV_GetTransferStatus ( SPIDRV_Handle_t handle, int *itemsTransferred, int *itemsRemaining) | 
| 
         Get the status of an SPI transfer.
          | 
       |
| Ecode_t | SPIDRV_Init ( SPIDRV_Handle_t handle, SPIDRV_Init_t *initData) | 
| 
         Initialize an SPI driver instance.
          | 
       |
| Ecode_t | SPIDRV_MReceive ( SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback) | 
| 
         Start an SPI master receive transfer.
          | 
       |
| Ecode_t | SPIDRV_MReceiveB ( SPIDRV_Handle_t handle, void *buffer, int count) | 
| 
         Start an SPI master blocking receive transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransfer ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count, SPIDRV_Callback_t callback) | 
| 
         Start an SPI master transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransferB ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count) | 
| 
         Start an SPI master blocking transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransferSingleItemB ( SPIDRV_Handle_t handle, uint32_t txValue, void *rxValue) | 
| 
         Start an SPI master blocking single item (frame) transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransmit ( SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback) | 
| 
         Start an SPI master transmit transfer.
          | 
       |
| Ecode_t | SPIDRV_MTransmitB ( SPIDRV_Handle_t handle, const void *buffer, int count) | 
| 
         Start an SPI master blocking transmit transfer.
          | 
       |
| Ecode_t | SPIDRV_SetBitrate ( SPIDRV_Handle_t handle, uint32_t bitRate) | 
| 
         Set SPI bus bitrate.
          | 
       |
| Ecode_t | SPIDRV_SetFramelength ( SPIDRV_Handle_t handle, uint32_t frameLength) | 
| 
         Set SPI framelength.
          | 
       |
| Ecode_t | SPIDRV_SReceive ( SPIDRV_Handle_t handle, void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs) | 
| 
         Start an SPI slave receive transfer.
          | 
       |
| Ecode_t | SPIDRV_SReceiveB ( SPIDRV_Handle_t handle, void *buffer, int count, int timeoutMs) | 
| 
         Start an SPI slave blocking receive transfer.
          | 
       |
| Ecode_t | SPIDRV_STransfer ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count, SPIDRV_Callback_t callback, int timeoutMs) | 
| 
         Start an SPI slave transfer.
          | 
       |
| Ecode_t | SPIDRV_STransferB ( SPIDRV_Handle_t handle, const void *txBuffer, void * rxBuffer , int count, int timeoutMs) | 
| 
         Start an SPI slave blocking transfer.
          | 
       |
| Ecode_t | SPIDRV_STransmit ( SPIDRV_Handle_t handle, const void *buffer, int count, SPIDRV_Callback_t callback, int timeoutMs) | 
| 
         Start an SPI slave transmit transfer.
          | 
       |
| Ecode_t | SPIDRV_STransmitB ( SPIDRV_Handle_t handle, const void *buffer, int count, int timeoutMs) | 
| 
         Start an SPI slave blocking transmit transfer.
          | 
       |