bsp_tdk.c File Reference
Board support package for Touch Display Kit.
License
Copyright 2018 Silicon Labs, http://www.silabs.com
This file is licensensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
bsp_tdk.c
.
#include <stdint.h>
#include <stdbool.h>
#include "
bsp_tdk.h
"
#include "bspconfig.h"
#include "
em_device.h
"
#include "
em_cmu.h
"
#include "
em_gpio.h
"
#include "
em_ebi.h
"
Functions |
|
| void * | BSP_getTftSRAMDirectDriveBaseAddress (void) |
|
Get the TFT SRAM base address.
|
|
| void | BSP_initEbiFlash (void) |
|
Initialize the flash.
|
|
| void | BSP_initEbiSram (void) |
|
Initialize the SRAM.
|
|
| void | BSP_initEbiTftDirectDrive (void) |
|
Initialize the TFT display.
|
|
| void | BSP_setTftSRAMDirectDriveBaseAddress (void *baseAddressIn) |
|
Set the TFT SRAM base address. The TFT address is updated according to the EBI_TFTCTRL_FBCTRIG bit. Default is every VSYNC.
|
|
| static void | initEbiCommon (void) |
|
Initialize common EBI settings (GPIO, power and pin routing)
|
|
| static void | initGpio (void) |
|
Initialize GPIO according to bsp_config.h.
|
|
Variables |
|
| static bool | BSP_ebiInitialized = false |
| static bool | BSP_flashInitialized = false |
| static bool | BSP_sramInitialized = false |
| static bool | BSP_tftInitialized = false |
Function Documentation
| void* BSP_getTftSRAMDirectDriveBaseAddress | ( | void |
|
) |
Get the TFT SRAM base address.
- Returns
- Pointer to current TFT base address
Definition at line
141
of file
bsp_tdk.c
.
References EBI , and EBI_BankAddress() .
| void BSP_setTftSRAMDirectDriveBaseAddress | ( | void * |
baseAddressIn
|
) |
Set the TFT SRAM base address. The TFT address is updated according to the EBI_TFTCTRL_FBCTRIG bit. Default is every VSYNC.
- Parameters
-
baseAddressInStart address for the TFT display. This has to be in the memory space corresponding to BSP_CONFIG_SRAM_EBI_BANK.
Definition at line
163
of file
bsp_tdk.c
.
References EBI , and EBI_BankAddress() .