rtcdriver.c File Reference
RTCDRV timer API implementation.
- Version
- 5.6.0
License
(C) Copyright 2018 Silicon Labs, www.silabs.com
This file is licensed under the Silabs License Agreement. See the file "Silabs_License_Agreement.txt" for details. Before using this software for any purpose, you must agree to the terms of that agreement.
Definition in file
rtcdriver.c
.
#include <string.h>
#include "
em_device.h
"
#include "
em_cmu.h
"
#include "
em_common.h
"
#include "
em_core.h
"
#include "
em_rtcc.h
"
#include "
rtcdriver.h
"
Functions |
|
Ecode_t | RTCDRV_AllocateTimer ( RTCDRV_TimerID_t *id) |
Allocate timer.
|
|
Ecode_t | RTCDRV_DeInit (void) |
Deinitialize the RTCDRV driver.
|
|
Ecode_t | RTCDRV_Delay (uint32_t ms) |
Millisecond delay function.
|
|
Ecode_t | RTCDRV_FreeTimer ( RTCDRV_TimerID_t id) |
Free timer.
|
|
uint32_t | RTCDRV_GetWallClock (void) |
Get wallclock time.
|
|
uint32_t | RTCDRV_GetWallClockTicks32 (void) |
Get wallclock tick count as a 32bit value. At 4 ticks per millisecond, overflow occurs after approximately 12.5 days.
|
|
uint64_t | RTCDRV_GetWallClockTicks64 (void) |
Get a wallclock tick count as a 64 bit value.
|
|
Ecode_t | RTCDRV_Init (void) |
Initialize the RTCDRV driver.
|
|
Ecode_t | RTCDRV_IsRunning ( RTCDRV_TimerID_t id, bool *isRunning) |
Check if a given timer is running.
|
|
uint64_t | RTCDRV_MsecsToTicks (uint32_t ms) |
Convert from milliseconds to RTC/RTCC ticks.
|
|
uint64_t | RTCDRV_SecsToTicks (uint32_t secs) |
Convert from seconds to RTC/RTCC ticks.
|
|
Ecode_t | RTCDRV_SetWallClock (uint32_t secs) |
Set wallclock time.
|
|
Ecode_t | RTCDRV_StartTimer ( RTCDRV_TimerID_t id, RTCDRV_TimerType_t type, uint32_t timeout, RTCDRV_Callback_t callback, void *user) |
Start a timer.
|
|
Ecode_t | RTCDRV_StopTimer ( RTCDRV_TimerID_t id) |
Stop a given timer.
|
|
uint32_t | RTCDRV_TicksToMsec (uint64_t ticks) |
Convert from RTC/RTCC ticks to milliseconds.
|
|
uint64_t | RTCDRV_TicksToMsec64 (uint64_t ticks) |
Convert from RTC/RTCC ticks to milliseconds with 64-bit resolution.
|
|
uint32_t | RTCDRV_TicksToSec (uint64_t ticks) |
Convert from RTC/RTCC ticks to seconds.
|
|
Ecode_t | RTCDRV_TimeRemaining ( RTCDRV_TimerID_t id, uint32_t *timeRemaining) |
Get time left before a given timer expires.
|
|