RMU_TypeDef Struct ReferenceDevices > RMU

RMU Register Declaration

Definition at line 49 of file efm32jg1b_rmu.h .

#include < efm32jg1b_rmu.h >

Data Fields

__IOM uint32_t CMD
__IOM uint32_t CTRL
__IOM uint32_t LOCK
__IOM uint32_t RST
__IM uint32_t RSTCAUSE

Field Documentation

__IOM uint32_t RMU_TypeDef::CMD

Command Register

Definition at line 52 of file efm32jg1b_rmu.h .

__IOM uint32_t RMU_TypeDef::CTRL

Control Register

Definition at line 50 of file efm32jg1b_rmu.h .

__IOM uint32_t RMU_TypeDef::LOCK

Configuration Lock Register

Definition at line 54 of file efm32jg1b_rmu.h .

__IOM uint32_t RMU_TypeDef::RST

Reset Control Register

Definition at line 53 of file efm32jg1b_rmu.h .

__IM uint32_t RMU_TypeDef::RSTCAUSE

Reset Cause Register

Definition at line 51 of file efm32jg1b_rmu.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32JG1B/Include/ efm32jg1b_rmu.h