MSDD_CmdStatus_TypeDef Struct ReferenceKit Drivers > Msd
Status info for one BOT CBW -> Data I/O -> CSW cycle.
       Definition at line
       
        37
       
       of file
       
        msdd.h
       
       .
      
      
       #include <
       
     
        msdd.h
       
       >
      
| Public Types | |
| enum | { XFER_MEMORYMAPPED = 0, XFER_INDIRECT } | 
| Data Fields | |
| uint8_t | direction | 
| uint32_t | lba | 
| uint32_t | maxBurst | 
| uint8_t * | pData | 
| bool | valid | 
| uint32_t | xferLen | 
| enum MSDD_CmdStatus_TypeDef:: { ... } | xferType | 
Field Documentation
| uint8_t MSDD_CmdStatus_TypeDef::direction | 
Set if BOT direction is IN.
        Definition at line
        
         39
        
        of file
        
         msdd.h
        
        .
       
| uint32_t MSDD_CmdStatus_TypeDef::lba | 
SCSI Read/Write lba address.
        Definition at line
        
         41
        
        of file
        
         msdd.h
        
        .
       
| uint32_t MSDD_CmdStatus_TypeDef::maxBurst | 
Max length of one transfer.
        Definition at line
        
         43
        
        of file
        
         msdd.h
        
        .
       
| uint8_t* MSDD_CmdStatus_TypeDef::pData | 
Media data pointer.
        Definition at line
        
         40
        
        of file
        
         msdd.h
        
        .
       
| bool MSDD_CmdStatus_TypeDef::valid | 
True if the CBW is valid.
        Definition at line
        
         38
        
        of file
        
         msdd.h
        
        .
       
| uint32_t MSDD_CmdStatus_TypeDef::xferLen | 
BOT transfer length.
        Definition at line
        
         42
        
        of file
        
         msdd.h
        
        .
       
| enum { ... } MSDD_CmdStatus_TypeDef::xferType | 
MSD media access type.
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/hardware/kit/common/drivers/
       msdd.h