ACMP_VAConfig_TypeDef Struct ReferenceEMLIB > ACMP
VA Configuration structure. This structure is used to configure the VA voltage input source and its dividers.
Definition at line
911
of file
em_acmp.h
.
#include <
em_acmp.h
>
Data Fields |
|
uint32_t | div0 |
uint32_t | div1 |
ACMP_VAInput_TypeDef | input |
Field Documentation
uint32_t ACMP_VAConfig_TypeDef::div0 |
A divider for VA voltage input source when ACMP output is 0. This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.
VA divided = VA input * (div0 + 1) / 64
Definition at line
921
of file
em_acmp.h
.
Referenced by ACMP_VASetup() .
uint32_t ACMP_VAConfig_TypeDef::div1 |
A divider for VA voltage input source when ACMP output is 1. This value is used to divide the VA voltage input source by a specific value. The valid range is between 0 and 63.
VA divided = VA input * (div1 + 1) / 64
Definition at line
930
of file
em_acmp.h
.
Referenced by ACMP_VASetup() .
ACMP_VAInput_TypeDef ACMP_VAConfig_TypeDef::input |
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_acmp.h