SegmentLcdKit Drivers

Macros

#define SEGMENT_LCD_BLOCK_MODE_BLANK   0
 
#define SEGMENT_LCD_BLOCK_MODE_FILL   1
 
#define SEGMENT_LCD_BLOCK_MODE_OUTLINE   2
 
#define SEGMENT_LCD_BLOCK_MODE_OUTLINE_FILL   3
 
#define SEGMENT_LCD_NUM_BLOCK_COLUMNS   7
 

Enumerations

enum  SegmentLCD_BlockMode_TypeDef {
  segmentLCDBlockModeBlank = SEGMENT_LCD_BLOCK_MODE_BLANK,
  segmentLCDBlockModeFill = SEGMENT_LCD_BLOCK_MODE_FILL,
  segmentLCDBlockModeOutline = SEGMENT_LCD_BLOCK_MODE_OUTLINE,
  segmentLCDBlockModeOutlineFill = SEGMENT_LCD_BLOCK_MODE_OUTLINE_FILL
}
 

Functions

void SegmentLCD_AllOff (void)
 Disable all segments.
 
void SegmentLCD_AllOn (void)
 Enable all segments.
 
void SegmentLCD_AlphaNumberOff (void)
 Turn all segments on alpha characters in display off.
 
void SegmentLCD_ARing (int anum, int on)
 Light up or shut off Ring of Indicators.
 
void SegmentLCD_Battery (int batteryLevel)
 Light up or shut off Battery Indicator.
 
void SegmentLCD_Block (SegmentLCD_BlockMode_TypeDef topMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS], SegmentLCD_BlockMode_TypeDef botMode[SEGMENT_LCD_NUM_BLOCK_COLUMNS])
 
void SegmentLCD_Disable (void)
 Disables LCD controller.
 
void SegmentLCD_EnergyMode (int em, int on)
 Light up or shut off Energy Mode indicator.
 
void SegmentLCD_Init (bool useBoost)
 Segment LCD Initialization routine for EFM32 STK display.
 
void SegmentLCD_LowerHex (uint32_t num)
 Write a hexadecimal number on lower alphanumeric part of Segment LCD display.
 
void SegmentLCD_LowerNumber (int num)
 Write number on lower alphanumeric part of Segment LCD display.
 
void SegmentLCD_Number (int value)
 Write number on numeric part on Segment LCD display.
 
void SegmentLCD_NumberOff (void)
 Turn all segments on numeric digits in display off.
 
void SegmentLCD_Symbol (lcdSymbol s, int on)
 Light up or shut off various symbols on Segment LCD.
 
void SegmentLCD_UnsignedHex (uint32_t value)
 Write hexadecimal number on numeric part on Segment LCD display.
 
void SegmentLCD_Write (const char *string)
 Write text on LCD display.
 

Enumeration Type Documentation

Enumerator
segmentLCDBlockModeBlank 

Blank

segmentLCDBlockModeFill 

Fill

segmentLCDBlockModeOutline 

Outline

segmentLCDBlockModeOutlineFill 

Outline and fill

Definition at line 50 of file segmentlcd.h.

Function Documentation

void SegmentLCD_ARing ( int  anum,
int  on 
)

Light up or shut off Ring of Indicators.

Parameters
anum"Segment number" on "Ring", range 0 - 7
onZero is off, non-zero is on

Definition at line 1361 of file segmentlcd.c.

References MCU_DISPLAY::ARing, ARING_TypeDef::bit, ARING_TypeDef::com, and LCD_SegmentSet().

void SegmentLCD_Battery ( int  batteryLevel)

Light up or shut off Battery Indicator.

Parameters
batteryLevelBattery Level, 0 to 4 (0 turns all off)

Definition at line 1379 of file segmentlcd.c.

References MCU_DISPLAY::Battery, BATTERY_TypeDef::bit, BATTERY_TypeDef::com, and LCD_SegmentSet().

void SegmentLCD_EnergyMode ( int  em,
int  on 
)

Light up or shut off Energy Mode indicator.

Parameters
emEnergy Mode numer 0 to 4
onZero is off, non-zero is on

Definition at line 1406 of file segmentlcd.c.

References EM_TypeDef::bit, EM_TypeDef::com, MCU_DISPLAY::EMode, and LCD_SegmentSet().

void SegmentLCD_Init ( bool  useBoost)

Segment LCD Initialization routine for EFM32 STK display.

Parameters
useBoostSet to use voltage boost

Definition at line 448 of file segmentlcd.c.

References CMU, CMU_ClockDivSet(), CMU_ClockEnable(), CMU_ClockSelectSet(), CMU_LCDClkFDIVSet(), CMU_LCDCTRL_VBOOSTEN, cmuClock_LCD, cmuClock_LCDpre, cmuClock_LFA, cmuSelect_LFRCO, LCD_Init(), LCD_IntDisable(), LCD_SyncBusyDelay(), LCD_VBoostSet(), LCD_VLCDSelect(), lcdVLCDSelVExtBoost, and SegmentLCD_AllOff().

void SegmentLCD_LowerHex ( uint32_t  num)

Write a hexadecimal number on lower alphanumeric part of Segment LCD display.

Parameters
numHexadecimal number value to put on display, in range 0 to 0x0FFFFFFF

Definition at line 502 of file segmentlcd.c.

References SegmentLCD_Symbol(), and SegmentLCD_Write().

void SegmentLCD_LowerNumber ( int  num)

Write number on lower alphanumeric part of Segment LCD display.

Parameters
numNumeric value to put on display, in range -9999999 to +9999999

Definition at line 535 of file segmentlcd.c.

References SegmentLCD_Symbol(), and SegmentLCD_Write().

void SegmentLCD_Number ( int  value)

Write number on numeric part on Segment LCD display.

Parameters
valueNumeric value to put on display, in range -999 to +9999

Definition at line 580 of file segmentlcd.c.

References NUMBER_TypeDef::bit, NUMBER_TypeDef::com, LCD_FreezeEnable(), LCD_SegmentSet(), LCD_SyncBusyDelay(), MCU_DISPLAY::Number, Segment_Numbers, and SegmentLCD_NumberOff().

void SegmentLCD_Symbol ( lcdSymbol  s,
int  on 
)

Light up or shut off various symbols on Segment LCD.

Parameters
sWhich symbol to turn on or off
onZero is off, non-zero is on

Definition at line 661 of file segmentlcd.c.

References LCD_SegmentSet().

Referenced by SegmentLCD_LowerHex(), and SegmentLCD_LowerNumber().

void SegmentLCD_UnsignedHex ( uint32_t  value)

Write hexadecimal number on numeric part on Segment LCD display.

Parameters
valueNumeric value to put on display

Definition at line 1015 of file segmentlcd.c.

References NUMBER_TypeDef::bit, NUMBER_TypeDef::com, LCD_FreezeEnable(), LCD_SegmentSet(), LCD_SyncBusyDelay(), MCU_DISPLAY::Number, Segment_Numbers, and SegmentLCD_NumberOff().

void SegmentLCD_Write ( const char *  string)

Write text on LCD display.

Parameters
stringText string to show on display

Definition at line 1062 of file segmentlcd.c.

References CHAR_TypeDef::bit, CHAR_TypeDef::com, LCD_FreezeEnable(), LCD_SegmentSet(), LCD_SyncBusyDelay(), Segment_Alphabet, SegmentLCD_AlphaNumberOff(), and MCU_DISPLAY::Text.

Referenced by SegmentLCD_LowerHex(), and SegmentLCD_LowerNumber().