GPIO_P_TypeDef Struct ReferenceDevices

GPIO_P EFM32TG GPIO P.

Definition at line 46 of file efm32tg_gpio_p.h.

#include <efm32tg_gpio_p.h>

Data Fields

__IOM uint32_t CTRL
 
__IM uint32_t DIN
 
__IOM uint32_t DOUT
 
__OM uint32_t DOUTCLR
 
__OM uint32_t DOUTSET
 
__OM uint32_t DOUTTGL
 
__IOM uint32_t MODEH
 
__IOM uint32_t MODEL
 
__IOM uint32_t PINLOCKN
 

Field Documentation

__IOM uint32_t GPIO_P_TypeDef::CTRL

Port Control Register

Definition at line 47 of file efm32tg_gpio_p.h.

__IM uint32_t GPIO_P_TypeDef::DIN

Port Data In Register

Definition at line 54 of file efm32tg_gpio_p.h.

__IOM uint32_t GPIO_P_TypeDef::DOUT

Port Data Out Register

Definition at line 50 of file efm32tg_gpio_p.h.

__OM uint32_t GPIO_P_TypeDef::DOUTCLR

Port Data Out Clear Register

Definition at line 52 of file efm32tg_gpio_p.h.

__OM uint32_t GPIO_P_TypeDef::DOUTSET

Port Data Out Set Register

Definition at line 51 of file efm32tg_gpio_p.h.

__OM uint32_t GPIO_P_TypeDef::DOUTTGL

Port Data Out Toggle Register

Definition at line 53 of file efm32tg_gpio_p.h.

__IOM uint32_t GPIO_P_TypeDef::MODEH

Port Pin Mode High Register

Definition at line 49 of file efm32tg_gpio_p.h.

__IOM uint32_t GPIO_P_TypeDef::MODEL

Port Pin Mode Low Register

Definition at line 48 of file efm32tg_gpio_p.h.

__IOM uint32_t GPIO_P_TypeDef::PINLOCKN

Port Unlocked Pins Register

Definition at line 55 of file efm32tg_gpio_p.h.


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG/Include/efm32tg_gpio_p.h