LESENSE_TypeDef Struct ReferenceDevices > EFM32TG_LESENSE
Definition at line
48
of file
efm32tg_lesense.h
.
Data Fields |
|
| __IOM uint32_t | ALTEXCONF |
| __IOM uint32_t | BIASCTRL |
| LESENSE_BUF_TypeDef | BUF [16U] |
| __IM uint32_t | BUFDATA |
| LESENSE_CH_TypeDef | CH [16U] |
| __IOM uint32_t | CHEN |
| __IOM uint32_t | CMD |
| __IOM uint32_t | CTRL |
| __IM uint32_t | CURCH |
| __IOM uint32_t | DECCTRL |
| __IOM uint32_t | DECSTATE |
| __IOM uint32_t | IDLECONF |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | PERCTRL |
| __IOM uint32_t | POWERDOWN |
| __IM uint32_t | PTR |
| uint32_t | RESERVED0 [105U] |
| __IOM uint32_t | ROUTE |
| __IM uint32_t | SCANRES |
| __IOM uint32_t | SENSORSTATE |
| LESENSE_ST_TypeDef | ST [16U] |
| __IM uint32_t | STATUS |
| __IM uint32_t | SYNCBUSY |
| __IOM uint32_t | TIMCTRL |
Field Documentation
| __IOM uint32_t LESENSE_TypeDef::ALTEXCONF |
Alternative excite pin configuration
Definition at line
64
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::BIASCTRL |
Bias Control Register
Definition at line
53
of file
efm32tg_lesense.h
.
| LESENSE_BUF_TypeDef LESENSE_TypeDef::BUF[16U] |
Scanresult
Definition at line
76
of file
efm32tg_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::BUFDATA |
Result buffer data register
Definition at line
59
of file
efm32tg_lesense.h
.
| LESENSE_CH_TypeDef LESENSE_TypeDef::CH[16U] |
Scanconfig
Definition at line
78
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::CHEN |
Channel enable Register
Definition at line
55
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::CMD |
Command Register
Definition at line
54
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::CTRL |
Control Register
Definition at line
49
of file
efm32tg_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::CURCH |
Current channel index
Definition at line
60
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::DECCTRL |
Decoder control Register
Definition at line
52
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::DECSTATE |
Current decoder state
Definition at line
61
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::IDLECONF |
GPIO Idle phase configuration
Definition at line
63
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::IEN |
Interrupt Enable Register
Definition at line
68
of file
efm32tg_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::IF |
Interrupt Flag Register
Definition at line
65
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line
66
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line
67
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::PERCTRL |
Peripheral Control Register
Definition at line
51
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::POWERDOWN |
LESENSE RAM power-down register
Definition at line
71
of file
efm32tg_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::PTR |
Result buffer pointers
Definition at line
58
of file
efm32tg_lesense.h
.
| uint32_t LESENSE_TypeDef::RESERVED0[105U] |
Reserved registers
Definition at line
73
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::ROUTE |
I/O Routing Register
Definition at line
70
of file
efm32tg_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::SCANRES |
Scan result register
Definition at line
56
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::SENSORSTATE |
Decoder input register
Definition at line
62
of file
efm32tg_lesense.h
.
| LESENSE_ST_TypeDef LESENSE_TypeDef::ST[16U] |
Decoding states
Definition at line
74
of file
efm32tg_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::STATUS |
Status Register
Definition at line
57
of file
efm32tg_lesense.h
.
| __IM uint32_t LESENSE_TypeDef::SYNCBUSY |
Synchronization Busy Register
Definition at line
69
of file
efm32tg_lesense.h
.
| __IOM uint32_t LESENSE_TypeDef::TIMCTRL |
Timing Control Register
Definition at line
50
of file
efm32tg_lesense.h
.
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG/Include/
efm32tg_lesense.h