CALIBRATE_TypeDef Struct ReferenceDevices > EFM32TG_CALIBRATE
Definition at line 49
of file efm32tg_calibrate.h
.
Data Fields | |
__IM uint32_t | ADDRESS |
__IM uint32_t | VALUE |
Field Documentation
__IM uint32_t CALIBRATE_TypeDef::ADDRESS |
Address of calibration register
Definition at line 50
of file efm32tg_calibrate.h
.
__IM uint32_t CALIBRATE_TypeDef::VALUE |
Default value for calibration register
Definition at line 51
of file efm32tg_calibrate.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG/Include/
efm32tg_calibrate.h