VCMP_TypeDef Struct ReferenceDevices > EFM32TG_VCMP

Definition at line 48 of file efm32tg_vcmp.h .

Data Fields

__IOM uint32_t CTRL
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
__IOM uint32_t INPUTSEL
__IM uint32_t STATUS

Field Documentation

__IOM uint32_t VCMP_TypeDef::CTRL

Control Register

Definition at line 49 of file efm32tg_vcmp.h .

__IOM uint32_t VCMP_TypeDef::IEN

Interrupt Enable Register

Definition at line 52 of file efm32tg_vcmp.h .

__IM uint32_t VCMP_TypeDef::IF

Interrupt Flag Register

Definition at line 53 of file efm32tg_vcmp.h .

__IOM uint32_t VCMP_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 55 of file efm32tg_vcmp.h .

__IOM uint32_t VCMP_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 54 of file efm32tg_vcmp.h .

__IOM uint32_t VCMP_TypeDef::INPUTSEL

Input Selection Register

Definition at line 50 of file efm32tg_vcmp.h .

__IM uint32_t VCMP_TypeDef::STATUS

Status Register

Definition at line 51 of file efm32tg_vcmp.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32TG/Include/ efm32tg_vcmp.h