CSEN_TypeDef Struct ReferenceDevices > CSEN
CSEN Register Declaration
Definition at line
49
of file
efr32bg13p_csen.h
.
#include <
efr32bg13p_csen.h
>
Data Fields |
|
| __IOM uint32_t | ANACTRL |
| __IM uint32_t | APORTCONFLICT |
| __IM uint32_t | APORTREQ |
| __IOM uint32_t | CMD |
| __IOM uint32_t | CMPTHR |
| __IOM uint32_t | CTRL |
| __IOM uint32_t | DATA |
| __IOM uint32_t | DMBASELINE |
| __IOM uint32_t | DMCFG |
| __IOM uint32_t | EMA |
| __IOM uint32_t | EMACTRL |
| __IOM uint32_t | IEN |
| __IM uint32_t | IF |
| __IOM uint32_t | IFC |
| __IOM uint32_t | IFS |
| __IOM uint32_t | PRSSEL |
| uint32_t | RESERVED0 [2U] |
| __IOM uint32_t | SCANINPUTSEL0 |
| __IOM uint32_t | SCANINPUTSEL1 |
| __IOM uint32_t | SCANMASK0 |
| __IOM uint32_t | SCANMASK1 |
| __IOM uint32_t | SINGLECTRL |
| __IM uint32_t | STATUS |
| __IOM uint32_t | TIMCTRL |
Field Documentation
| __IOM uint32_t CSEN_TypeDef::ANACTRL |
Analog Control
Definition at line
68
of file
efr32bg13p_csen.h
.
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IM uint32_t CSEN_TypeDef::APORTCONFLICT |
APORT Request Conflict
Definition at line
61
of file
efr32bg13p_csen.h
.
| __IM uint32_t CSEN_TypeDef::APORTREQ |
APORT Request Status
Definition at line
60
of file
efr32bg13p_csen.h
.
| __IOM uint32_t CSEN_TypeDef::CMD |
| __IOM uint32_t CSEN_TypeDef::CMPTHR |
Comparator Threshold
Definition at line
62
of file
efr32bg13p_csen.h
.
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::CTRL |
Control
Definition at line
50
of file
efr32bg13p_csen.h
.
Referenced by CSEN_Disable() , CSEN_Enable() , CSEN_Init() , CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::DATA |
Output Data
Definition at line
55
of file
efr32bg13p_csen.h
.
Referenced by CSEN_DataGet() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::DMBASELINE |
Delta Modulation Baseline
Definition at line
66
of file
efr32bg13p_csen.h
.
Referenced by CSEN_DMBaselineSet() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::DMCFG |
Delta Modulation Configuration
Definition at line
67
of file
efr32bg13p_csen.h
.
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::EMA |
Exponential Moving Average
Definition at line
63
of file
efr32bg13p_csen.h
.
Referenced by CSEN_EMAGet() , CSEN_EMASet() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::EMACTRL |
Exponential Moving Average Control
Definition at line
64
of file
efr32bg13p_csen.h
.
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::IEN |
Interrupt Enable
Definition at line
74
of file
efr32bg13p_csen.h
.
Referenced by CSEN_IntDisable() , CSEN_IntEnable() , CSEN_IntGetEnabled() , and CSEN_Reset() .
| __IM uint32_t CSEN_TypeDef::IF |
Interrupt Flag
Definition at line
71
of file
efr32bg13p_csen.h
.
Referenced by CSEN_IntGet() , and CSEN_IntGetEnabled() .
| __IOM uint32_t CSEN_TypeDef::IFC |
Interrupt Flag Clear
Definition at line
73
of file
efr32bg13p_csen.h
.
Referenced by CSEN_IntClear() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::IFS |
| __IOM uint32_t CSEN_TypeDef::PRSSEL |
PRS Select
Definition at line
54
of file
efr32bg13p_csen.h
.
Referenced by CSEN_Init() , and CSEN_Reset() .
| uint32_t CSEN_TypeDef::RESERVED0[2U] |
Reserved for future use
Definition at line
70
of file
efr32bg13p_csen.h
.
| __IOM uint32_t CSEN_TypeDef::SCANINPUTSEL0 |
Scan Input Selection 0
Definition at line
57
of file
efr32bg13p_csen.h
.
Referenced by CSEN_Init() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::SCANINPUTSEL1 |
Scan Input Selection 1
Definition at line
59
of file
efr32bg13p_csen.h
.
Referenced by CSEN_Init() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::SCANMASK0 |
Scan Channel Mask 0
Definition at line
56
of file
efr32bg13p_csen.h
.
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::SCANMASK1 |
Scan Channel Mask 1
Definition at line
58
of file
efr32bg13p_csen.h
.
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IOM uint32_t CSEN_TypeDef::SINGLECTRL |
Single Conversion Control
Definition at line
65
of file
efr32bg13p_csen.h
.
Referenced by CSEN_InitMode() , and CSEN_Reset() .
| __IM uint32_t CSEN_TypeDef::STATUS |
| __IOM uint32_t CSEN_TypeDef::TIMCTRL |
Timing Control
Definition at line
51
of file
efr32bg13p_csen.h
.
Referenced by CSEN_Init() , and CSEN_Reset() .
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG13P/Include/
efr32bg13p_csen.h