FPUEH_TypeDef Struct ReferenceDevices > FPUEH
FPUEH Register Declaration
Definition at line 49
of file efr32bg13p_fpueh.h
.
#include <
efr32bg13p_fpueh.h
>
Data Fields | |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
Field Documentation
__IOM uint32_t FPUEH_TypeDef::IEN |
Interrupt Enable Register
Definition at line 53
of file efr32bg13p_fpueh.h
.
__IM uint32_t FPUEH_TypeDef::IF |
Interrupt Flag Register
Definition at line 50
of file efr32bg13p_fpueh.h
.
__IOM uint32_t FPUEH_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 52
of file efr32bg13p_fpueh.h
.
__IOM uint32_t FPUEH_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 51
of file efr32bg13p_fpueh.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFR32BG13P/Include/
efr32bg13p_fpueh.h