MSC_ExecConfig_TypeDef Struct ReferenceEMLIB > MSC
Code execution configuration.
Definition at line 165
of file em_msc.h
.
#include <
em_msc.h
>
Data Fields | |
bool | aiDis |
bool | iccDis |
bool | ifcDis |
bool | prefetchEn |
bool | scbtEn |
bool | useHprot |
Field Documentation
bool MSC_ExecConfig_TypeDef::aiDis |
Disable automatic cache invalidation on write or erase.
Definition at line 169
of file em_msc.h
.
Referenced by MSC_ExecConfigSet().
bool MSC_ExecConfig_TypeDef::iccDis |
Disable automatic caching of fetches in interrupt context.
Definition at line 170
of file em_msc.h
.
Referenced by MSC_ExecConfigSet().
bool MSC_ExecConfig_TypeDef::ifcDis |
Disable instruction cache.
Definition at line 168
of file em_msc.h
.
Referenced by MSC_ExecConfigSet().
bool MSC_ExecConfig_TypeDef::prefetchEn |
bool MSC_ExecConfig_TypeDef::scbtEn |
Enable Suppressed Conditional Branch Target Prefetch.
Definition at line 166
of file em_msc.h
.
Referenced by MSC_ExecConfigSet().
bool MSC_ExecConfig_TypeDef::useHprot |
Use ahb_hprot to determine if the instruction is cacheable or not.
Definition at line 171
of file em_msc.h
.
Referenced by MSC_ExecConfigSet().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_msc.h