EZRADIODRV_HandleData Struct ReferenceEMDRV > EZRADIODRV > Plugin_System > Plugin_Manager

EzRadio driver instance initialization and handler structure. This data structure contains a number of EzRadio driver configuration options. Handler to this structure is passed to ezradioInit() when initializing an EzRadio driver instance. Some common initialization data sets are predefined in EZRADIODRV_INIT_DEFAULT. Note: All the referenced plug-in instances has there own handler sturcture, that is referenced from this structure.

Definition at line 302 of file ezradio_plugin_manager.h.

#include <ezradio_plugin_manager.h>

Data Fields

EZRADIODRV_AutoAckHandle_t autoAck
 Auto-acknowledge plug-in handler.
 
EZRADIODRV_DirectRxHandle_t directRx
 Direct reception plug-in handler.
 
EZRADIODRV_DirectTxHandle_t directTx
 Direct transmission plug-in handler.
 
EZRADIODRV_PacketCrcErrorHandle_t packetCrcError
 Packet reception with CRC error plug-in handler.
 
EZRADIODRV_PacketRxHandle_t packetRx
 Packet reception plug-in handler.
 
EZRADIODRV_PacketTxHandle_t packetTx
 Packet transmission plug-in handler.
 
EZRADIODRV_Pn9Handle_t pn9
 PN9 plug-in handler.
 
EZRADIODRV_UnmodCarrierHandle_t unmodCarrier
 Unmodulated carrier plug-in handler.
 

The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emdrv/ezradiodrv/plugins/inc/ezradio_plugin_manager.h