MSCEMLIB
Detailed Description
Memory System Controller API.
Contains functions to control the MSC, primarily the Flash. Users can perform Flash memory write and erase operations, as well as optimization of the CPU instruction fetch interface for the application. Available instruction fetch features depends on the MCU or SoC family, but features such as instruction pre-fetch, cache, and configurable branch prediction are typically available.
- Note
- Flash wait-state configuration is handled by CMU module. When core clock configuration is changed by a call to functions such as CMU_ClockSelectSet() or CMU_HFRCOBandSet() , then Flash wait-state configuration is also updated.
MSC resets into a safe state. To initialize the instruction interface to recommended settings:
- Note
- The optimal configuration is highly application dependent. Performance benchmarking is supported by most families. See MSC_StartCacheMeasurement() and MSC_GetCacheMeasurement() for more details.
Support for Flash write and erase runs from RAM by default. This code may be allocated to Flash by defining EM_MSC_RUN_FROM_FLASH .
- Note
- Flash erase may add ms of delay to interrupt latency if executing from Flash.
Flash write and erase operations are supported by MSC_WriteWord() , MSC_WriteWordFast(), MSC_ErasePage() , and MSC_MassErase(). Fast write is not supported for EFM32G and mass erase is supported for MCU and SoC families with larger Flash sizes.
- Note
- MSC_Init() must be called prior to any Flash write or erase operation.
The following steps are necessary to perform a page erase and write:
Data Structures |
|
| struct | MSC_ExecConfig_TypeDef |
Macros |
|
| #define | EM_MSC_RUN_FROM_FLASH |
|
By compiling with define EM_MSC_RUN_FROM_FLASH, functions performing erase or write operations will remain in and execute from Flash. This is useful for targets that don't want to allocate RAM space to hold the flash functions. Without this define, code for Flash operations will be copied into RAM at startup.
|
|
| #define | MSC_EXECCONFIG_DEFAULT |
| #define | MSC_PROGRAM_TIMEOUT 10000000ul |
|
Timeout used while waiting for Flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout.
|
|
| #define | MSC_RAMFUNC_DECLARATOR |
|
Expands to
SL_RAMFUNC_DECLARATOR
if
EM_MSC_RUN_FROM_FLASH
is undefined and to nothing if
EM_MSC_RUN_FROM_FLASH
is defined.
|
|
| #define | MSC_RAMFUNC_DEFINITION_BEGIN |
|
Expands to
SL_RAMFUNC_DEFINITION_BEGIN
if
EM_MSC_RUN_FROM_FLASH
is undefined and to nothing if
EM_MSC_RUN_FROM_FLASH
is defined.
|
|
| #define | MSC_RAMFUNC_DEFINITION_END |
|
Expands to
SL_RAMFUNC_DEFINITION_END
if
EM_MSC_RUN_FROM_FLASH
is undefined and to nothing if
EM_MSC_RUN_FROM_FLASH
is defined.
|
|
Enumerations |
|
| enum |
MSC_Status_TypeDef
{
mscReturnOk = 0, mscReturnInvalidAddr = -1, mscReturnLocked = -2, mscReturnTimeOut = -3, mscReturnUnaligned = -4 } |
Functions |
|
| void | MSC_Deinit (void) |
|
Disables the flash controller for writing.
|
|
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_ErasePage (uint32_t *startAddress) |
|
Erases a page in flash memory.
|
|
| void | MSC_ExecConfigSet ( MSC_ExecConfig_TypeDef *execConfig) |
|
Set the MSC code execution configuration.
|
|
| void | MSC_Init (void) |
|
Enables the flash controller for writing.
|
|
| __STATIC_INLINE void | MSC_IntClear (uint32_t flags) |
|
Clear one or more pending MSC interrupts.
|
|
| __STATIC_INLINE void | MSC_IntDisable (uint32_t flags) |
|
Disable one or more MSC interrupts.
|
|
| __STATIC_INLINE void | MSC_IntEnable (uint32_t flags) |
|
Enable one or more MSC interrupts.
|
|
| __STATIC_INLINE uint32_t | MSC_IntGet (void) |
|
Get pending MSC interrupt flags.
|
|
| __STATIC_INLINE uint32_t | MSC_IntGetEnabled (void) |
|
Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
|
|
| __STATIC_INLINE void | MSC_IntSet (uint32_t flags) |
|
Set one or more pending MSC interrupts from SW.
|
|
| MSC_RAMFUNC_DECLARATOR MSC_Status_TypeDef | MSC_WriteWord (uint32_t *address, void const *data, uint32_t numBytes) |
|
Writes data to flash memory. This function is interrupt-safe, but slower than MSC_WriteWordFast(), which writes to flash with interrupts disabled. Write data must be aligned to words and contain a number of bytes that is divisible by four.
|
|
Macro Definition Documentation
| #define EM_MSC_RUN_FROM_FLASH |
By compiling with define EM_MSC_RUN_FROM_FLASH, functions performing erase or write operations will remain in and execute from Flash. This is useful for targets that don't want to allocate RAM space to hold the flash functions. Without this define, code for Flash operations will be copied into RAM at startup.
- Note
- This define is not present by default. The MSC controller API will run from RAM by default.
Definition at line
124
of file
em_msc.h
.
| #define MSC_EXECCONFIG_DEFAULT |
Default MSC ExecConfig initialization.
Definition at line
174
of file
em_msc.h
.
| #define MSC_PROGRAM_TIMEOUT 10000000ul |
Timeout used while waiting for Flash to become ready after a write. This number indicates the number of iterations to perform before issuing a timeout.
- Note
- Timeout is set very large (in the order of 100x longer than necessary). This is to avoid any corner case.
Definition at line
109
of file
em_msc.h
.
Referenced by MSC_ErasePage() .
Enumeration Type Documentation
| enum MSC_Status_TypeDef |
Return codes for writing/erasing Flash.
Definition at line
132
of file
em_msc.h
.
Function Documentation
| MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_ErasePage | ( | uint32_t * |
startAddress
|
) |
Erases a page in flash memory.
- Note
- It is recommended to run this code from RAM. On the Gecko family, it is required to run this function from RAM.
For IAR IDE, Rowley IDE, SimplicityStudio IDE, Atollic IDE, and ARM GCC IDE, this is achieved automatically by using attributes in the function proctype. For Keil uVision IDE, define a section called "ram_code" and place this manually in the project's scatter file.
- Parameters
-
[in] startAddressA pointer to the flash page to erase. Must be aligned to the beginning of the page boundary.
- Returns
-
Returns the status of erase operation,
MSC_Status_TypeDef
* mscReturnOk - The operation completed successfully. * mscReturnInvalidAddr - The operation tried to erase a non-flash area. * mscReturnLocked - The operation tried to erase a locked area of the flash. * mscReturnTimeOut - The operation timed out waiting for the flash operation * to complete. *
Definition at line
1140
of file
em_msc.c
.
References EMU , FLASH_PAGE_SIZE , MSC , MSC_LOCK_LOCKKEY_LOCK , MSC_LOCK_LOCKKEY_UNLOCK , MSC_PROGRAM_TIMEOUT , MSC_STATUS_BUSY , MSC_STATUS_INVADDR , MSC_STATUS_LOCKED , MSC_WRITECMD_ERASEPAGE , MSC_WRITECMD_LADDRIM , MSC_WRITECTRL_WREN , mscReturnInvalidAddr , mscReturnLocked , mscReturnOk , and mscReturnTimeOut .
Referenced by NVMHAL_PageErase() .
| void MSC_ExecConfigSet | ( | MSC_ExecConfig_TypeDef * |
execConfig
|
) |
Set the MSC code execution configuration.
- Parameters
-
[in] execConfigThe code execution configuration.
Definition at line
661
of file
em_msc.c
.
References _MSC_READCTRL_MODE_MASK , MSC_ExecConfig_TypeDef::aiDis , MSC_ExecConfig_TypeDef::iccDis , MSC_ExecConfig_TypeDef::ifcDis , MSC , MSC_READCTRL_MODE_WS0 , MSC_READCTRL_MODE_WS0SCBTP , MSC_READCTRL_MODE_WS1 , MSC_READCTRL_MODE_WS1SCBTP , MSC_ExecConfig_TypeDef::prefetchEn , MSC_ExecConfig_TypeDef::scbtEn , and MSC_ExecConfig_TypeDef::useHprot .
| void MSC_Init | ( | void |
|
) |
Enables the flash controller for writing.
- Note
- This function must be called before flash operations when AUXHFRCO clock has been changed from a default band.
Definition at line
595
of file
em_msc.c
.
References CMU_ClockFreqGet() , cmuClock_AUX , EMU , MSC , MSC_UNLOCK_CODE , and MSC_WRITECTRL_WREN .
Referenced by DBG_DisableDebugAccess() , and NVMHAL_Init() .
| __STATIC_INLINE void MSC_IntClear | ( | uint32_t |
flags
|
) |
Clear one or more pending MSC interrupts.
- Parameters
-
[in] flagsPending MSC intterupt source to clear. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
248
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE void MSC_IntDisable | ( | uint32_t |
flags
|
) |
Disable one or more MSC interrupts.
- Parameters
-
[in] flagsMSC interrupt sources to disable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
265
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE void MSC_IntEnable | ( | uint32_t |
flags
|
) |
Enable one or more MSC interrupts.
- Note
- Depending on the use, a pending interrupt may already be set prior to enabling the interrupt. To ignore a pending interrupt, consider using MSC_IntClear() prior to enabling the interrupt.
- Parameters
-
[in] flagsMSC interrupt sources to enable. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
287
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE uint32_t MSC_IntGet | ( | void |
|
) |
Get pending MSC interrupt flags.
- Note
- The event bits are not cleared by the use of this function.
- Returns
- MSC interrupt sources pending. A bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
307
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE uint32_t MSC_IntGetEnabled | ( | void |
|
) |
Get enabled and pending MSC interrupt flags. Useful for handling more interrupt sources in the same interrupt handler.
- Note
- Interrupt flags are not cleared by the use of this function.
- Returns
-
Pending and enabled MSC interrupt sources. The return value is the bitwise AND of
- the enabled interrupt sources in MSC_IEN and
- the pending interrupt flags MSC_IF
Definition at line
326
of file
em_msc.h
.
References MSC .
| __STATIC_INLINE void MSC_IntSet | ( | uint32_t |
flags
|
) |
Set one or more pending MSC interrupts from SW.
- Parameters
-
[in] flagsMSC interrupt sources to set to pending. Use a bitwise logic OR combination of valid interrupt flags for the MSC module (MSC_IF_nnn).
Definition at line
342
of file
em_msc.h
.
References MSC .
| MSC_RAMFUNC_DEFINITION_END MSC_RAMFUNC_DEFINITION_BEGIN MSC_Status_TypeDef MSC_WriteWord | ( | uint32_t * |
address,
|
| void const * |
data,
|
||
| uint32_t |
numBytes
|
||
| ) |
Writes data to flash memory. This function is interrupt-safe, but slower than MSC_WriteWordFast(), which writes to flash with interrupts disabled. Write data must be aligned to words and contain a number of bytes that is divisible by four.
- Note
- It is recommended to erase the flash page before performing a write.
It is recommended to run this code from RAM. On the Gecko family, it is required to run this function from RAM.
For IAR IDE, Rowley IDE, SimplicityStudio IDE, Atollic IDE, and ARM GCC IDE, this is done automatically by using attributes in the function proctype. For Keil uVision IDE, define a section called "ram_code" and place it manually in the project's scatter file.
This function requires a system core clock at 1 MHz or higher.
- Parameters
-
[in] addressA pointer to the flash word to write to. Must be aligned to words. [in] dataData to write to flash. [in] numBytesA number of bytes to write from flash. NB: Must be divisible by four.
- Returns
-
Returns the status of the write operation.
* flashReturnOk - The operation completed successfully. * flashReturnInvalidAddr - The operation tried to erase a non-flash area. * flashReturnLocked - The operation tried to erase a locked area of the Flash. * flashReturnTimeOut - The operation timed out waiting for the flash operation * to complete, or the MSC module timed out waiting for the software to write * the next word into the DWORD register. *
Definition at line
1243
of file
em_msc.c
.
Referenced by DBG_DisableDebugAccess() , and NVMHAL_Write() .