DAC_Init_TypeDef Struct ReferenceEMLIB > DAC
DAC initialization structure, common for both channels.
       Definition at line
       
        134
       
       of file
       
        em_dac.h
       
       .
      
      
       #include <
       
     
        em_dac.h
       
       >
      
         Data Fields | 
       |
| bool | ch0ResetPre | 
| DAC_ConvMode_TypeDef | convMode | 
| bool | diff | 
| bool | lpEnable | 
| bool | outEnablePRS | 
| DAC_Output_TypeDef | outMode | 
| uint8_t | prescale | 
| DAC_Ref_TypeDef | reference | 
| DAC_Refresh_TypeDef | refresh | 
| bool | sineEnable | 
Field Documentation
| bool DAC_Init_TypeDef::ch0ResetPre | 
Enable/disable reset of prescaler on ch0 start.
        Definition at line
        
         157
        
        of file
        
         em_dac.h
        
        .
       
Referenced by DAC_Init() .
| DAC_ConvMode_TypeDef DAC_Init_TypeDef::convMode | 
| bool DAC_Init_TypeDef::diff | 
Select if single ended or differential mode.
        Definition at line
        
         166
        
        of file
        
         em_dac.h
        
        .
       
Referenced by DAC_Init() .
| bool DAC_Init_TypeDef::lpEnable | 
Enable/disable use of low pass filter on output.
        Definition at line
        
         154
        
        of file
        
         em_dac.h
        
        .
       
| bool DAC_Init_TypeDef::outEnablePRS | 
Enable/disable output enable control by CH1 PRS signal.
        Definition at line
        
         160
        
        of file
        
         em_dac.h
        
        .
       
Referenced by DAC_Init() .
| DAC_Output_TypeDef DAC_Init_TypeDef::outMode | 
| uint8_t DAC_Init_TypeDef::prescale | 
Prescaler used to get DAC clock. Derived as follows: DACclk=HFPERclk/(2^prescale). The DAC clock should be <= 1MHz.
        Definition at line
        
         151
        
        of file
        
         em_dac.h
        
        .
       
Referenced by DAC_Init() .
| DAC_Ref_TypeDef DAC_Init_TypeDef::reference | 
| DAC_Refresh_TypeDef DAC_Init_TypeDef::refresh | 
Refresh interval. Only used if REFREN bit set for a DAC channel.
        Definition at line
        
         136
        
        of file
        
         em_dac.h
        
        .
       
Referenced by DAC_Init() .
| bool DAC_Init_TypeDef::sineEnable | 
The documentation for this struct was generated from the following file:
- 
       C:/repos/super_h1/platform/emlib/inc/
       
em_dac.h