CMU_HFXOInit_TypeDef Struct ReferenceEMLIB > CMU

HFXO initialization structure. Initialization values should be obtained from a configuration tool, app note, or xtal data sheet.

Definition at line 2182 of file em_cmu.h.

#include <em_cmu.h>

Data Fields

bool autoSelEm01
 
bool autoStartEm01
 
bool autoStartSelOnRacWakeup
 
uint16_t ctuneStartup
 
uint16_t ctuneSteadyState
 
bool lowPowerMode
 
CMU_OscMode_TypeDef mode
 
uint8_t regIshSteadyState
 
uint8_t thresholdPeakDetect
 
uint8_t timeoutPeakDetect
 
uint8_t timeoutShuntOptimization
 
uint8_t timeoutStartup
 
uint8_t timeoutSteady
 
uint8_t xoCoreBiasTrimStartup
 
uint8_t xoCoreBiasTrimSteadyState
 

Field Documentation

bool CMU_HFXOInit_TypeDef::autoSelEm01
Deprecated:
Use CMU_HFXOAutostartEnable instead.

Definition at line 2194 of file em_cmu.h.

Referenced by CMU_HFXOInit().

bool CMU_HFXOInit_TypeDef::autoStartEm01
Deprecated:
Use CMU_HFXOAutostartEnable instead.

Definition at line 2193 of file em_cmu.h.

Referenced by CMU_HFXOInit().

bool CMU_HFXOInit_TypeDef::autoStartSelOnRacWakeup
Deprecated:
Use CMU_HFXOAutostartEnable instead.

Definition at line 2195 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint16_t CMU_HFXOInit_TypeDef::ctuneStartup

Startup phase CTUNE (load capacitance) value

Definition at line 2196 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint16_t CMU_HFXOInit_TypeDef::ctuneSteadyState

Steady-state phase CTUNE (load capacitance) value

Definition at line 2197 of file em_cmu.h.

Referenced by BSP_initClocks(), and CMU_HFXOInit().

bool CMU_HFXOInit_TypeDef::lowPowerMode

Enable low-power mode

Definition at line 2192 of file em_cmu.h.

Referenced by CMU_HFXOInit().

CMU_OscMode_TypeDef CMU_HFXOInit_TypeDef::mode

Oscillator mode

Definition at line 2211 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::regIshSteadyState

Shunt steady-state current

Definition at line 2198 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::thresholdPeakDetect

Peak detection threshold

Definition at line 2201 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::timeoutPeakDetect

Timeout - peak detection

Definition at line 2203 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::timeoutShuntOptimization

Timeout - shunt optimization

Definition at line 2202 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::timeoutStartup

Timeout - startup

Definition at line 2205 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::timeoutSteady

Timeout - steady-state

Definition at line 2204 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimStartup

Startup XO core bias current trim

Definition at line 2199 of file em_cmu.h.

Referenced by CMU_HFXOInit().

uint8_t CMU_HFXOInit_TypeDef::xoCoreBiasTrimSteadyState

Steady-state XO core bias current trim

Definition at line 2200 of file em_cmu.h.

Referenced by CMU_HFXOInit().


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/platform/emlib/inc/em_cmu.h