cal_ref_t Struct Reference

Structure Definition for calref array.

Definition at line 780 of file si114x_functions.c .

Data Fields

uint32_t ledi_65ma
uint32_t lirpd_adchi_irled
uint32_t sirpd_adchi_irled
uint32_t sirpd_adclo_irled
uint32_t sirpd_adclo_whled
uint8_t ucoef [4]
uint32_t vispd_adchi_whled
uint32_t vispd_adclo_whled

Field Documentation

uint32_t cal_ref_t::ledi_65ma

LED Current Ratio at 65 mA

Definition at line 787 of file si114x_functions.c .

uint32_t cal_ref_t::lirpd_adchi_irled

Large IR PD gain, IR LED, Hi ADC Range

Definition at line 786 of file si114x_functions.c .

uint32_t cal_ref_t::sirpd_adchi_irled

Small IR PD gain, IR LED, Hi ADC Range

Definition at line 781 of file si114x_functions.c .

uint32_t cal_ref_t::sirpd_adclo_irled

Small IR PD gain, IR LED, Lo ADC Range

Definition at line 782 of file si114x_functions.c .

uint32_t cal_ref_t::sirpd_adclo_whled

Small IR PD gain, White LED, Lo ADC Range

Definition at line 783 of file si114x_functions.c .

uint8_t cal_ref_t::ucoef[4]

UV Coefficient Storage

Definition at line 788 of file si114x_functions.c .

Referenced by si114x_get_calibration() .

uint32_t cal_ref_t::vispd_adchi_whled

VIS PD gain, White LED, Lo ADC Range

Definition at line 784 of file si114x_functions.c .

uint32_t cal_ref_t::vispd_adclo_whled

VIS PD gain, White LED, Lo ADC Range

Definition at line 785 of file si114x_functions.c .


The documentation for this struct was generated from the following file:
  • C:/repos/super_h1/hardware/kit/common/drivers/ si114x_functions.c