ASSERT
Detailed Description
Error checking module.
By default, EMLIB library assert usage is not included to reduce footprint and processing overhead. Further, EMLIB assert usage is decoupled from ISO C assert handling (NDEBUG usage) to allow using ISO C assert without including EMLIB assert statements.
Below are available defines for controlling EMLIB assert inclusion. The defines are typically for a project to be used by the preprocessor.
- If DEBUG_EFM is defined, the internal EMLIB library assert handling will be used. This is implemented as a simple while(true) loop. DEBUG_EFM is not defined by default.
 
- If DEBUG_EFM_USER is defined, the user must provide custom implementation of the assertEFM() function.
 
- If both DEBUG_EFM and DEBUG_EFM_USER are undefined, all EFM_ASSERT() statements are not operational.
 
- Note
 - The internal EMLIB assert is documented because DEBUG_EFM is defined in the doxygen configuration.
 
This module contains functions to control the ASSERT peripheral of Silicon Labs 32-bit MCUs and SoCs.
         Macros | 
       |
| #define | EFM_ASSERT (expr) ((expr) ? ((void)0) : assertEFM (__FILE__, __LINE__)) | 
         Functions | 
       |
| void | assertEFM (const char *file, int line) | 
| 
         EFM internal assert handling.
          | 
       |
Function Documentation
| void assertEFM | ( | const char * | 
           
            file,
           
           | 
         
| int | 
           
            line
           
           | 
         ||
| ) | 
EFM internal assert handling.
This function is invoked through EFM_ASSERT() macro usage only and should not be used explicitly.
This implementation enters an indefinite loop, allowing the use of a debugger to determine a cause of failure. By defining DEBUG_EFM_USER to the preprocessor for all files, a user-defined version of this function must be defined and will be invoked instead, possibly providing output of assertion location.
- Note
 - This function is not used unless DEBUG_EFM is defined during preprocessing of EFM_ASSERT() usage.
 
- Parameters
 - 
         
[in] fileName of the source file where assertion failed. [in] lineA line number in the source file where assertion failed.  
        Definition at line
        
         71
        
        of file
        
         em_assert.c
        
        .