RetargetIo
Detailed Description
Standard I/O retargeting driver.
This module provide low-level retargeting of stdio for all supported toolchains.
      
     
Retarget TextDisplay Module
      The source code of the RETARGETTEXTDISPLAY module is implemented in kits/common/drivers/retargettextdisplay.c and
      
       retargettextdisplay.h
      
      .
     
      
     
Introduction
The RETARGETTEXTDISPLAY Library implements a stdout interface to a textdisplay device ( TextDisplay Library ) in order for the user to print text by calling standard C language functions that prints text to stdout.
      
     
Retarget TextDisplay Configuration.
This section contains a description of the configuration parameters of the RETARGETTEXTDISPLAY Library.
#define RETARGETTEXTDISPLAY_SCROLL_MODE
       Set to 'true' to enable scroll mode on the text display device where
       stdout is retargeted. Set to 'false' to disable scroll mode.
#define RETARGETTEXTDISPLAY_LINE_FEED_MODE
       Set to 'true' to enable adding Carriage Return (CR) to Line Feed (LF)
       characters on the text display device where stdout is retargeted.
       Set to 'false' to disable line feed mode.
#define RETARGETTEXTDISPLAY_DISPLAY_NO
       Select which TEXTDISPLAY device number to retarget stdout to. Normally
       there is only one display device present in the system therefore this
       parameter should be zero. However if there are more than one display
       device the user may want to select a different display device.
     
         Macros | 
       |
| #define | RXBUFSIZE 8 | 
| #define | setupSWOForPrint RETARGET_SwoInit | 
         Functions | 
       |
| int | _close (int file) | 
| 
         Close a file.
          | 
       |
| void | _exit (int status) | 
| 
         Exit the program.
          | 
       |
| int | _fstat (int file, struct stat *st) | 
| 
         Status of an open file.
          | 
       |
| int | _getpid (void) | 
| 
         Get process ID.
          | 
       |
| int | _isatty (int file) | 
| 
         Query whether output stream is a terminal.
          | 
       |
| int | _kill (int pid, int sig) | 
| 
         Send signal to process.
          | 
       |
| int | _lseek (int file, int ptr, int dir) | 
| 
         Set position in a file.
          | 
       |
| int | _read (int file, char *ptr, int len) | 
| 
         Read from a file.
          | 
       |
| caddr_t | _sbrk (int incr) | 
| 
         Increase heap.
          | 
       |
| int | _write (int file, const char *ptr, int len) | 
| 
         Write to a file.
          | 
       |
| static void | disableRxInterrupt () | 
| 
         Disable RX interrupt.
          | 
       |
| static void | enableRxInterrupt () | 
| 
         Enable RX interrupt.
          | 
       |
| void | RETARGET_IRQ_NAME (void) | 
| 
         UART/LEUART IRQ Handler.
          | 
       |
| int | RETARGET_ReadChar (void) | 
| 
         Receive a byte from USART/LEUART and put into global buffer.
          | 
       |
| void | RETARGET_SerialCrLf (int on) | 
| 
         UART/LEUART toggle LF to CRLF conversion.
          | 
       |
| bool | RETARGET_SerialEnableFlowControl (void) | 
| 
         Enable hardware flow control. (RTS + CTS)
          | 
       |
| void | RETARGET_SerialFlush (void) | 
| 
         Flush UART/LEUART.
          | 
       |
| void | RETARGET_SerialInit (void) | 
| 
         Intializes UART/LEUART.
          | 
       |
| void | RETARGET_SwoInit (void) | 
| 
         Setup SWO for output.
          | 
       |
| EMSTATUS | RETARGET_TextDisplayInit (void) | 
| 
         Initialize/retarget a TEXTDISPLAY device to receivie stdout(put).
          | 
       |
| void | RETARGET_TftCrLf (int on) | 
| 
         Toggle LF to CRLF conversion.
          | 
       |
| void | RETARGET_TftInit (void) | 
| 
         Intializes TFT text display.
          | 
       |
| void | RETARGET_TFTTX (int c) | 
| 
         Transmit/display a character.
          | 
       |
| void | RETARGET_TFTUpdate (bool fullFrame) | 
| 
         Display framebuffer.
          | 
       |
| int | RETARGET_WriteChar (char c) | 
| 
         Transmit single byte to USART/LEUART.
          | 
       |
| EMSTATUS | RETARGET_WriteString (char *str) | 
| 
         Write a string of characters to the RETARGET text display device.
          | 
       |
         Variables | 
       |
| char | _end | 
| static bool | initialized = false | 
| static uint8_t | LFtoCRLF = 0 | 
| static volatile uint8_t | rxBuffer [ RXBUFSIZE ] | 
| static volatile int | rxCount = 0 | 
| static volatile int | rxReadIndex = 0 | 
| static volatile int | rxWriteIndex = 0 | 
Macro Definition Documentation
| #define RXBUFSIZE 8 | 
Buffer size for RX
        Definition at line
        
         64
        
        of file
        
         retargetserial.c
        
        .
       
Referenced by RETARGET_IRQ_NAME() , and RETARGET_ReadChar() .
| #define setupSWOForPrint RETARGET_SwoInit | 
- 
         
          
Deprecated: - Use RETARGET_SwoInit instead
 
        Definition at line
        
         55
        
        of file
        
         retargetswo.h
        
        .
       
Function Documentation
| int _close | ( | int | 
           
            file
           
           | 
          ) | 
Close a file.
- Parameters
 - 
         
[in] fileFile you want to close.  
- Returns
 - Returns 0 when the file is closed.
 
        Definition at line
        
         76
        
        of file
        
         retargetio.c
        
        .
       
| void _exit | ( | int | 
           
            status
           
           | 
          ) | 
Exit the program.
- Parameters
 - 
         
[in] statusThe value to return to the parent process as the exit status (not used).  
        Definition at line
        
         87
        
        of file
        
         retargetio.c
        
        .
       
| int _fstat | ( | int | 
           
            file,
           
           | 
         
| struct stat * | 
           
            st
           
           | 
         ||
| ) | 
Status of an open file.
- Parameters
 - 
         
[in] fileCheck status for this file. [in] stStatus information.  
- Returns
 - Returns 0 when st_mode is set to character special.
 
        Definition at line
        
         107
        
        of file
        
         retargetio.c
        
        .
       
| int _isatty | ( | int | 
           
            file
           
           | 
          ) | 
Query whether output stream is a terminal.
- Parameters
 - 
         
[in] fileDescriptor for the file.  
- Returns
 - Returns 1 when query is done.
 
        Definition at line
        
         132
        
        of file
        
         retargetio.c
        
        .
       
| int _kill | ( | int | 
           
            pid,
           
           | 
         
| int | 
           
            sig
           
           | 
         ||
| ) | 
Send signal to process.
- Parameters
 - 
         
[in] pidProcess id (not used). [in] sigSignal to send (not used).  
        Definition at line
        
         143
        
        of file
        
         retargetio.c
        
        .
       
| int _lseek | ( | int | 
           
            file,
           
           | 
         
| int | 
           
            ptr,
           
           | 
         ||
| int | 
           
            dir
           
           | 
         ||
| ) | 
Set position in a file.
- Parameters
 - 
         
[in] fileDescriptor for the file. [in] ptrPoiter to the argument offset. [in] dirDirectory whence.  
- Returns
 - Returns 0 when position is set.
 
        Definition at line
        
         166
        
        of file
        
         retargetio.c
        
        .
       
| int _read | ( | int | 
           
            file,
           
           | 
         
| char * | 
           
            ptr,
           
           | 
         ||
| int | 
           
            len
           
           | 
         ||
| ) | 
Read from a file.
- Parameters
 - 
         
[in] fileDescriptor for the file you want to read from. [in] ptrPointer to the chacaters that are beeing read. [in] lenNumber of characters to be read.  
- Returns
 - Number of characters that have been read.
 
        Definition at line
        
         190
        
        of file
        
         retargetio.c
        
        .
       
References RETARGET_ReadChar() , and rxCount .
| caddr_t _sbrk | ( | int | 
           
            incr
           
           | 
          ) | 
Increase heap.
- Parameters
 - 
         
[in] incrNumber of bytes you want increment the program's data space.  
- Returns
 - Rsturns a pointer to the start of the new area.
 
        Definition at line
        
         222
        
        of file
        
         retargetio.c
        
        .
       
References _end .
| int _write | ( | int | 
           
            file,
           
           | 
         
| const char * | 
           
            ptr,
           
           | 
         ||
| int | 
           
            len
           
           | 
         ||
| ) | 
Write to a file.
- Parameters
 - 
         
[in] fileDescriptor for the file you want to write to. [in] ptrPointer to the text you want to write [in] lenNumber of characters to be written.  
- Returns
 - Number of characters that have been written.
 
        Definition at line
        
         253
        
        of file
        
         retargetio.c
        
        .
       
References RETARGET_WriteChar() .
| int RETARGET_ReadChar | ( | void | 
           
           
           | 
          ) | 
Receive a byte from USART/LEUART and put into global buffer.
- Returns
 - -1 on failure, or positive character integer on sucesss
 
        Definition at line
        
         271
        
        of file
        
         retargetserial.c
        
        .
       
References CORE_DECLARE_IRQ_STATE , CORE_ENTER_ATOMIC , CORE_EXIT_ATOMIC , enableRxInterrupt() , initialized , RETARGET_SerialInit() , rxBuffer , RXBUFSIZE , rxCount , and rxReadIndex .
Referenced by _read() .
| void RETARGET_SerialCrLf | ( | int | 
           
            on
           
           | 
          ) | 
UART/LEUART toggle LF to CRLF conversion.
- Parameters
 - 
         
onIf non-zero, automatic LF to CRLF conversion will be enabled  
        Definition at line
        
         130
        
        of file
        
         retargetserial.c
        
        .
       
References LFtoCRLF .
| bool RETARGET_SerialEnableFlowControl | ( | void | 
           
           
           | 
          ) | 
Enable hardware flow control. (RTS + CTS)
- Returns
 - true if hardware flow control was enabled and false otherwise.
 
        Definition at line
        
         323
        
        of file
        
         retargetserial.c
        
        .
       
References GPIO_PinModeSet() , gpioModeInputPull , and gpioModePushPull .
| EMSTATUS RETARGET_TextDisplayInit | ( | void | 
           
           
           | 
          ) | 
Initialize/retarget a TEXTDISPLAY device to receivie stdout(put).
- Returns
 - EMSTATUS code of the operation.
 
        Definition at line
        
         59
        
        of file
        
         retargettextdisplay.c
        
        .
       
References DISPLAY_DeviceGet() , DISPLAY_EMSTATUS_OK , TEXTDISPLAY_Config_t::displayDeviceNo , TEXTDISPLAY_Config_t::lfToCrLf , TEXTDISPLAY_Config_t::scrollEnable , TEXTDISPLAY_EMSTATUS_OK , and TEXTDISPLAY_New() .
| void RETARGET_TftCrLf | ( | int | 
           
            on
           
           | 
          ) | 
Toggle LF to CRLF conversion.
- Parameters
 - 
         
onIf non-zero, automatic LF to CRLF conversion will be enabled  
        Definition at line
        
         80
        
        of file
        
         retargettft.c
        
        .
       
References LFtoCRLF .
| void RETARGET_TFTTX | ( | int | 
           
            c
           
           | 
          ) | 
Transmit/display a character.
- Parameters
 - 
         
[in] cASCII character to output  
- Returns
 - -1 on failure, or positive character integer on sucesss
 
        Definition at line
        
         185
        
        of file
        
         retargettft.c
        
        .
       
References charBuffer , CHARS , LINES , rgbColor , tftTextScrollUp() , xpos , and ypos .
Referenced by RETARGET_WriteChar() .
| void RETARGET_TFTUpdate | ( | bool | 
           
            fullFrame
           
           | 
          ) | 
Display framebuffer.
- Parameters
 - 
         
[in] fullFrameIf true, draw entire screen, if false, draw incremental update (faster)  
        Definition at line
        
         236
        
        of file
        
         retargettft.c
        
        .
       
References charBuffer , CHARS , fontBits , LINES , rgbColor , xpos , and ypos .
Referenced by RETARGET_WriteChar() .
| int RETARGET_WriteChar | ( | char | 
           
            c
           
           | 
          ) | 
Transmit single byte to USART/LEUART.
- Parameters
 - 
         
cCharacter to transmit  
- Returns
 - Transmitted character
 
        Definition at line
        
         304
        
        of file
        
         retargetserial.c
        
        .
       
References initialized , LFtoCRLF , and RETARGET_SerialInit() .
Referenced by _write() .
| EMSTATUS RETARGET_WriteString | ( | char * | 
           
            str
           
           | 
          ) | 
Write a string of characters to the RETARGET text display device.
- Parameters
 - 
         
[in] strString to write.  
- Returns
 - EMSTATUS code of the operation.
 
        Definition at line
        
         123
        
        of file
        
         retargettextdisplay.c
        
        .
       
References TEXTDISPLAY_EMSTATUS_NOT_INITIALIZED , and TEXTDISPLAY_WriteString() .
Variable Documentation
| char _end | 
Defined by the linker
Referenced by _sbrk() .
           
  | 
          static | 
Initialize UART/LEUART
        Definition at line
        
         71
        
        of file
        
         retargetserial.c
        
        .
       
Referenced by DMADRV_AllocateChannel() , DMADRV_DeInit() , DMADRV_FreeChannel() , DMADRV_Init() , DMADRV_LdmaStartTransfer() , DMADRV_PauseTransfer() , DMADRV_ResumeTransfer() , DMADRV_StopTransfer() , DMADRV_TransferActive() , DMADRV_TransferCompletePending() , DMADRV_TransferDone() , DMADRV_TransferRemainingCount() , RETARGET_ReadChar() , RETARGET_SerialInit() , RETARGET_WriteChar() , and TEXTDISPLAY_New() .
           
  | 
          static | 
LF to CRLF conversion disabled
        Definition at line
        
         70
        
        of file
        
         retargetserial.c
        
        .
       
Referenced by RETARGET_SerialCrLf() , and RETARGET_WriteChar() .
           
  | 
          static | 
Buffer to store data
        Definition at line
        
         69
        
        of file
        
         retargetserial.c
        
        .
       
Referenced by KSZ8851SNL_SPI_ReadRegister() , RETARGET_IRQ_NAME() , RETARGET_ReadChar() , SPIDRV_MTransferSingleItemB() , UARTDRV_Abort() , and UARTDRV_GetReceiveStatus() .
           
  | 
          static | 
Keeps track of how much data which are stored in the buffer
        Definition at line
        
         68
        
        of file
        
         retargetserial.c
        
        .
       
Referenced by _read() , RETARGET_IRQ_NAME() , and RETARGET_ReadChar() .
           
  | 
          static | 
Index in buffer to be read
        Definition at line
        
         66
        
        of file
        
         retargetserial.c
        
        .
       
Referenced by RETARGET_ReadChar() .
           
  | 
          static | 
Index in buffer to be written to
        Definition at line
        
         67
        
        of file
        
         retargetserial.c
        
        .
       
Referenced by RETARGET_IRQ_NAME() .