Plugin_Manager
Detailed Description
Plugin manager, see Plugin System Layer for detailed documentation.
.
Data Structures |
|
struct | EZRADIODRV_HandleData |
Macros |
|
#define | ECODE_EMDRV_EZRADIODRV_AUTO_ACK_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000400) |
Receive plugin base error code.
|
|
#define | ECODE_EMDRV_EZRADIODRV_CRC_ERROR_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000300) |
CRC error plugin base error code.
|
|
#define | ECODE_EMDRV_EZRADIODRV_DIRECT_RECEIVE_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000800) |
Receive plugin base error code.
|
|
#define | ECODE_EMDRV_EZRADIODRV_DIRECT_TRANSMIT_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000700) |
Transmit plugin base error code.
|
|
#define | ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000001) |
Illegal SPI handle.
|
|
#define | ECODE_EMDRV_EZRADIODRV_OK ( ECODE_OK ) |
Success return value.
|
|
#define | ECODE_EMDRV_EZRADIODRV_PN9_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000600) |
Receive plugin base error code.
|
|
#define | ECODE_EMDRV_EZRADIODRV_RECEIVE_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000200) |
Receive plugin base error code.
|
|
#define | ECODE_EMDRV_EZRADIODRV_TRANSMIT_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000100) |
Transmit plugin base error code.
|
|
#define | ECODE_EMDRV_EZRADIODRV_UNMOD_CARRIER_PLUGIN_BASE ( ECODE_EMDRV_EZRADIODRV_BASE | 0x00000500) |
Receive plugin base error code.
|
|
#define | EZRADIODRV_INIT_DEFAULT |
Configuration data for EzRadio plugin manager.
|
|
#define | RADIO_CONFIG_DATA_FIELD_LENGTH |
#define | RADIO_CONFIG_DATA_MAX_PACKET_LENGTH RADIO_CONFIG_DATA_FIELD1_LENGTH |
Typedefs |
|
typedef void(* | EZRADIODRV_Callback_t ) ( EZRADIODRV_Handle_t handle, Ecode_t status) |
EZRADIODRV feature callback function interface.
|
|
typedef EZRADIODRV_HandleData_t * | EZRADIODRV_Handle_t |
EZRadio driver instance handle.
|
|
typedef struct EZRADIODRV_HandleData | EZRADIODRV_HandleData_t |
Interface for
EZRADIODRV_HandleData
structure type defined below.
|
|
typedef ezradio_cmd_reply_t * | EZRADIODRV_ReplyHandle_t |
EZradio reply union handle.
|
|
Functions |
|
void | ezradioInit ( EZRADIODRV_Handle_t handle) |
Radio Initialization.
|
|
Ecode_t | ezradioPluginManager ( EZRADIODRV_Handle_t handle) |
EzRadio plugin manager state machine handler. This function should be called in the application in an infinite loop, in order to manage the EzRadio plug-ins properly.
|
|
void | ezradioResetTRxFifo (void) |
Resets both the TX and RX FIFOs.
|
|
Macro Definition Documentation
#define EZRADIODRV_INIT_DEFAULT |
Configuration data for EzRadio plugin manager.
Definition at line
334
of file
ezradio_plugin_manager.h
.
#define RADIO_CONFIG_DATA_FIELD_LENGTH |
Definition at line
139
of file
ezradio_plugin_manager.h
.
Typedef Documentation
typedef void(* EZRADIODRV_Callback_t) ( EZRADIODRV_Handle_t handle, Ecode_t status) |
EZRADIODRV feature callback function interface.
- Parameters
-
[in] handle
EZRadioDrv instance handler. [in] status
Callback status.
- Returns
- None
Definition at line
279
of file
ezradio_plugin_manager.h
.
Function Documentation
void ezradioInit | ( | EZRADIODRV_Handle_t |
handle
|
) |
Radio Initialization.
- Parameters
-
[in] handle
EzRadio driver instance handler.
Definition at line
78
of file
ezradio_plugin_manager.c
.
References EZRADIO_CONFIG_SUCCESS , ezradio_configuration_init() , ezradio_get_int_status() , ezradio_hal_GpioInit() , ezradio_hal_SpiInit() , USTIMER_DeInit() , USTIMER_Delay() , and USTIMER_Init() .
Ecode_t ezradioPluginManager | ( | EZRADIODRV_Handle_t |
radioHandle
|
) |
EzRadio plugin manager state machine handler. This function should be called in the application in an infinite loop, in order to manage the EzRadio plug-ins properly.
- Parameters
-
[in] radioHandle
EzRadio driver instance handler.
Definition at line
123
of file
ezradio_plugin_manager.c
.
References ECODE_EMDRV_EZRADIODRV_ILLEGAL_HANDLE , ECODE_EMDRV_EZRADIODRV_OK , and ezradio_get_int_status() .