Single conversion initialization structure.
       Definition at line
       
        963
       
       of file
       
        em_adc.h
       
       .
      
      
       #include <
       
     
        em_adc.h
       
       >
      
         Data Fields | 
       |
| ADC_AcqTime_TypeDef | acqTime | 
| bool | diff | 
| bool | fifoOverwrite | 
| bool | leftAdjust | 
| ADC_NegSel_TypeDef | negSel | 
| ADC_PosSel_TypeDef | posSel | 
| bool | prsEnable | 
| ADC_PRSSEL_TypeDef | prsSel | 
| ADC_Ref_TypeDef | reference | 
| bool | rep | 
| ADC_Res_TypeDef | resolution | 
| bool | singleDmaEm2Wu | 
Field Documentation
| ADC_AcqTime_TypeDef ADC_InitSingle_TypeDef::acqTime | 
Acquisition time (in ADC clock cycles).
        Definition at line
        
         971
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and adcInit() .
| bool ADC_InitSingle_TypeDef::diff | 
Select if single-ended or differential input.
        Definition at line
        
         1002
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitSingle() .
| bool ADC_InitSingle_TypeDef::fifoOverwrite | 
When true, FIFO overwrites old data when full. If false, FIFO discards new data. The SCANOF IRQ is triggered in both cases.
        Definition at line
        
         1021
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitSingle() .
| bool ADC_InitSingle_TypeDef::leftAdjust | 
Select if left adjustment should be done.
        Definition at line
        
         1008
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitSingle() .
| ADC_NegSel_TypeDef ADC_InitSingle_TypeDef::negSel | 
Select negative input for single channel conversion mode. Negative input is grounded for single-ended (non-differential) converison.
        Definition at line
        
         998
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitSingle() , and adcInit() .
| ADC_PosSel_TypeDef ADC_InitSingle_TypeDef::posSel | 
Select positive input for single channel conversion mode.
        Definition at line
        
         992
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitSingle() , and adcInit() .
| bool ADC_InitSingle_TypeDef::prsEnable | 
Peripheral reflex system trigger enable.
        Definition at line
        
         1005
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitSingle() , and adcInit() .
| ADC_PRSSEL_TypeDef ADC_InitSingle_TypeDef::prsSel | 
        Peripheral reflex system trigger selection. Only applicable if
        
         prsEnable
        
        is enabled.
       
        Definition at line
        
         968
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitSingle() , and adcInit() .
| ADC_Ref_TypeDef ADC_InitSingle_TypeDef::reference | 
Sample reference selection. Note that, for external references, the ADC calibration register must be set explicitly.
        Definition at line
        
         977
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , adcInit() , and TOUCH_Init() .
| bool ADC_InitSingle_TypeDef::rep | 
Select if continuous conversion until explicit stop.
        Definition at line
        
         1011
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitSingle() .
| ADC_Res_TypeDef ADC_InitSingle_TypeDef::resolution | 
Sample resolution.
        Definition at line
        
         980
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC0_IRQHandler() , ADC_InitSingle() , and TOUCH_Init() .
| bool ADC_InitSingle_TypeDef::singleDmaEm2Wu | 
When true, DMA is available in EM2 for single conversion
        Definition at line
        
         1015
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitSingle() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_adc.h