ADC initialization structure, common for single conversion and scan sequence.
Definition at line
782
of file
em_adc.h
.
#include <
em_adc.h
>
Data Fields |
|
ADC_EM2ClockConfig_TypeDef | em2ClockConfig |
ADC_OvsRateSel_TypeDef | ovsRateSel |
uint8_t | prescale |
bool | tailgate |
uint8_t | timebase |
ADC_Warmup_TypeDef | warmUpMode |
Field Documentation
ADC_EM2ClockConfig_TypeDef ADC_Init_TypeDef::em2ClockConfig |
ADC EM2 clock configuration
Definition at line
814
of file
em_adc.h
.
Referenced by ADC_Init() , and MIC_init() .
ADC_OvsRateSel_TypeDef ADC_Init_TypeDef::ovsRateSel |
Oversampling rate select. To have any effect, oversampling must be enabled for single/scan mode.
Definition at line
787
of file
em_adc.h
.
Referenced by ADC_Init() , and TOUCH_Init() .
uint8_t ADC_Init_TypeDef::prescale |
Clock division factor N, ADC clock = (HFPERCLK or HFPERCCLK) / (N + 1).
Definition at line
807
of file
em_adc.h
.
Referenced by ADC_Init() , adcInit() , MIC_init() , and TOUCH_Init() .
bool ADC_Init_TypeDef::tailgate |
Enable/disable conversion tailgating.
Definition at line
810
of file
em_adc.h
.
Referenced by ADC_Init() .
uint8_t ADC_Init_TypeDef::timebase |
Timebase for ADC warm up. Select N to give (N+1) HFPERCLK / HFPERCCLK cycles. (Additional delay is added for bandgap references. See the reference manual for more information.) Normally, N should be selected so that the timebase is at least 1 us. See ADC_TimebaseCalc() to obtain a suggested timebase of, at least, 1 us.
Definition at line
804
of file
em_adc.h
.
Referenced by ADC_Init() , adcInit() , and MIC_init() .
ADC_Warmup_TypeDef ADC_Init_TypeDef::warmUpMode |
The documentation for this struct was generated from the following file:
-
C:/HandsOn/super/platform/emlib/inc/
em_adc.h