__GLIB_Context_t Struct Reference
GLIB Drawing Context (Multiple instances of GLIB_Context_t can exist)
       Definition at line
       
        270
       
       of file
       
        glib.h
       
       .
      
      
       #include <
       
     
        glib.h
       
       >
      
         Data Fields | 
       |
| uint32_t | backgroundColor | 
| GLIB_Rectangle_t | clippingRegion | 
| GLIB_Font_t | font | 
| uint32_t | foregroundColor | 
| const DMD_DisplayGeometry * | pDisplayGeometry | 
Field Documentation
| uint32_t __GLIB_Context_t::backgroundColor | 
Background color
        Definition at line
        
         275
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_clear() , GLIB_clearRegion() , GLIB_contextInit() , and GLIB_drawChar() .
| GLIB_Rectangle_t __GLIB_Context_t::clippingRegion | 
Clipping rectangle
        Definition at line
        
         281
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_applyClippingRegion() , GLIB_clearRegion() , GLIB_clipLine() , GLIB_drawLineH() , GLIB_drawLineV() , GLIB_drawPixel() , GLIB_drawPixelColor() , GLIB_drawPixelRGB() , GLIB_drawPolygonFilled() , GLIB_drawRect() , GLIB_drawRectFilled() , GLIB_getClipCode() , GLIB_resetClippingRegion() , and GLIB_setClippingRegion() .
| GLIB_Font_t __GLIB_Context_t::font | 
Font definition
        Definition at line
        
         284
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_drawChar() , GLIB_drawString() , and GLIB_setFont() .
| uint32_t __GLIB_Context_t::foregroundColor | 
Foreground color
        Definition at line
        
         278
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_contextInit() , GLIB_drawLineH() , GLIB_drawLineV() , GLIB_drawPixel() , and GLIB_drawRectFilled() .
| const DMD_DisplayGeometry* __GLIB_Context_t::pDisplayGeometry | 
Pointer to the dimensions of the display
        Definition at line
        
         272
        
        of file
        
         glib.h
        
        .
       
Referenced by GLIB_clear() , GLIB_contextInit() , GLIB_resetClippingRegion() , GLIB_resetDisplayClippingArea() , and GLIB_setClippingRegion() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/middleware/glib/glib/
       
glib.h