nvm.c File Reference

Non-Volatile Memory Wear-Leveling driver API implementation.

License

Copyright 2018 Silicon Laboratories Inc. www.silabs.com

SPDX-License-Identifier: Zlib

The licensor of this software is Silicon Laboratories Inc.

This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.

Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:

  1. The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
  2. Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
  3. This notice may not be removed or altered from any source distribution.

Definition in file nvm.c .

#include <stdbool.h>
#include <stddef.h>
#include " nvm.h "

Functions

Ecode_t NVM_Erase (uint32_t eraseCount)
Erase the entire allocated NVM area.
Ecode_t NVM_Init (NVM_Config_t const *config)
Initialize the NVM manager.
Ecode_t NVM_Read (uint16_t pageId, uint8_t objectId)
Read an object or an entire page.
Ecode_t NVM_Write (uint16_t pageId, uint8_t objectId)
Write an object or a page.