BAP - Barometric Pressure Sensor
Detailed Description
Driver for the Bosch Sensortec BMP280 pressure sensor.
         Data Structures | 
       |
| struct | __BAP_Config | 
| 
         Structure to configure the BMP280 device.
          | 
       |
         Typedefs | 
       |
| typedef struct __BAP_Config | BAP_Config | 
| 
         Structure to configure the BMP280 device.
          | 
       |
         Functions | 
       |
| uint32_t | BAP_config ( BAP_Config *cfg) | 
| 
         Configure the barometric pressure sensor.
          | 
       |
| void | BAP_deInit (void) | 
| 
         De-initializes the barometric pressure module.
          | 
       |
| uint32_t | BAP_getPressure (float *pressure) | 
| 
         Initiates pressure measurement on the barometric pressure sensor and reads pressure from it.
          | 
       |
| uint32_t | BAP_getTemperature (float *temperature) | 
| 
         Initiates temperature measurement on the barometric pressure sensor and reads pressure from it.
          | 
       |
| uint32_t | BAP_init (uint8_t *deviceId) | 
| 
         Initializes the barometric pressure sensor chip.
          | 
       |
         Error Codes | 
       |
| #define | BAP_OK 0x0000 | 
| #define | BAP_ERROR_DRIVER_NOT_INITIALIZED 0x0001 | 
| #define | BAP_ERROR_I2C_TRANSACTION_FAILED 0x0002 | 
| #define | BAP_ERROR_DEVICE_ID_MISMATCH 0x0003 | 
Macro Definition Documentation
| #define BAP_ERROR_DEVICE_ID_MISMATCH 0x0003 | 
The device ID does not match the expected value
        Definition at line
        
         48
        
        of file
        
         bap.h
        
        .
       
Referenced by BAP_init() .
| #define BAP_ERROR_DRIVER_NOT_INITIALIZED 0x0001 | 
The driver is not initialized
        Definition at line
        
         46
        
        of file
        
         bap.h
        
        .
       
| #define BAP_ERROR_I2C_TRANSACTION_FAILED 0x0002 | 
I2C transaction failed
        Definition at line
        
         47
        
        of file
        
         bap.h
        
        .
       
| #define BAP_OK 0x0000 | 
No errors
        Definition at line
        
         45
        
        of file
        
         bap.h
        
        .
       
Referenced by BAP_getPressure() , BAP_getTemperature() , and BAP_init() .
Function Documentation
| uint32_t BAP_config | ( | BAP_Config * | 
           
            cfg
           
           | 
          ) | 
Configure the barometric pressure sensor.
- Parameters
 - 
         
[in] cfgStructure, which holds the configuration parameters  
- Returns
 - Returns zero on OK, non-zero otherwise
 
        Definition at line
        
         158
        
        of file
        
         bap.c
        
        .
       
References bmp280_set_power_mode() , bmp280_set_standby_durn() , bmp280_set_work_mode() , __BAP_Config::oversampling , __BAP_Config::powerMode , and __BAP_Config::standbyTime .
| void BAP_deInit | ( | void | 
           
           
           | 
          ) | 
De-initializes the barometric pressure module.
- Returns
 - None
 
        Definition at line
        
         138
        
        of file
        
         bap.c
        
        .
       
References bmp280_set_power_mode() , and BOARD_bapEnable() .
| uint32_t BAP_getPressure | ( | float * | 
           
            pressure
           
           | 
          ) | 
Initiates pressure measurement on the barometric pressure sensor and reads pressure from it.
- Parameters
 - 
         
[out] pressureThe measured pressure in millibars  
- Returns
 - Returns zero on OK, non-zero otherwise
 
        Definition at line
        
         218
        
        of file
        
         bap.c
        
        .
       
References BAP_OK , bmp280_compensate_pressure_int64() , bmp280_compensate_temperature_int32() , bmp280_get_forced_uncomp_pressure_temperature() , bmp280_read_uncomp_pressure() , and bmp280_read_uncomp_temperature() .
| uint32_t BAP_getTemperature | ( | float * | 
           
            temperature
           
           | 
          ) | 
Initiates temperature measurement on the barometric pressure sensor and reads pressure from it.
- Parameters
 - 
         
[out] temperatureThe measured temperature in degrees Celsius  
- Returns
 - Returns zero on OK, non-zero otherwise
 
        Definition at line
        
         183
        
        of file
        
         bap.c
        
        .
       
References BAP_OK , bmp280_compensate_temperature_int32() , bmp280_get_forced_uncomp_pressure_temperature() , and bmp280_read_uncomp_temperature() .
| uint32_t BAP_init | ( | uint8_t * | 
           
            deviceId
           
           | 
          ) | 
Initializes the barometric pressure sensor chip.
- Parameters
 - 
         
[out] deviceIdThe device ID of the connected chip  
- Returns
 - Returns zero on OK, non-zero otherwise
 
        Definition at line
        
         84
        
        of file
        
         bap.c
        
        .
       
References BAP_ERROR_DEVICE_ID_MISMATCH , BAP_OK , bmp280_init() , bmp280_set_power_mode() , bmp280_set_work_mode() , BOARD_bapEnable() , bmp280_t::delay_msec , bmp280_t::dev_addr , and UTIL_delay() .