__GLIB_Font_t Struct Reference

Font definition structure.

Definition at line 224 of file glib.h .

#include < glib.h >

Data Fields

uint8_t charSpacing
GLIB_Font_Class class
uint16_t cntOfMapElements
uint8_t fontHeight
uint8_t fontRowOffset
uint8_t fontWidth
uint8_t lineSpacing
void * pFontPixMap
uint8_t sizeOfMapElement

Field Documentation

uint8_t __GLIB_Font_t::charSpacing

Number of pixels between each character in this font.

Definition at line 247 of file glib.h .

Referenced by GLIB_drawChar() , and GLIB_drawString() .

GLIB_Font_Class __GLIB_Font_t::class

The font class is used to tell glib if the font contains numbers only or characters and numbers

Definition at line 251 of file glib.h .

Referenced by GLIB_drawChar() , and GLIB_drawString() .

uint16_t __GLIB_Font_t::cntOfMapElements

Number of elements in the font pixel map.

Definition at line 229 of file glib.h .

Referenced by GLIB_drawChar() .

uint8_t __GLIB_Font_t::fontHeight

Height in pixels of each character.

Definition at line 241 of file glib.h .

Referenced by GLIB_drawChar() , and GLIB_drawString() .

uint8_t __GLIB_Font_t::fontRowOffset

Font row offset.

Definition at line 235 of file glib.h .

Referenced by GLIB_drawChar() .

uint8_t __GLIB_Font_t::fontWidth

Width in pixels of each character.

Definition at line 238 of file glib.h .

Referenced by GLIB_drawChar() , and GLIB_drawString() .

uint8_t __GLIB_Font_t::lineSpacing

Number of pixels between each line in this font.

Definition at line 244 of file glib.h .

Referenced by GLIB_drawString() .

void* __GLIB_Font_t::pFontPixMap

Pointer to the pixel map for the font.

Definition at line 226 of file glib.h .

Referenced by GLIB_drawChar() .

uint8_t __GLIB_Font_t::sizeOfMapElement

Size of each element in the font pixel map.

Definition at line 232 of file glib.h .

Referenced by GLIB_drawChar() .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/middleware/glib/glib/ glib.h