USART PRS trigger enable.
       Definition at line
       
        334
       
       of file
       
        em_usart.h
       
       .
      
      
       #include <
       
     
        em_usart.h
       
       >
      
         Data Fields | 
       |
| bool | autoTxTriggerEnable | 
| USART_PRS_Channel_t | prsTriggerChannel | 
| bool | rxTriggerEnable | 
| bool | txTriggerEnable | 
Field Documentation
| bool USART_PrsTriggerInit_TypeDef::autoTxTriggerEnable | 
| USART_PRS_Channel_t USART_PrsTriggerInit_TypeDef::prsTriggerChannel | 
PRS channel to be used to trigger auto transmission.
        Definition at line
        
         344
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitPrsTrigger() .
| bool USART_PrsTriggerInit_TypeDef::rxTriggerEnable | 
Trigger receive via PRS channel.
        Definition at line
        
         340
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitPrsTrigger() .
| bool USART_PrsTriggerInit_TypeDef::txTriggerEnable | 
Trigger transmit via PRS channel.
        Definition at line
        
         342
        
        of file
        
         em_usart.h
        
        .
       
Referenced by USART_InitPrsTrigger() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_usart.h