ARING_TypeDef Struct Reference

Defines segment COM and BIT fields for A-wheel (suited for Anim)

Definition at line 120 of file segmentlcd.c .

Data Fields

uint8_t bit [8]
uint8_t com [8]

Field Documentation

uint8_t ARING_TypeDef::bit[8]

LCD bit number

Definition at line 122 of file segmentlcd.c .

uint8_t ARING_TypeDef::com[8]

LCD COM line (for multiplexing)

Definition at line 121 of file segmentlcd.c .


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/hardware/kit/common/drivers/ segmentlcd.c