Scan sequence initialization structure.
       Definition at line
       
        863
       
       of file
       
        em_adc.h
       
       .
      
      
       #include <
       
     
        em_adc.h
       
       >
      
         Data Fields | 
       |
| ADC_AcqTime_TypeDef | acqTime | 
| bool | diff | 
| bool | fifoOverwrite | 
| bool | leftAdjust | 
| bool | prsEnable | 
| ADC_PRSSEL_TypeDef | prsSel | 
| ADC_Ref_TypeDef | reference | 
| bool | rep | 
| ADC_Res_TypeDef | resolution | 
| bool | scanDmaEm2Wu | 
| ADC_InitScanInput_TypeDef | scanInputConfig | 
Field Documentation
| ADC_AcqTime_TypeDef ADC_InitScan_TypeDef::acqTime | 
Acquisition time (in ADC clock cycles).
        Definition at line
        
         871
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() .
| bool ADC_InitScan_TypeDef::diff | 
Select if single-ended or differential input.
        Definition at line
        
         901
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() , ADC_ScanDifferentialInputAdd() , and ADC_ScanSingleEndedInputAdd() .
| bool ADC_InitScan_TypeDef::fifoOverwrite | 
When true, FIFO overwrites old data when full. If false, FIFO discards new data. The SINGLEOF IRQ is triggered in both cases.
        Definition at line
        
         920
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() .
| bool ADC_InitScan_TypeDef::leftAdjust | 
Select if left adjustment should be done.
        Definition at line
        
         907
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() .
| bool ADC_InitScan_TypeDef::prsEnable | 
Peripheral reflex system trigger enable.
        Definition at line
        
         904
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() , and MIC_init() .
| ADC_PRSSEL_TypeDef ADC_InitScan_TypeDef::prsSel | 
        Peripheral reflex system trigger selection. Only applicable if
        
         prsEnable
        
        is enabled.
       
        Definition at line
        
         868
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() , and MIC_init() .
| ADC_Ref_TypeDef ADC_InitScan_TypeDef::reference | 
Sample reference selection. Note that, for external references, the ADC calibration register must be set explicitly.
        Definition at line
        
         877
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() , and MIC_init() .
| bool ADC_InitScan_TypeDef::rep | 
Select if continuous conversion until explicit stop.
        Definition at line
        
         910
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() .
| ADC_Res_TypeDef ADC_InitScan_TypeDef::resolution | 
| bool ADC_InitScan_TypeDef::scanDmaEm2Wu | 
When true, DMA is available in EM2 for scan conversion
        Definition at line
        
         914
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() , and MIC_init() .
| ADC_InitScanInput_TypeDef ADC_InitScan_TypeDef::scanInputConfig | 
Scan input configuration. Use ADC_ScanInputClear() , ADC_ScanSingleEndedInputAdd() or ADC_ScanDifferentialInputAdd() to update this structure.
        Definition at line
        
         897
        
        of file
        
         em_adc.h
        
        .
       
Referenced by ADC_InitScan() , ADC_ScanDifferentialInputAdd() , ADC_ScanInputClear() , and ADC_ScanSingleEndedInputAdd() .
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/platform/emlib/inc/
       
em_adc.h