EM_TypeDef Struct Reference
Defines segment COM and BIT fields for Energy Modes on display.
       Definition at line
       
        112
       
       of file
       
        segmentlcd.c
       
       .
      
         Data Fields | 
       |
| uint8_t | bit [5] | 
| uint8_t | com [5] | 
Field Documentation
| uint8_t EM_TypeDef::bit[5] | 
LCD bit number
        Definition at line
        
         114
        
        of file
        
         segmentlcd.c
        
        .
       
| uint8_t EM_TypeDef::com[5] | 
LCD COM line (for multiplexing)
        Definition at line
        
         113
        
        of file
        
         segmentlcd.c
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/HandsOn/super/hardware/kit/common/drivers/
       
segmentlcd.c