retargettft.c File Reference
Provide stdio retargeting to TFT address mapped mode.
License
Copyright 2018 Silicon Laboratories Inc. www.silabs.com
SPDX-License-Identifier: Zlib
The licensor of this software is Silicon Laboratories Inc.
This software is provided 'as-is', without any express or implied warranty. In no event will the authors be held liable for any damages arising from the use of this software.
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
- The origin of this software must not be misrepresented; you must not claim that you wrote the original software. If you use this software in a product, an acknowledgment in the product documentation would be appreciated but is not required.
 - Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
 - This notice may not be removed or altered from any source distribution.
 
       Definition in file
       
        retargettft.c
       
       .
      
       #include <stdio.h>
      
      
       #include <stdint.h>
      
      
       #include "em_device.h"
      
      
       #include "
       
        em_cmu.h
       
       "
      
      
       #include "
       
        em_ebi.h
       
       "
      
      
       #include "
       
        em_gpio.h
       
       "
      
      
       #include "dmd/ssd2119/dmd_ssd2119.h"
      
      
       #include "
       
        bsp.h
       
       "
      
      
       #include "
       
        retargettft.h
       
       "
      
      
       #include "
       
        displayfont8x8.h
       
       "
      
      
         Macros | 
       |
| #define | CHARS 40 | 
| #define | fontBits chars_8x8_bits | 
| #define | LINES 30 | 
         Functions | 
       |
| int | RETARGET_ReadChar (void) | 
| 
         Receive a byte No input method from TFT is possible, thus we always return -1.
          | 
       |
| void | RETARGET_TftCrLf (int on) | 
| 
         Toggle LF to CRLF conversion.
          | 
       |
| void | RETARGET_TftInit (void) | 
| 
         Intializes TFT text display.
          | 
       |
| void | RETARGET_TFTTX (int c) | 
| 
         Transmit/display a character.
          | 
       |
| void | RETARGET_TFTUpdate (bool fullFrame) | 
| 
         Display framebuffer.
          | 
       |
| int | RETARGET_WriteChar (char c) | 
| 
         Transmit single byte to the TFT.
          | 
       |
| static void | tftTextReset (void) | 
| 
         Reset TFT text display state.
          | 
       |
| static void | tftTextScrollUp (void) | 
| 
         Scroll one line of characters up on the screen.
          | 
       |
         Variables | 
       |
| static bool | bufferReset = true | 
| static uint8_t | charBuffer [ LINES ][ CHARS ] | 
| static bool | fullUpdate = true | 
| static bool | initialized = false | 
| static bool | LFtoCRLF = 0 | 
| static uint8_t | rgbColor [3] | 
| static bool | tftReset = true | 
| static int | xpos | 
| static int | ypos | 
Macro Definition Documentation
| #define CHARS 40 | 
Characters
        Definition at line
        
         44
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .
| #define fontBits chars_8x8_bits | 
| #define LINES 30 | 
Lines
        Definition at line
        
         45
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .
Function Documentation
| int RETARGET_ReadChar | ( | void | 
           
           
           | 
          ) | 
Receive a byte No input method from TFT is possible, thus we always return -1.
- Returns
 - -1 on failure, or positive character integer on sucesss
 
        Definition at line
        
         364
        
        of file
        
         retargettft.c
        
        .
       
| int RETARGET_WriteChar | ( | char | 
           
            c
           
           | 
          ) | 
Transmit single byte to the TFT.
- Parameters
 - 
         
cCharacter to transmit  
- Returns
 - Transmitted character
 
        Definition at line
        
         374
        
        of file
        
         retargettft.c
        
        .
       
References BC_ARB_CTRL_EBI , BC_REGISTER , BC_UIF_AEM_EFM , BSP_RegisterRead() , bufferReset , fullUpdate , initialized , LFtoCRLF , RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftReset , and tftTextReset() .
Variable Documentation
           
  | 
          static | 
Reset buffer
        Definition at line
        
         54
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_WriteChar() , and tftTextReset() .
Character buffer
        Definition at line
        
         47
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .
           
  | 
          static | 
Display updated
        Definition at line
        
         53
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_WriteChar() , and tftTextScrollUp() .
           
  | 
          static | 
Intialize TFT stdio retarget
        Definition at line
        
         57
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_WriteChar() , and tftTextReset() .
           
  | 
          static | 
LF to CRLF conversion disabled
        Definition at line
        
         56
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_TftCrLf() , and RETARGET_WriteChar() .
           
  | 
          static | 
Color for font
        Definition at line
        
         48
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , and tftTextReset() .
           
  | 
          static | 
Reset TFT
        Definition at line
        
         55
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_WriteChar() , and tftTextReset() .
           
  | 
          static | 
Cursor position
        Definition at line
        
         51
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .
           
  | 
          static | 
Cursor position
        Definition at line
        
         51
        
        of file
        
         retargettft.c
        
        .
       
Referenced by RETARGET_TFTTX() , RETARGET_TFTUpdate() , tftTextReset() , and tftTextScrollUp() .