More generic structure containing information about piecewise linear curves and mapping tables, instead of specific PA's.

DeprecatedThis RAIL 2.x type has been replaced in RAIL 3 by sl_rail_tx_power_table_config_t with different fields.

Public Attributes#

The curves for each PA.

uint32_t

Signature used for validation of the curves configuruation.

uint16_t

PA VDD voltage, in millivolts.

Public Attribute Documentation#

curves#

RAIL_PaDescriptor_t RAIL_TxPowerCurvesConfigAlt_t::curves[RAIL_NUM_PA]

The curves for each PA.

DeprecatedThis RAIL 2.x field has been replaced in RAIL 3 by other sl_rail_tx_power_table_config_t fields.


signature#

uint32_t RAIL_TxPowerCurvesConfigAlt_t::signature

Signature used for validation of the curves configuruation.

DeprecatedThis RAIL 2.x field has been replaced in RAIL 3 by sl_rail_tx_power_table_config_t::signature.


paVoltage#

uint16_t RAIL_TxPowerCurvesConfigAlt_t::paVoltage

PA VDD voltage, in millivolts.

DeprecatedThis RAIL 2.x field has been replaced in RAIL 3 by sl_rail_tx_power_table_config_t::pa_voltage_mv .