Data Management#

Data management functions.

These functions allow the application to choose how data is presented to the application. RAIL provides data in a packet-based method or in a FIFO-based method. As originally conceived, RAIL_DataMethod_t::PACKET_MODE was designed for handling packets that fit within RAIL's FIFOs while RAIL_DataMethod_t::FIFO_MODE was designed for handling packets larger than RAIL's FIFOs could hold. Conceptually it is still useful to think of these modes this way, but functionally their distinction has become blurred by improvements in RAIL's flexibility – applications now have much more control over both receive and transmit FIFO sizes, and the FIFO-management and threshold APIs and related events are no longer restricted to RAIL_DataMethod_t::FIFO_MODE operation but can be used in RAIL_DataMethod_t::PACKET_MODE too.

The application can configure RAIL data management through RAIL_ConfigData(). This function allows the application to specify the type of radio data (RAIL_TxDataSource_t and RAIL_RxDataSource_t) and the method of interacting with data (RAIL_DataMethod_t). By default, RAIL configures TX and RX both with packet data source and RAIL_DataMethod_t::PACKET_MODE.

For transmit, RAIL_DataMethod_t::PACKET_MODE and RAIL_DataMethod_t::FIFO_MODE are functionally the same:

The transmit FIFO is specified by the application and its size is the value returned from the most recent call to RAIL_SetTxFifo(). The transmit FIFO is edge-based in that it only provides the RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event once when the threshold is crossed in the emptying direction.

On EFR32xG25 platforms, the transmit FIFO must contain at least two bytes before starting a transmit. For OFDM and SUN OQPSK modulations, it must contain at least the PHY header (PHR) and first two payload bytes. When actively transmitting, loading data must be done by chunks of at least two bytes, except for the last one.

For receive, the distinction between RAIL_DataMethod_t::PACKET_MODE and RAIL_DataMethod_t::FIFO_MODE basically boils down to how unsuccessfully-received packets are handled. In RAIL_DataMethod_t::PACKET_MODE, data from such packets is automatically rolled back as if the packet was never received, while in RAIL_DataMethod_t::FIFO_MODE, rollback does not occur putting more onus on the application to deal with that data.

In receive RAIL_DataMethod_t::PACKET_MODE data management:

In receive RAIL_DataMethod_t::FIFO_MODE data management:

  • Packet Lengths are determined from the Radio Configurator configuration or by application knowledge of packet payload structure.

  • Received data can be retrieved prior to packet completion through RAIL_ReadRxFifo() and is never rolled back on FILTERED, ABORTED, or FRAMEERROR packets. The application should enable and handle these events so it can flush any packet data it's already retrieved.

  • After packet completion, remaining packet data for FILTERED, ABORTED, or FRAMEERROR packets remains in the FIFO and the appropriate event is triggered to the user. This data may be consumed in the callback unlike in packet mode where it is automatically rolled back. At the end of the callback all remaining data in the FIFO will be cleaned up as usual. Keep in mind that RAIL_GetRxPacketDetailsAlt() provides full packet detailed information only for successfully received packets.

Common receive data management features:

When trying to determine an appropriate threshold, the application needs to know the size of each FIFO. The default receive FIFO is internal to RAIL with a size of 512 bytes. This can be changed, however, using RAIL_SetRxFifo() and the default may be removed entirely by calling this from the RAILCb_SetupRxFifo() callback. The receive FIFO event is level-based in that the RAIL_EVENT_RX_FIFO_ALMOST_FULL event will constantly pend if the threshold is exceeded. This normally means that inside this event's callback, the application should empty enough of the FIFO to go under the threshold. To defer reading the FIFO to main context, the application can disable or re-enable the receive FIFO threshold event using RAIL_ConfigEvents() with the mask RAIL_EVENT_RX_FIFO_ALMOST_FULL.

The receive FIFO can store multiple packets and processing of a packet can be deferred from the RAIL event callback to main-loop processing by using RAIL_HoldRxPacket() in the event callback and RAIL_ReleaseRxPacket() in the main-loop. On some platforms, the receive FIFO is supplemented by an internal fixed-size packet metadata FIFO that limits the number of packets RAIL and applications can hold onto for deferred processing. See chip-specific documentation, such as EFR32, for more information.

Note

  • When using multiprotocol the receive FIFO is reset prior to a protocol switch so held packets will be lost if not processed before then.

While RAIL_EVENT_RX_FIFO_ALMOST_FULL occurs solely based on the state of the receive FIFO used for packet data, both RAIL_EVENT_RX_FIFO_FULL and RAIL_EVENT_RX_FIFO_OVERFLOW can occur coincident with packet completion when either that or the internal packet metadata FIFO fills or overflows. RAIL_EVENT_RX_FIFO_FULL informs the application it should immediately process and free up the oldest packets/data to make room for new packets/data, reducing the possibility of packet/data loss and RAIL_EVENT_RX_FIFO_OVERFLOW.

Before a packet is fully received you can always use RAIL_PeekRxPacket() to look at the contents. In FIFO mode, you may also consume its data with RAIL_ReadRxFifo(). Remember that none of these APIs will read across a packet boundary (even in FIFO mode) so you will need to handle each received packet individually.

While RAIL defaults to RAIL_DataMethod_t::PACKET_MODE, the application can explicitly initialize RAIL for RAIL_DataMethod_t::PACKET_MODE in the following manner:

extern RAIL_Handle_t railHandle;

void configRailForPacketModeOperation(void)
{
  RAIL_DataConfig_t railDataConfig = {
    .txSource = TX_PACKET_DATA,
    .rxSource = RX_PACKET_DATA,
    .txMethod = PACKET_MODE,
    .rxMethod = PACKET_MODE,
  };

  (void) RAIL_ConfigData(railHandle, &railDataConfig);

  // Events that can occur in Packet Mode:
  //   RAIL_EVENT_TX_PACKET_SENT
  //   RAIL_EVENT_RX_PACKET_RECEIVED
  // and optionally (packet data automatically dropped):
  //   RAIL_EVENT_RX_ADDRESS_FILTERED
  //   RAIL_EVENT_RX_PACKET_ABORTED
  //   RAIL_EVENT_RX_FRAME_ERROR
  //   RAIL_EVENT_RX_FIFO_OVERFLOW
  // and if enabled:
  //   RAIL_EVENT_TX_UNDERFLOW
  //   RAIL_EVENT_TXACK_UNDERFLOW
  //   RAIL_EVENT_TX_FIFO_ALMOST_EMPTY
  //   RAIL_EVENT_RX_FIFO_ALMOST_FULL
}

Initializing RAIL for RAIL_DataMethod_t::FIFO_MODE requires a few more function calls:

extern RAIL_Handle_t railHandle;

void config_rail_for_fifo_mode_operation(void)
{
  RAIL_DataConfig_t railDataConfig = {
    .txSource = TX_PACKET_DATA,
    .rxSource = RX_PACKET_DATA,
    .txMethod = FIFO_MODE,
    .rxMethod = FIFO_MODE,
  };

  (void) RAIL_ConfigData(railHandle, &railDataConfig);

  // Gets the size of the FIFOs.
  // Assume that the transmit and receive FIFOs are the same size
  uint16_t fifoSize = RAIL_GetTxFifoSpaceAvailable(railHandle);

  // Sets the transmit and receive FIFO thresholds.
  // For this example, set the threshold in the middle of each FIFO.
  (void) RAIL_SetRxFifoThreshold(railHandle, fifoSize / 2);
  (void) RAIL_SetTxFifoThreshold(railHandle, fifoSize / 2);

  // Events that can occur in FIFO mode:
  //   RAIL_EVENT_TX_FIFO_ALMOST_EMPTY
  //   RAIL_EVENT_TX_UNDERFLOW
  //   RAIL_EVENT_TXACK_UNDERFLOW
  //   RAIL_EVENT_TX_PACKET_SENT
  //   RAIL_EVENT_RX_FIFO_ALMOST_FULL
  //   RAIL_EVENT_RX_FIFO_OVERFLOW
  //   RAIL_EVENT_RX_ADDRESS_FILTERED
  //   RAIL_EVENT_RX_PACKET_ABORTED
  //   RAIL_EVENT_RX_FRAME_ERROR
  //   RAIL_EVENT_RX_PACKET_RECEIVED
}

On receive, an application can use a different RAIL_RxDataSource_t that is only compatible with RAIL_DataMethod_t::FIFO_MODE. All that differs from the FIFO mode example above is the RAIL_DataConfig_t::rxSource setting. IQ data samples are taken at the hardware's oversample rate and the amount of data can easily overwhelm the CPU processing time. The sample rate depends on the chosen PHY, as determined by the data rate and the decimation chain. It is not recommended to use the IQ data source with sample rates above 300 k samples/second because the CPU might not be able to keep up with the data stream. Depending on the application and the needed CPU bandwidth, slower data rates may be required. On EFR32xG22 and later platforms, it is recommended to reset the RX buffer before initiating a receive for all modes except RAIL_RxDataSource_t::RX_PACKET_DATA since these other modes require the RX buffer's current write offset to be 32-bit aligned. If not reset, capture is performed to the remaining aligned space available. An unaligned write offset will cause RAIL_ConfigData() to return error RAIL_STATUS_INVALID_STATE.

// Reset RX buffer (EFR32xG22 and later platforms)
RAIL_ResetFifo(railHandle, false, true);

// IQ data is provided into the receive FIFO.
RAIL_DataConfig_t railDataConfig = {
  .txSource = TX_PACKET_DATA,
  .rxSource = RX_IQDATA_FILTLSB,
  .txMethod = FIFO_MODE,
  .rxMethod = FIFO_MODE,
};

// IQ data comes in the following format when reading out of the FIFO:
//------------------------------------
// I[LSB] | I[MSB] | Q[LSB] | Q[MSB] |
//------------------------------------

These functions allow the application to choose how data is presented to the application. RAIL provides data in a packet-based method or in a FIFO-based method. As originally conceived, sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE was designed for handling packets that fit within RAIL's FIFOs while sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE was designed for handling packets larger than RAIL's FIFOs could hold. Conceptually it is still useful to think of these modes this way, but functionally their distinction has become blurred by improvements in RAIL's flexibility – applications now have much more control over both receive and transmit FIFO sizes, and the FIFO-management and threshold APIs and related events are no longer restricted to sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE operation but can be used in sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE too.

The application can configure RAIL data management through sl_rail_config_tx_data() and sl_rail_config_rx_data(). These functions allows the application to specify the type of radio data (sl_rail_tx_data_source_t and sl_rail_rx_data_source_t) and the method of interacting with data (sl_rail_data_method_t). By default, RAIL configures TX and RX both with packet data source and sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE.

For transmit, sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE and sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE are functionally the same:

The transmit FIFO is specified by the application and its size is the value returned from the most recent call to sl_rail_set_tx_fifo(). The transmit FIFO is edge-based in that it only provides the SL_RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event once when the threshold is crossed in the emptying direction.

On EFR32xG25 platforms, the transmit FIFO must contain at least two bytes before starting a transmit. For OFDM and SUN OQPSK modulations, it must contain at least the PHY header (PHR) and first two payload bytes. When actively transmitting, loading data must be done by chunks of at least two bytes, except for the last one.

For receive, the distinction between sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE and sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE basically boils down to how unsuccessfully-received packets are handled. In sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE, data from such packets is automatically rolled back as if the packet was never received, while in sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE, rollback does not occur putting more onus on the application to deal with that data.

In receive sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE data management:

In receive sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE data management:

  • Packet Lengths are determined from the Radio Configurator configuration or by application knowledge of packet payload structure.

  • Received data can be retrieved prior to packet completion through sl_rail_read_rx_fifo() and is never rolled back on FILTERED, ABORTED, or FRAMEERROR packets. The application should enable and handle these events so it can flush any packet data it's already retrieved.

  • After packet completion, remaining packet data for FILTERED, ABORTED, or FRAMEERROR packets remains in the FIFO and the appropriate event is triggered to the user. This data may be consumed in the callback unlike in packet mode where it is automatically rolled back. At the end of the callback all remaining data in the FIFO will be cleaned up as usual. Keep in mind that sl_rail_get_rx_packet_details() provides full packet detailed information only for successfully received packets.

Common receive data management features:

When trying to determine an appropriate threshold, the application needs to know the size of each FIFO. This can be obtained via sl_rail_get_config() if not already known. The receive FIFO event is level-based in that the SL_RAIL_EVENT_RX_FIFO_ALMOST_FULL event will constantly pend if the threshold is exceeded. This normally means that inside this event's callback, the application should empty enough of the FIFO to go under the threshold. To defer reading the FIFO to main context, the application can disable or re-enable the receive FIFO threshold event using sl_rail_config_events() with the mask SL_RAIL_EVENT_RX_FIFO_ALMOST_FULL.

The receive FIFO can store multiple packets and processing of a packet can be deferred from the RAIL event callback to main-loop processing by using sl_rail_hold_rx_packet() in the event callback and sl_rail_release_rx_packet() in the main-loop. The receive FIFO is supplemented by the receive Packet Queue that limits the number of packets RAIL and applications can hold onto for deferred processing.

Note

  • When using multiprotocol, if a protocol's receive FIFO or receive Packet Queue is shared with another protocol, they will be reset during a protocol switch so held packets will be lost if not processed before then.

While SL_RAIL_EVENT_RX_FIFO_ALMOST_FULL occurs solely based on the state of the receive FIFO used for packet data, both SL_RAIL_EVENT_RX_FIFO_FULL and SL_RAIL_EVENT_RX_FIFO_OVERFLOW can occur coincident with packet completion when either that or the receive Packet Queue fills or overflows. SL_RAIL_EVENT_RX_FIFO_FULL informs the application it should immediately process and free up the oldest packets/data to make room for new packets/data, reducing the possibility of packet/data loss and SL_RAIL_EVENT_RX_FIFO_OVERFLOW.

Before a packet is fully received you can always use sl_rail_peek_rx_packet() to look at the contents. In FIFO mode, you may also consume its data with sl_rail_read_rx_fifo(). Remember that none of these APIs will read across a packet boundary (even in FIFO mode) so you will need to handle each received packet individually.

While RAIL defaults to sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE, the application can explicitly initialize RAIL for sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE in the following manner:

extern sl_rail_handle_t rail_handle;

void config_rail_for_packet_mode_operation(void)
{
  sl_rail_tx_data_config_t rail_tx_data_config = {
    .tx_source = SL_RAIL_TX_DATA_SOURCE_PACKET_DATA,
    .tx_method = SL_RAIL_DATA_METHOD_PACKET_MODE,
  };
  sl_rail_rx_data_config_t rail_rx_data_config = {
    .rx_source = SL_RAIL_RX_DATA_SOURCE_PACKET_DATA,
    .rx_method = SL_RAIL_DATA_METHOD_PACKET_MODE,
  };

  (void) sl_rail_config_tx_data(rail_handle, &rail_tx_data_config);
  (void) sl_rail_config_rx_data(rail_handle, &rail_rx_data_config);

  // Events that can occur in Packet Mode:
  //   SL_RAIL_EVENT_TX_PACKET_SENT
  //   SL_RAIL_EVENT_RX_PACKET_RECEIVED
  // and optionally (packet data automatically dropped):
  //   SL_RAIL_EVENT_RX_ADDRESS_FILTERED
  //   SL_RAIL_EVENT_RX_PACKET_ABORTED
  //   SL_RAIL_EVENT_RX_FRAME_ERROR
  //   SL_RAIL_EVENT_RX_FIFO_OVERFLOW
  // and if enabled:
  //   SL_RAIL_EVENT_TX_UNDERFLOW
  //   SL_RAIL_EVENT_TXACK_UNDERFLOW
  //   SL_RAIL_EVENT_TX_FIFO_ALMOST_EMPTY
  //   SL_RAIL_EVENT_RX_FIFO_ALMOST_FULL
}

Initializing RAIL for sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE requires a few more function calls:

extern sl_rail_handle_t rail_handle;

void config_rail_for_fifo_mode_operation(void)
{
  sl_rail_tx_data_config_t rail_tx_data_config = {
    .tx_source = SL_RAIL_TX_DATA_SOURCE_PACKET_DATA,
    .tx_method = SL_RAIL_DATA_METHOD_FIFO_MODE,
  };
  sl_rail_rx_data_config_t rail_rx_data_config = {
    .rx_source = SL_RAIL_RX_DATA_SOURCE_PACKET_DATA,
    .rx_method = SL_RAIL_DATA_METHOD_FIFO_MODE,
  };

  (void) sl_rail_config_tx_data(rail_handle, &rail_tx_data_config);
  (void) sl_rail_config_rx_data(rail_handle, &rail_rx_data_config);

  // Gets the size of the FIFOs.
  // Assume that the transmit and receive FIFOs are the same size
  uint16_t fifo_size = sl_rail_get_tx_fifo_space_available(rail_handle);

  // Sets the transmit and receive FIFO thresholds.
  // For this example, set the threshold in the middle of each FIFO.
  (void) sl_rail_set_rx_fifo_threshold(rail_handle, fifo_size / 2);
  (void) sl_rail_set_tx_fifo_threshold(rail_handle, fifo_size / 2);

  // Events that can occur in FIFO mode:
  //   SL_RAIL_EVENT_TX_FIFO_ALMOST_EMPTY
  //   SL_RAIL_EVENT_TX_UNDERFLOW
  //   SL_RAIL_EVENT_TXACK_UNDERFLOW
  //   SL_RAIL_EVENT_TX_PACKET_SENT
  //   SL_RAIL_EVENT_RX_FIFO_ALMOST_FULL
  //   SL_RAIL_EVENT_RX_FIFO_OVERFLOW
  //   SL_RAIL_EVENT_RX_ADDRESS_FILTERED
  //   SL_RAIL_EVENT_RX_PACKET_ABORTED
  //   SL_RAIL_EVENT_RX_FRAME_ERROR
  //   SL_RAIL_EVENT_RX_PACKET_RECEIVED
}

On receive, an application can use a different sl_rail_rx_data_source_t that is only compatible with sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE. All that differs from the FIFO mode example above is the sl_rail_rx_data_config_t::rx_source setting. IQ data samples are taken at the hardware's oversample rate and the amount of data can easily overwhelm the CPU processing time. The sample rate depends on the chosen PHY, as determined by the data rate and the decimation chain. It is not recommended to use the IQ data source with sample rates above 300 k samples/second because the CPU might not be able to keep up with the data stream. Depending on the application and the needed CPU bandwidth, slower data rates may be required. On EFR32xG22 and later platforms, it is recommended to reset the RX buffer before initiating a receive for all modes except sl_rail_rx_data_source_t::SL_RAIL_RX_DATA_SOURCE_PACKET_DATA since these other modes require the RX buffer's current write offset to be 32-bit aligned. If not reset, capture is performed to the remaining aligned space available. An unaligned write offset will cause sl_rail_config_rx_data() to return error SL_RAIL_STATUS_INVALID_STATE.

// Reset RX buffer (EFR32xG22 and later platforms)
sl_rail_reset_fifo(rail_handle, false, true);

// IQ data is provided into the receive FIFO.
sl_rail_tx_data_config_t rail_tx_data_config = {
  .tx_source = SL_RAIL_TX_DATA_SOURCE_PACKET_DATA,
  .tx_method = SL_RAIL_DATA_METHOD_FIFO_MODE,
};
sl_rail_tx_data_config_t rail_tx_data_config = {
  .rx_source = SL_RAIL_RX_DATA_SOURCE_IQDATA_FILTLSB,
  .rx_method = SL_RAIL_DATA_METHOD_FIFO_MODE,
};

// IQ data comes in the following format when reading out of the FIFO:
//------------------------------------
// I[LSB] | I[MSB] | Q[LSB] | Q[MSB] |
//------------------------------------

Modules#

RAIL_DataConfig_t

sl_rail_tx_data_config_t

sl_rail_rx_data_config_t

Enumerations#

enum
TX_PACKET_DATA = 0
TX_MFM_DATA = 1
RAIL_TX_DATA_SOURCE_COUNT
}

Transmit data sources supported by RAIL.

enum
RX_PACKET_DATA = 0
RX_DEMOD_DATA = 1
RX_IQDATA_FILTLSB = 2
RX_IQDATA_FILTMSB = 3
RX_DIRECT_MODE_DATA = 4
RX_DIRECT_SYNCHRONOUS_MODE_DATA = 5
RAIL_RX_DATA_SOURCE_COUNT
}

Receive data sources supported by RAIL.

enum
PACKET_MODE = 0
FIFO_MODE = 1
RAIL_DATA_METHOD_COUNT
}

Methods for the application to provide and retrieve data from RAIL.

enum
SL_RAIL_TX_DATA_SOURCE_PACKET_DATA = 0u
SL_RAIL_TX_DATA_SOURCE_MFM_DATA = 1u
SL_RAIL_TX_DATA_SOURCE_COUNT
}

Transmit data sources supported by RAIL.

enum
SL_RAIL_RX_DATA_SOURCE_PACKET_DATA = 0u
SL_RAIL_RX_DATA_SOURCE_DEMOD_DATA = 1u
SL_RAIL_RX_DATA_SOURCE_IQDATA_FILTLSB = 2u
SL_RAIL_RX_DATA_SOURCE_IQDATA_FILTMSB = 3u
SL_RAIL_RX_DATA_SOURCE_DIRECT_MODE_DATA = 4u
SL_RAIL_RX_DATA_SOURCE_DIRECT_SYNCHRONOUS_MODE_DATA = 5u
SL_RAIL_RX_DATA_SOURCE_COUNT
}

Receive data sources supported by RAIL.

enum
SL_RAIL_DATA_METHOD_PACKET_MODE = 0
SL_RAIL_DATA_METHOD_FIFO_MODE = 1
SL_RAIL_DATA_METHOD_COUNT
}

Methods for the application to provide and retrieve data from RAIL.

Typedefs#

typedef uint32_t

Type indicating the needed alignment for RX and TX FIFOs.

typedef uint64_t

Type used for Packet Queue entries.

Variables#

const uint16_t

Run-time size in bytes of the built-in receive FIFO buffer to which sl_rail_builtin_rx_fifo_ptr points.

Pointer to built-in receive FIFO buffer that can be shared among built-in protocols on the same radio like RAIL 2.x provided internally.

const uint16_t

Run-time number of entries in the built-in receive Packet Queue to which sl_rail_builtin_rx_packet_queue_ptr points.

Pointer to built-in receive Packet queue that can be shared among built-in protocols on the same radio like RAIL 2.x provided internally.

Functions#

RAIL_ConfigData(RAIL_Handle_t railHandle, const RAIL_DataConfig_t *dataConfig)

RAIL data management configuration.

uint16_t
RAIL_WriteTxFifo(RAIL_Handle_t railHandle, const uint8_t *dataPtr, uint16_t writeLength, bool reset)

Write data to the transmit FIFO previously established by RAIL_SetTxFifo().

uint16_t
RAIL_SetTxFifo(RAIL_Handle_t railHandle, uint8_t *addr, uint16_t initLength, uint16_t size)

Set the address of the transmit FIFO, a circular buffer used for TX data, possibly pre-populated with transmit data.

uint16_t
RAIL_SetTxFifoAlt(RAIL_Handle_t railHandle, uint8_t *addr, uint16_t startOffset, uint16_t initLength, uint16_t size)

Set the address of the transmit FIFO, a circular buffer used for TX data which can start at offset distance from the FIFO base address.

RAIL_SetRxFifo(RAIL_Handle_t railHandle, uint8_t *addr, uint16_t *size)

Set the address of the receive FIFO, a circular buffer used for receive data.

RAILCb_SetupRxFifo(RAIL_Handle_t railHandle)

Set up the receive FIFO to use.

uint16_t
RAIL_ReadRxFifo(RAIL_Handle_t railHandle, uint8_t *dataPtr, uint16_t readLength)

Read packet data from RAIL's receive FIFO.

uint16_t
RAIL_SetTxFifoThreshold(RAIL_Handle_t railHandle, uint16_t txThreshold)

Configure the RAIL transmit FIFO almost empty threshold.

uint16_t
RAIL_SetRxFifoThreshold(RAIL_Handle_t railHandle, uint16_t rxThreshold)

Configure the RAIL receive FIFO almost full threshold.

uint16_t
RAIL_GetTxFifoThreshold(RAIL_Handle_t railHandle)

Get the RAIL transmit FIFO almost empty threshold value.

uint16_t
RAIL_GetRxFifoThreshold(RAIL_Handle_t railHandle)

Get the RAIL receive FIFO almost full threshold value.

RAIL_ResetFifo(RAIL_Handle_t railHandle, bool txFifo, bool rxFifo)

Reset the RAIL transmit and/or receive FIFOs.

uint16_t
RAIL_GetRxFifoBytesAvailable(RAIL_Handle_t railHandle)

Get the number of bytes used in the receive FIFO.

uint16_t
RAIL_GetTxFifoSpaceAvailable(RAIL_Handle_t railHandle)

Get the number of bytes unused in the transmit FIFO.

sl_rail_config_tx_data(sl_rail_handle_t rail_handle, const sl_rail_tx_data_config_t *p_tx_data_config)

RAIL TX data management configuration.

sl_rail_config_rx_data(sl_rail_handle_t rail_handle, const sl_rail_rx_data_config_t *p_rx_data_config)

RAIL RX data management configuration.

uint16_t
sl_rail_write_tx_fifo(sl_rail_handle_t rail_handle, const uint8_t *p_data, uint16_t write_bytes, bool reset)

Write data to the transmit FIFO previously established by sl_rail_set_tx_fifo().

sl_rail_set_tx_fifo(sl_rail_handle_t rail_handle, sl_rail_fifo_buffer_align_t *p_addr, uint16_t size_bytes, uint16_t init_bytes, uint16_t start_offset_bytes)

Set the address of the transmit FIFO, a circular buffer used for TX data, possibly pre-populated with transmit data.

sl_rail_set_rx_fifo(sl_rail_handle_t rail_handle, sl_rail_fifo_buffer_align_t *p_addr, uint16_t *p_size_bytes)

Set the address of the receive FIFO, a circular buffer used for receive data.

uint16_t
sl_rail_read_rx_fifo(sl_rail_handle_t rail_handle, uint8_t *p_data, uint16_t read_bytes)

Read packet data from RAIL's receive FIFO.

sl_rail_set_rx_packet_queue(sl_rail_handle_t rail_handle, sl_rail_packet_queue_entry_t *p_rx_packet_queue, uint16_t *p_entries)

Set the address of the receive Packet Queue, a circular buffer used by RAIL for received packet metadata that supplements the receive FIFO.

uint16_t
sl_rail_set_tx_fifo_threshold(sl_rail_handle_t rail_handle, uint16_t tx_threshold_bytes)

Configure the RAIL transmit FIFO almost empty threshold.

uint16_t
sl_rail_set_rx_fifo_threshold(sl_rail_handle_t rail_handle, uint16_t rx_threshold_bytes)

Configure the RAIL receive FIFO almost full threshold.

uint16_t
sl_rail_get_tx_fifo_threshold(sl_rail_handle_t rail_handle)

Get the RAIL transmit FIFO almost empty threshold value.

uint16_t
sl_rail_get_rx_fifo_threshold(sl_rail_handle_t rail_handle)

Get the RAIL receive FIFO almost full threshold value.

sl_rail_reset_fifo(sl_rail_handle_t rail_handle, bool tx_fifo, bool rx_fifo)

Reset the RAIL transmit and/or receive FIFOs.

uint16_t
sl_rail_get_rx_fifo_bytes_available(sl_rail_handle_t rail_handle)

Get the number of bytes used in the receive FIFO.

uint16_t
sl_rail_get_tx_fifo_space_available(sl_rail_handle_t rail_handle)

Get the number of bytes unused in the transmit FIFO.

Macros#

#define

Fixed-width type indicating the needed alignment for RX and TX FIFOs.

#define
RAIL_FIFO_ALIGNMENT (sizeof(RAIL_FIFO_ALIGNMENT_TYPE))

Alignment that is needed for the RX and TX FIFOs.

#define

A FIFO threshold value that disables the threshold.

#define

Compile-time size in bytes of the built-in receive FIFO buffer to which sl_rail_builtin_rx_fifo_ptr points.

#define

Compile-time number of entries in the built-in receive Packet Queue to which sl_rail_builtin_rx_packet_queue_ptr points.

#define
SL_RAIL_DECLARE_FIFO_BUFFER (buffer_name, bytes)

Convenience macro for declaring RAIL FIFO buffers of desired size.

#define

The minimum size in bytes of a receive / transmit / Auto-Ack FIFO.

#define

The maximum size in bytes of a receive / transmit / Auto-Ack FIFO.

#define

A FIFO threshold value that disables the threshold.

Enumeration Documentation#

RAIL_TxDataSource_t#

RAIL_TxDataSource_t

Transmit data sources supported by RAIL.

DeprecatedRAIL 2.x synonym of sl_rail_tx_data_source_t.

Enumerator
TX_PACKET_DATA

Uses the frame hardware to packetize data.

TX_MFM_DATA

Uses the multi-level frequency modulation data.

RAIL_TX_DATA_SOURCE_COUNT

A count of the choices in this enumeration.


RAIL_RxDataSource_t#

RAIL_RxDataSource_t

Receive data sources supported by RAIL.

Note

DeprecatedRAIL 2.x synonym of sl_rail_rx_data_source_t.

Enumerator
RX_PACKET_DATA

Uses the frame hardware to packetize data.

RX_DEMOD_DATA

Gets 8-bit data output from the demodulator.

RX_IQDATA_FILTLSB

Gets lower 16 bits of I/Q data provided to the demodulator.

RX_IQDATA_FILTMSB

Gets highest 16 bits of I/Q data provided to the demodulator.

RX_DIRECT_MODE_DATA

Gets RX direct mode data output from the demodulator.

RX_DIRECT_SYNCHRONOUS_MODE_DATA

Gets synchronous RX direct mode data output from the demodulator.

RAIL_RX_DATA_SOURCE_COUNT

A count of the choices in this enumeration.


RAIL_DataMethod_t#

RAIL_DataMethod_t

Methods for the application to provide and retrieve data from RAIL.

For Transmit the distinction between RAIL_DataMethod_t::PACKET_MODE and RAIL_DataMethod_t::FIFO_MODE has become more cosmetic than functional, as the RAIL_WriteTxFifo() and RAIL_SetTxFifoThreshold() APIs and related RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event can be used in either mode. For Receive the distinction is functionally important because in RAIL_DataMethod_t::PACKET_MODE rollback occurs automatically for unsuccessfully-received packets (RAIL_RxPacketStatus_t ABORT statuses), flushing their data. In RAIL_DataMethod_t::FIFO_MODE rollback is prevented, leaving the data from unsuccessfully-received packets in the receive FIFO for the application to deal with. This allows for packets larger than the receive FIFO size where automatic rollback would corrupt the receive FIFO.

DeprecatedRAIL 2.x synonym of sl_rail_data_method_t.

Enumerator
PACKET_MODE

Packet-based data method.

FIFO_MODE

FIFO-based data method.

RAIL_DATA_METHOD_COUNT

A count of the choices in this enumeration.


sl_rail_tx_data_source_t#

sl_rail_tx_data_source_t

Transmit data sources supported by RAIL.

Enumerator
SL_RAIL_TX_DATA_SOURCE_PACKET_DATA

Uses the frame hardware to packetize data.

SL_RAIL_TX_DATA_SOURCE_MFM_DATA

Uses the multi-level frequency modulation data.

SL_RAIL_TX_DATA_SOURCE_COUNT

A count of the choices in this enumeration.


sl_rail_rx_data_source_t#

sl_rail_rx_data_source_t

Receive data sources supported by RAIL.

Note

Enumerator
SL_RAIL_RX_DATA_SOURCE_PACKET_DATA

Uses the frame hardware to packetize data.

SL_RAIL_RX_DATA_SOURCE_DEMOD_DATA

Gets 8-bit data output from the demodulator.

SL_RAIL_RX_DATA_SOURCE_IQDATA_FILTLSB

Gets lower 16 bits of I/Q data provided to the demodulator.

SL_RAIL_RX_DATA_SOURCE_IQDATA_FILTMSB

Gets highest 16 bits of I/Q data provided to the demodulator.

SL_RAIL_RX_DATA_SOURCE_DIRECT_MODE_DATA

Gets RX direct mode data output from the demodulator.

SL_RAIL_RX_DATA_SOURCE_DIRECT_SYNCHRONOUS_MODE_DATA

Gets synchronous RX direct mode data output from the demodulator.

SL_RAIL_RX_DATA_SOURCE_COUNT

A count of the choices in this enumeration.


sl_rail_data_method_t#

sl_rail_data_method_t

Methods for the application to provide and retrieve data from RAIL.

For Transmit the distinction between sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE and sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE has become more cosmetic than functional, as the sl_rail_write_tx_fifo() and sl_rail_set_tx_fifo_threshold() APIs and related SL_RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event can be used in either mode. For Receive the distinction is functionally important because in sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE rollback occurs automatically for unsuccessfully-received packets (sl_rail_rx_packet_status_t ABORT statuses), flushing their data. In sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE rollback is prevented, leaving the data from unsuccessfully-received packets in the receive FIFO for the application to deal with. This allows for packets larger than the receive FIFO size where automatic rollback would corrupt the receive FIFO.

Enumerator
SL_RAIL_DATA_METHOD_PACKET_MODE

Packet-based data method.

SL_RAIL_DATA_METHOD_FIFO_MODE

FIFO-based data method.

SL_RAIL_DATA_METHOD_COUNT

A count of the choices in this enumeration.


Typedef Documentation#

sl_rail_fifo_buffer_align_t#

typedef uint32_t sl_rail_fifo_buffer_align_t

Type indicating the needed alignment for RX and TX FIFOs.


sl_rail_packet_queue_entry_t#

typedef uint64_t sl_rail_packet_queue_entry_t

Type used for Packet Queue entries.

RAIL utilizes a receive Packet Queue for packet reception metadata that supplements the receive FIFO, helping sl_rail_get_rx_packet_info() and sl_rail_get_rx_packet_details() provide their information in the order that packets were received.


Variable Documentation#

sl_rail_builtin_rx_fifo_bytes#

const uint16_t sl_rail_builtin_rx_fifo_bytes

Run-time size in bytes of the built-in receive FIFO buffer to which sl_rail_builtin_rx_fifo_ptr points.

Can be assigned to sl_rail_config_t::rx_fifo_bytes.


sl_rail_builtin_rx_fifo_ptr#

sl_rail_fifo_buffer_align_t* const sl_rail_builtin_rx_fifo_ptr

Pointer to built-in receive FIFO buffer that can be shared among built-in protocols on the same radio like RAIL 2.x provided internally.

Can be assigned to sl_rail_config_t::p_rx_fifo_buffer.


sl_rail_builtin_rx_packet_queue_entries#

const uint16_t sl_rail_builtin_rx_packet_queue_entries

Run-time number of entries in the built-in receive Packet Queue to which sl_rail_builtin_rx_packet_queue_ptr points.

Can be assigned to sl_rail_config_t::rx_packet_queue_entries.


sl_rail_builtin_rx_packet_queue_ptr#

sl_rail_packet_queue_entry_t* const sl_rail_builtin_rx_packet_queue_ptr

Pointer to built-in receive Packet queue that can be shared among built-in protocols on the same radio like RAIL 2.x provided internally.

Can be assigned to sl_rail_config_t::p_rx_packet_queue.


Function Documentation#

RAIL_ConfigData#

RAIL_Status_t RAIL_ConfigData (RAIL_Handle_t railHandle, const RAIL_DataConfig_t * dataConfig)

RAIL data management configuration.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

const RAIL_DataConfig_t *[in]dataConfig

A pointer to a non-NULL RAIL data configuration structure.

Returns

This function configures how RAIL manages data. The application can configure RAIL to receive data in a packet-based or FIFO-based manner. RAIL_DataMethod_t::FIFO_MODE is necessary to receive packets larger than the radio's receive FIFO. It is also required for receive data sources other than RAIL_RxDataSource_t::RX_PACKET_DATA.

Generally with RAIL_DataMethod_t::FIFO_MODE, the application sets appropriate FIFO thresholds via RAIL_SetTxFifoThreshold() and RAIL_SetRxFifoThreshold() and then enables and handles the RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event callback (to feed more packet data via RAIL_WriteTxFifo() before the FIFO underflows) and the RAIL_EVENT_RX_FIFO_ALMOST_FULL event callback (to consume packet data via RAIL_ReadRxFifo() before the receive FIFO overflows).

When configuring TX for RAIL_DataMethod_t::FIFO_MODE, this function resets the transmit FIFO. When configuring TX or RX for RAIL_DataMethod_t::PACKET_MODE, this function will reset the corresponding FIFO thresholds such that they won't trigger the RAIL_EVENT_RX_FIFO_ALMOST_FULL or RAIL_EVENT_TX_FIFO_ALMOST_EMPTY events.

When RAIL_DataConfig_t::rxMethod is set to RAIL_DataMethod_t::FIFO_MODE, the radio won't drop packet data of aborted or CRC error packets, but will present it to the application to deal with accordingly. On completion of erroneous packets, the RAIL_Config_t::eventsCallback() with RAIL_EVENT_RX_PACKET_ABORTED, RAIL_EVENT_RX_FRAME_ERROR, or RAIL_EVENT_RX_ADDRESS_FILTERED will tell the application it can drop any data it read via RAIL_ReadRxFifo() during reception. For CRC error packets when the RAIL_RX_OPTION_IGNORE_CRC_ERRORS RX option is in effect, the application should check for that from the RAIL_RxPacketStatus_t obtained by calling RAIL_GetRxPacketInfo(). RAIL will automatically flush any remaining packet data after reporting one of these packet completion events or the application can explicitly flush it by calling RAIL_ReleaseRxPacket().

When RAIL_DataConfig_t::rxMethod is set to RAIL_DataMethod_t::PACKET_MODE, the radio will roll back (drop) all packet data associated with aborted packets including those with CRC errors (unless configured to ignore CRC errors via the RAIL_RX_OPTION_IGNORE_CRC_ERRORS RX option). The application will never have to deal with packet data from these packets. In either mode, the application can set RX options as needed.

When RAIL_DataConfig_t::rxSource is set to a value other than RX_PACKET_DATA and RAIL_Config_t::eventsCallback()RAIL_EVENT_RX_FIFO_OVERFLOW is enabled RX will be terminated if a RX FIFO overflow occurs. If RAIL_EVENT_RX_FIFO_OVERFLOW is not enabled, data will be discarded until the overflow condition is resolved. To continue capturing data RX must be restarted using RAIL_StartRx().

DeprecatedThis RAIL 2.x function has been replaced in RAIL 3 by separate sl_rail_config_rx_data() and sl_rail_config_tx_data() functions.


RAIL_WriteTxFifo#

uint16_t RAIL_WriteTxFifo (RAIL_Handle_t railHandle, const uint8_t * dataPtr, uint16_t writeLength, bool reset)

Write data to the transmit FIFO previously established by RAIL_SetTxFifo().

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

const uint8_t *[in]dataPtr

A pointer to transmit data.

uint16_t[in]writeLength

A number of bytes to write to the transmit FIFO.

bool[in]reset

If true, resets transmit FIFO before writing the data.

Returns

  • The number of bytes written to the transmit FIFO.

This function copies writeLength bytes of data from the provided dataPtr into the transmit FIFO previously established by RAIL_SetTxFifo() or RAIL_Init(). If the requested writeLength exceeds the current number of bytes open in the transmit FIFO, the function only writes until the transmit FIFO is full. The function returns the number of bytes written to the transmit FIFO or returns zero if railHandle is NULL or if the transmit FIFO is full.

Note

  • The protocol's packet configuration, as set up by the radio configurator or via RAIL_SetFixedLength(), determines how many bytes of data are consumed from the transmit FIFO for a successful transmit operation, not the writeLength value passed in. If not enough data has been put into the transmit FIFO, a RAIL_EVENT_TX_UNDERFLOW event will occur. If too much data is put into the transmit FIFO, the extra data will either become the first bytes sent in a subsequent packet, or will be thrown away if the FIFO gets reset prior to the next transmit. In general, the proper number of packet bytes to put into the transmit FIFO are all payload bytes except for any CRC bytes, which the packet configuration causes to be sent automatically.

  • This function does not utilize a critical section but, depending on the application, calling it within a critical section could be appropriate.

DeprecatedRAIL 2.x synonym of sl_rail_write_tx_fifo().


RAIL_SetTxFifo#

uint16_t RAIL_SetTxFifo (RAIL_Handle_t railHandle, uint8_t * addr, uint16_t initLength, uint16_t size)

Set the address of the transmit FIFO, a circular buffer used for TX data, possibly pre-populated with transmit data.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint8_t *[inout]addr

An appropriately-aligned (see below) pointer to a read-write memory location in RAM used as the transmit FIFO. This memory must persist until the next call to this function or RAIL_SetTxFifoAlt.

uint16_t[in]initLength

A number of initial bytes already in the transmit FIFO.

uint16_t[in]size

A desired size of the transmit FIFO in bytes.

Returns

  • The transmit FIFO size in bytes, 0 if an error occurs.

This function sets the memory location for the transmit FIFO. RAIL_SetTxFifo or RAIL_SetTxFifoAlt must be called at least once before any transmit operations occur.

FIFO size can be determined by the return value of this function. The chosen size is determined based on the available FIFO sizes supported by the hardware. Similarly, some hardware has stricter FIFO alignment requirements; 32-bit alignment provides the maximum portability across all RAIL platforms. For more on supported FIFO sizes and alignments, see chip-specific documentation, such as EFR32. The returned FIFO size will be the closest allowed size less than or equal to the passed in size parameter, unless the size parameter is smaller than the minimum FIFO size, in that case 0 is returned. If the initLength parameter is larger than the returned size, the FIFO will be filled up to its size.

A user may write to the custom memory location directly before calling this function, or use RAIL_WriteTxFifo() to write to the memory location after calling this function. Users must specify the initLength for previously-written memory to be set in the transmit FIFO.

This function reserves the block of RAM starting at addr with a length of the returned FIFO size, which is used internally as a circular buffer for the transmit FIFO. It must be able to hold the entire FIFO size. The caller must guarantee that the custom FIFO remains intact and unchanged (except via calls to RAIL_WriteTxFifo()) until the next call to this function.

Note

  • The protocol's packet configuration, as set up by the radio configurator or via RAIL_SetFixedLength(), determines how many bytes of data are consumed from the transmit FIFO for a successful transmit operation, not the initLength value passed in. If not enough data has been put into the transmit FIFO, a RAIL_EVENT_TX_UNDERFLOW event will occur. If too much data is put into the transmit FIFO, the extra data will either become the first bytes sent in a subsequent packet, or will be thrown away if the FIFO gets reset prior to the next transmit. In general, the proper number of packet bytes to put into the transmit FIFO are all payload bytes except for any CRC bytes which the packet configuration causes to be sent automatically.

DeprecatedThis RAIL 2.x function has been replaced in RAIL 3 by sl_rail_set_tx_fifo() with additional parameters and permits establishing a non-power-of-2-sized Tx FIFO.


RAIL_SetTxFifoAlt#

uint16_t RAIL_SetTxFifoAlt (RAIL_Handle_t railHandle, uint8_t * addr, uint16_t startOffset, uint16_t initLength, uint16_t size)

Set the address of the transmit FIFO, a circular buffer used for TX data which can start at offset distance from the FIFO base address.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint8_t *[inout]addr

An appropriately-aligned (see RAIL_SetTxFifo description) pointer to a read-write memory location in RAM used as the transmit FIFO. This memory must persist until the next call to this function or RAIL_SetTxFifo.

uint16_t[in]startOffset

A number of bytes defining the start position of the TX data from the transmit FIFO base address, only valid if initLength is not 0.

uint16_t[in]initLength

The number of valid bytes already in the transmit FIFO after startOffset.

uint16_t[in]size

A desired size of the transmit FIFO in bytes.

Returns

  • The transmit FIFO size in bytes, 0 if an error occurs.

This function is similar to RAIL_SetTxFifo except a startOffset can be specified to indicate where the transmit packet data starts. This allows an application to place unaligned initial packet data within the aligned transmit FIFO (initLength > 0). Specifying a startOffset will not reduce the FIFO threshold or affect RAIL_GetTxFifoSpaceAvailable(). RAIL_SetTxFifo or RAIL_SetTxFifoAlt must be called at least once before any transmit operations occur. FIFO size handling is quite same as RAIL_SetTxFifo. Only difference is that if the initLength plus startOffset parameters are larger than the returned size, the FIFO will be filled up to its size from startOffset. Note that the startOffset is essentially forgotten after the next transmit – i.e. it applies onto to the next transmit operation, and is not re-established when the transmit FIFO is reset.

DeprecatedThis RAIL 2.x function has been replaced in RAIL 3 by sl_rail_set_tx_fifo() with parameters in a different order and permits establishing a non-power-of-2-sized Tx FIFO.


RAIL_SetRxFifo#

RAIL_Status_t RAIL_SetRxFifo (RAIL_Handle_t railHandle, uint8_t * addr, uint16_t * size)

Set the address of the receive FIFO, a circular buffer used for receive data.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint8_t *[inout]addr

A pointer to a read-write memory location in RAM used as the receive FIFO. This memory must persist until the next call to this function.

uint16_t *[inout]size

A pointer to the desired size of the receive FIFO in bytes. This will be updated with the actual size during the function call.

Returns

  • Status code indicating success of the function call.

This function sets the memory location for the receive FIFO. It must be called at least once before any receive operations occur.

Note

  • After it is called, any prior receive FIFO is orphaned. To avoid orphaning the default internal 512-byte receive FIFO so it does not unnecessarily consume RAM resources in your application, implement RAILCb_SetupRxFifo() to call this function.

FIFO size can be determined by the return value of this function. The chosen size is determined based on the available FIFO sizes supported by the hardware. Similarly, some hardware has stricter FIFO alignment requirements; 32-bit alignment provides the maximum portability across all RAIL platforms. For more on supported FIFO sizes and alignments, see chip-specific documentation, such as EFR32. The returned FIFO size will be the closest allowed size less than or equal to the passed in size parameter, unless the size parameter is smaller than the minimum FIFO size.

This function reserves the block of RAM starting at addr with a length of size, which is used internally as a circular buffer for the receive FIFO. It must be able to hold the entire FIFO size. The caller must guarantee that the custom FIFO remains intact and unchanged (except via incoming packet data being written) until the next call to this function.

In multiprotocol, RAIL currently shares one receive FIFO across all protocols. This function will return RAIL_STATUS_INVALID_STATE if the requested RAIL_Handle_t is not active.

DeprecatedRAIL 2.x synonym of sl_rail_set_rx_fifo(). Also see sl_rail_set_rx_packet_queue(). Unlike in RAIL 2.x where the Rx FIFO and internal Packet Queue are shared among all protocols, those RAIL 3 APIs allow a protocol to establish, even when inactive, its own Rx FIFO and Packet Queue independent of other protocols' which are preserved and not reset during protocol switches.


RAILCb_SetupRxFifo#

RAIL_Status_t RAILCb_SetupRxFifo (RAIL_Handle_t railHandle)

Set up the receive FIFO to use.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

This function is optional to implement.

Returns

  • Status code indicating success of the function call.

This callback is called during the RAIL_Init() process to set up the FIFO to use for received packets. If not implemented by the application, a default implementation from within the RAIL library will be used to initialize an internal default 512-byte receive FIFO.

If this function returns an error, the RAIL_Init() process will fail.

During this function, the application should generally call RAIL_SetRxFifo(). If that does not happen, the application needs to set up the receive FIFO via a call to RAIL_SetRxFifo() before attempting to receive any packets. An example implementation may look like the following:

#define RX_FIFO_BYTES 1024
static __ALIGNED(RAIL_FIFO_ALIGNMENT) uint8_t rxFifo[RX_FIFO_BYTES];

RAIL_Status_t RAILCb_SetupRxFifo(RAIL_Handle_t railHandle)
{
  uint16_t rxFifoBytes = RX_FIFO_BYTES;
  RAIL_Status_t status = RAIL_SetRxFifo(railHandle, &rxFifo[0], &rxFifoBytes);
  if (rxFifoBytes != RX_FIFO_BYTES) {
    // We set up an incorrect FIFO size
    return RAIL_STATUS_INVALID_PARAMETER;
  }
  if (status == RAIL_STATUS_INVALID_STATE) {
    // Allow failures due to multiprotocol
    return RAIL_STATUS_NO_ERROR;
  }
  return status;
}

DeprecatedThis RAIL 2.x callback has been eliminated in RAIL 3. The Rx FIFO (and Packet Queue) can be configured in the sl_rail_config_t passed into sl_rail_init(), or later via sl_rail_set_rx_fifo() and/or sl_rail_set_rx_packet_queue(). Unlike in RAIL 2.x where the Rx FIFO and internal Packet Queue are shared among all protocols, those RAIL 3 APIs allow a protocol to establish, even when inactive, its own Rx FIFO and Packet Queue independent of other protocols' which are preserved and not reset during protocol switches.


RAIL_ReadRxFifo#

uint16_t RAIL_ReadRxFifo (RAIL_Handle_t railHandle, uint8_t * dataPtr, uint16_t readLength)

Read packet data from RAIL's receive FIFO.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint8_t *[out]dataPtr

An application-provided pointer to store data. If NULL, the data is thrown away rather than copied out.

uint16_t[in]readLength

A number of packet bytes to read from the FIFO.

Returns

  • The number of packet bytes read from the receive FIFO.

This function reads packet data from the head of receive FIFO and writes it to the provided dataPtr. It does not permit reading more data than is available in the FIFO, nor does it permit reading more data than remains in the oldest unreleased packet.

Because this function does not have a critical section, use it only in one context or make sure function calls are protected to prevent buffer corruption.

Warnings

Note

  • When reading data from an arriving packet that is not yet complete, keep in mind its data is highly suspect because it has not yet passed any CRC integrity checking. Also note that the packet could be aborted, canceled, or fail momentarily, invalidating its data in Packet mode. Furthermore, there is a small chance towards the end of packet reception that the receive FIFO could include not only packet data received so far, but also some raw radio-appended info detail bytes that RAIL's packet-completion processing will subsequently deal with. It's up to the application to know its packet format well enough to know where a packet's payload ends and not interpret appended info as payload data coming from over the air.

DeprecatedRAIL 2.x synonym of sl_rail_read_rx_fifo().


RAIL_SetTxFifoThreshold#

uint16_t RAIL_SetTxFifoThreshold (RAIL_Handle_t railHandle, uint16_t txThreshold)

Configure the RAIL transmit FIFO almost empty threshold.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint16_t[in]txThreshold

The threshold below which the RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event will fire.

Returns

  • Configured transmit FIFO threshold value.

This function configures the threshold for the transmit FIFO. When the number of bytes in the transmit FIFO falls below the configured threshold, RAIL_Config_t::eventsCallback() will fire with RAIL_EVENT_TX_FIFO_ALMOST_EMPTY set. The txThreshold value should be smaller than or equal to the transmit FIFO size; higher values will be pegged to the FIFO size. A value of 0 or RAIL_FIFO_THRESHOLD_DISABLED will disable the threshold, returning RAIL_FIFO_THRESHOLD_DISABLED.

DeprecatedRAIL 2.x synonym of sl_rail_set_tx_fifo_threshold().


RAIL_SetRxFifoThreshold#

uint16_t RAIL_SetRxFifoThreshold (RAIL_Handle_t railHandle, uint16_t rxThreshold)

Configure the RAIL receive FIFO almost full threshold.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint16_t[in]rxThreshold

The threshold above which the RAIL_EVENT_RX_FIFO_ALMOST_FULL event will fire.

Returns

  • Configured receive FIFO threshold value.

This function configures the threshold for the receive FIFO. When the number of bytes of packet data in the receive FIFO exceeds the configured threshold, RAIL_Config_t::eventsCallback() will keep firing with RAIL_EVENT_RX_FIFO_ALMOST_FULL set as long as the number of bytes in the receive FIFO exceeds the configured threshold value. The rxThreshold value should be smaller than the receive FIFO size; anything else, including a value of RAIL_FIFO_THRESHOLD_DISABLED, will disable the threshold, returning RAIL_FIFO_THRESHOLD_DISABLED.

Note

DeprecatedRAIL 2.x synonym of sl_rail_set_rx_fifo_threshold().


RAIL_GetTxFifoThreshold#

uint16_t RAIL_GetTxFifoThreshold (RAIL_Handle_t railHandle)

Get the RAIL transmit FIFO almost empty threshold value.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • Configured TX Threshold value in bytes.

Retrieves the configured TX threshold value.

DeprecatedRAIL 2.x synonym of sl_rail_get_tx_fifo_threshold().


RAIL_GetRxFifoThreshold#

uint16_t RAIL_GetRxFifoThreshold (RAIL_Handle_t railHandle)

Get the RAIL receive FIFO almost full threshold value.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • Configured RX Threshold value in bytes.

Retrieves the configured RX threshold value.

DeprecatedRAIL 2.x synonym of sl_rail_get_rx_fifo_threshold().


RAIL_ResetFifo#

RAIL_Status_t RAIL_ResetFifo (RAIL_Handle_t railHandle, bool txFifo, bool rxFifo)

Reset the RAIL transmit and/or receive FIFOs.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

bool[in]txFifo

If true, reset the transmit FIFO.

bool[in]rxFifo

If true, reset the receive FIFO and its internal metadata FIFO.

Returns

  • Status code indicating success of the function call.

This function can reset each FIFO independently. The application should not reset the receive FIFO while receiving a frame, nor should it reset the transmit FIFO while transmitting a frame.

DeprecatedRAIL 2.x synonym of sl_rail_reset_fifo().


RAIL_GetRxFifoBytesAvailable#

uint16_t RAIL_GetRxFifoBytesAvailable (RAIL_Handle_t railHandle)

Get the number of bytes used in the receive FIFO.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Only use this function in RX RAIL_DataMethod_t::FIFO_MODE. Apps should use RAIL_GetRxPacketInfo() instead.

Returns

  • Number of bytes used in the receive FIFO.

This function indicates how much packet-related data exists in the receive FIFO that could be read.

Note

  • The number of bytes returned may not just reflect the current packet's data but could also include raw appended info bytes added after successful packet reception and bytes from subsequently received packets. It is up to the app to never try to consume more than the packet's actual data when using the value returned here in a subsequent call to RAIL_ReadRxFifo(), otherwise the receive FIFO will be corrupted.

DeprecatedRAIL 2.x synonym of sl_rail_get_rx_fifo_bytes_available(). Unlike in RAIL 2.x where this function returns 0 when a protocol is inactive, in RAIL 3 if the protocol has established its own independent Rx FIFO and Packet Queue, this function returns the amount of data preserved in the Rx FIFO.


RAIL_GetTxFifoSpaceAvailable#

uint16_t RAIL_GetTxFifoSpaceAvailable (RAIL_Handle_t railHandle)

Get the number of bytes unused in the transmit FIFO.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • Number of bytes unused in the transmit FIFO.

This function indicates how much space is available in the transmit FIFO for writing additional packet data.

DeprecatedRAIL 2.x synonym of sl_rail_get_tx_fifo_space_available().


sl_rail_config_tx_data#

sl_rail_status_t sl_rail_config_tx_data (sl_rail_handle_t rail_handle, const sl_rail_tx_data_config_t * p_tx_data_config)

RAIL TX data management configuration.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

const sl_rail_tx_data_config_t *[in]p_tx_data_config

A non-NULL pointer to RAIL TX data configuration structure.

Returns

  • Status code indicating success of the function call.

This function configures how RAIL manages TX data.

Generally with sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE, the application sets an appropriate FIFO threshold via sl_rail_set_tx_fifo_threshold() and then enables and handles the SL_RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event callback (to feed more packet data via sl_rail_write_tx_fifo() before the FIFO underflows).

When configuring TX for sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE, this function resets the transmit FIFO. When configuring TX for sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE, this function will reset the corresponding FIFO thresholds such that they won't trigger SL_RAIL_EVENT_TX_FIFO_ALMOST_EMPTY events.


sl_rail_config_rx_data#

sl_rail_status_t sl_rail_config_rx_data (sl_rail_handle_t rail_handle, const sl_rail_rx_data_config_t * p_rx_data_config)

RAIL RX data management configuration.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

const sl_rail_rx_data_config_t *[in]p_rx_data_config

A non-NULL pointer to RAIL RX data configuration structure.

Returns

This function configures how RAIL manages RX data. The application can configure RAIL to receive data in a packet-based or FIFO-based manner. sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE is necessary to receive packets larger than the radio's receive FIFO. It is also required for receive data sources other than sl_rail_rx_data_source_t::SL_RAIL_RX_DATA_SOURCE_PACKET_DATA.

Generally with sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE, the application sets an appropriate FIFO threshold via sl_rail_set_rx_fifo_threshold() and then enables and handles the SL_RAIL_EVENT_RX_FIFO_ALMOST_FULL event callback (to consume packet data via sl_rail_read_rx_fifo() before the receive FIFO overflows).

When configuring RX for sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE, this function will reset the corresponding FIFO thresholds such that they won't trigger SL_RAIL_EVENT_RX_FIFO_ALMOST_FULL events.

When sl_rail_rx_data_config_t::rx_method is set to sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE, the radio won't drop packet data of aborted or CRC error packets, but will present it to the application to deal with accordingly. On completion of erroneous packets, the sl_rail_config_t::events_callback() with SL_RAIL_EVENT_RX_PACKET_ABORTED, SL_RAIL_EVENT_RX_FRAME_ERROR, or SL_RAIL_EVENT_RX_ADDRESS_FILTERED will tell the application it can drop any data it read via sl_rail_read_rx_fifo() during reception. For CRC error packets when the SL_RAIL_RX_OPTION_IGNORE_CRC_ERRORS RX option is in effect, the application should check for that from the sl_rail_rx_packet_status_t obtained by calling sl_rail_get_rx_packet_info(). RAIL will automatically flush any remaining packet data after reporting one of these packet completion events or the application can explicitly flush it by calling sl_rail_release_rx_packet().

When sl_rail_rx_data_config_t::rx_method is set to sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE, the radio will roll back (drop) all packet data associated with aborted packets including those with CRC errors (unless configured to ignore CRC errors via the SL_RAIL_RX_OPTION_IGNORE_CRC_ERRORS RX option). The application will never have to deal with packet data from these packets. In either mode, the application can set RX options as needed.

When sl_rail_rx_data_config_t::rx_source is set to a value other than SL_RAIL_RX_DATA_SOURCE_PACKET_DATA and sl_rail_config_t::events_callback()SL_RAIL_EVENT_RX_FIFO_OVERFLOW is enabled RX will be terminated if a RX FIFO overflow occurs. If SL_RAIL_EVENT_RX_FIFO_OVERFLOW is not enabled, data will be discarded until the overflow condition is resolved. To continue capturing data RX must be restarted using sl_rail_start_rx().


sl_rail_write_tx_fifo#

uint16_t sl_rail_write_tx_fifo (sl_rail_handle_t rail_handle, const uint8_t * p_data, uint16_t write_bytes, bool reset)

Write data to the transmit FIFO previously established by sl_rail_set_tx_fifo().

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

const uint8_t *[in]p_data

A pointer to transmit data.

uint16_t[in]write_bytes

A number of bytes to write to the transmit FIFO.

bool[in]reset

If true, resets transmit FIFO before writing the data.

Returns

  • The number of bytes written to the transmit FIFO.

This function copies write_bytes of data from the provided p_data into the transmit FIFO previously established by sl_rail_set_tx_fifo() or sl_rail_init(). If the requested write_bytes exceeds the current number of bytes open in the transmit FIFO, the function only writes until the transmit FIFO is full. The function returns the number of bytes written to the transmit FIFO or returns zero if rail_handle is NULL or if the transmit FIFO is full.

Note

  • The protocol's packet configuration, as set up by the radio configurator or via sl_rail_set_fixed_length(), determines how many bytes of data are consumed from the transmit FIFO for a successful transmit operation, not the write_bytes value passed in. If not enough data has been put into the transmit FIFO, a SL_RAIL_EVENT_TX_UNDERFLOW event will occur. If too much data is put into the transmit FIFO, the extra data will either become the first bytes sent in a subsequent packet, or will be thrown away if the FIFO gets reset prior to the next transmit. In general, the proper number of packet bytes to put into the transmit FIFO are all payload bytes except for any CRC bytes, which the packet configuration causes to be sent automatically.

  • This function does not utilize a critical section but, depending on the application, calling it within a critical section could be appropriate.


sl_rail_set_tx_fifo#

sl_rail_status_t sl_rail_set_tx_fifo (sl_rail_handle_t rail_handle, sl_rail_fifo_buffer_align_t * p_addr, uint16_t size_bytes, uint16_t init_bytes, uint16_t start_offset_bytes)

Set the address of the transmit FIFO, a circular buffer used for TX data, possibly pre-populated with transmit data.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

sl_rail_fifo_buffer_align_t *[inout]p_addr

An appropriately-aligned (see sl_rail_set_tx_fifo description) pointer to a read-write memory location in RAM used as the transmit FIFO. This memory must persist until the next call to this function.

uint16_t[in]size_bytes

The size of the transmit FIFO in bytes. See below for the range of sizes supported and non-power-of-2 limitations.

uint16_t[in]init_bytes

The number of valid bytes already populated in the transmit FIFO after start_offset.

uint16_t[in]start_offset_bytes

A number of bytes defining the start position of the TX data from the transmit FIFO p_addr, only valid if init_bytes is not 0.

Returns

  • Status code indicating success of the function call.

This function sets the RAM memory area for the transmit FIFO. It must be called at least once before any transmit operations occur, unless a transmit FIFO was previously established by sl_rail_init() in its sl_rail_config_t.

The actual FIFO size is specified by the size_bytes argument. It is recommended that size_bytes be a power-of-2 between SL_RAIL_MINIMUM_FIFO_BYTES and SL_RAIL_MAXIMUM_FIFO_BYTES, inclusive, so RAIL can treat the buffer as circular and support sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE operation. If size_bytes is a non-power-of-2 it must be below SL_RAIL_MAXIMUM_FIFO_BYTES and is treated as a linear buffer suitable for sl_rail_data_method_t::SL_RAIL_DATA_METHOD_PACKET_MODE only.

Note

Platforms have different FIFO alignment requirements. The sl_rail_fifo_buffer_align_t accurately reflects the platform's alignment requirement, and the SL_RAIL_DECLARE_FIFO_BUFFER() convenience macro should be used to declare it. If the FIFO is improperly aligned, an error is returned.

Typically sl_rail_write_tx_fifo() is used to write transmit data to the FIFO after calling this function. However, users may pre-populate transmit data directly in the FIFO's memory before calling this function, in which case they must specify the start_offset (allowing unaligned packet data in the aligned FIFO) and init_bytes (relative to start_offset) of that data. If the start_offset plus init_bytes is larger than the FIFOs actual size, the data will be truncated to the FIFO's actual size. Specifying a start_offset will not reduce the FIFO threshold or affect sl_rail_get_tx_fifo_space_available().

Note

  • The start_offset is essentially forgotten after the next transmit – it applies only to the next transmit operation, and is not re-established when the transmit FIFO is reset.

In multiprotocol, each protocol should establish its own transmit FIFO; it's not feasible to share a single transmit FIFO among multiple protocols.

Note

  • The protocol's packet configuration, as set up by the radio configurator or via sl_rail_set_fixed_length(), determines how many bytes of data are consumed from the transmit FIFO for a successful transmit operation, not the init_bytes value passed in. If not enough data has been put into the transmit FIFO, a SL_RAIL_EVENT_TX_UNDERFLOW event will occur. If too much data is put into the transmit FIFO, the extra data will either become the first bytes sent in a subsequent packet, or will be thrown away if the FIFO gets reset or re-established prior to the next transmit. In general, the proper number of packet bytes to put into the transmit FIFO are all payload bytes except for any CRC bytes which the packet configuration causes to be sent automatically.

  • After this function is successfully called, any prior transmit FIFO is orphaned.


sl_rail_set_rx_fifo#

sl_rail_status_t sl_rail_set_rx_fifo (sl_rail_handle_t rail_handle, sl_rail_fifo_buffer_align_t * p_addr, uint16_t * p_size_bytes)

Set the address of the receive FIFO, a circular buffer used for receive data.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

sl_rail_fifo_buffer_align_t *[inout]p_addr

A pointer to a read-write memory location in RAM used as the receive FIFO. This memory must persist until the next call to this function.

uint16_t *[inout]p_size_bytes

A pointer to the desired size of the receive FIFO in bytes. This will be updated with the actual size during the function call.

Returns

  • Status code indicating success of the function call.

This function sets the RAM memory area for the receive FIFO, a circular buffer used to hold received data from one or more packets. It must be called at least once before any receive operations occur, unless a receive FIFO was previously established by sl_rail_init() in its sl_rail_config_t.

The actual FIFO size can be determined by the output p_size_bytes argument. The chosen size is determined based on the available FIFO sizes supported by the hardware and will be the closest allowed size less than or equal to the requested size, unless the requested size is smaller than the minimum FIFO size, in which case an error is returned. For more on supported FIFO sizes and alignments, see chip-specific documentation, such as EFR32.

Platforms have different FIFO alignment requirements. The sl_rail_fifo_buffer_align_t accurately reflects the platform's alignment requirement, and the SL_RAIL_DECLARE_FIFO_BUFFER() convenience macro should be used to declare it. If the FIFO is improperly aligned, an error is returned.

In multiprotocol, RAIL allows each protocol to have its own receive FIFO (and receive packet queue) or to share one receive FIFO and receive Packet Queue across multiple protocols.

Note


sl_rail_read_rx_fifo#

uint16_t sl_rail_read_rx_fifo (sl_rail_handle_t rail_handle, uint8_t * p_data, uint16_t read_bytes)

Read packet data from RAIL's receive FIFO.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

uint8_t *[out]p_data

An application-provided pointer to store data. If NULL, the data is thrown away rather than copied out.

uint16_t[in]read_bytes

A number of packet bytes to read from the FIFO.

Returns

  • The number of packet bytes read from the receive FIFO.

This function reads packet data from the head of receive FIFO and writes it to the provided p_data. It does not permit reading more data than is available in the FIFO, nor does it permit reading more data than remains in the oldest unreleased packet.

Because this function does not have a critical section, use it only in one context or make sure function calls are protected to prevent buffer corruption.

Warnings

Note

  • When reading data from an arriving packet that is not yet complete, keep in mind its data is highly suspect because it has not yet passed any CRC integrity checking. Also note that the packet could be aborted, canceled, or fail momentarily, invalidating its data in Packet mode. Furthermore, there is a small chance towards the end of packet reception that the receive FIFO could include not only packet data received so far, but also some raw radio-appended info detail bytes that RAIL's packet-completion processing will subsequently deal with. It's up to the application to know its packet format well enough to know where a packet's payload ends and not interpret appended info as payload data coming from over the air.


sl_rail_set_rx_packet_queue#

sl_rail_status_t sl_rail_set_rx_packet_queue (sl_rail_handle_t rail_handle, sl_rail_packet_queue_entry_t * p_rx_packet_queue, uint16_t * p_entries)

Set the address of the receive Packet Queue, a circular buffer used by RAIL for received packet metadata that supplements the receive FIFO.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

sl_rail_packet_queue_entry_t *[in]p_rx_packet_queue

A pointer to a read-write memory location in RAM to use for the receive Packet Queue. This memory must persist until the next call to this function and must be able to hold at least the specified p_entries packets.

uint16_t *[inout]p_entries

The desired number of entries in the receive Packet Queue. This will be updated with the actual number of entries if the requested entries are not feasible but fewer are.

Returns

  • Status code indicating success of the function call.

This function sets the RAM memory location for the receive Packet Queue. The number of entries in this circular queue represents the number of packets RAIL can queue to the application before SL_RAIL_EVENT_RX_FIFO_OVERFLOW might occur.

This queue is used for per-packet metadata separate from actual packet payload data placed in the receive FIFO buffer. This function must be called at least once before any receive operations occur if a receive Packet Queue was not provided at sl_rail_init() time via sl_rail_config_t::p_rx_packet_queue.

The actual number of entries can be determined by the output p_entries argument. The chosen number is determined based on the available queue entries supported by the radio and will be the closest allowed number less than or equal to the requested number, unless the requested number is smaller than the minimum number of queue entries, in which case an error is returned. For more on the supported number of receive Packet Queue entries see chip-specific documentation, such as EFR32.

Note


sl_rail_set_tx_fifo_threshold#

uint16_t sl_rail_set_tx_fifo_threshold (sl_rail_handle_t rail_handle, uint16_t tx_threshold_bytes)

Configure the RAIL transmit FIFO almost empty threshold.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

uint16_t[in]tx_threshold_bytes

The threshold below which the SL_RAIL_EVENT_TX_FIFO_ALMOST_EMPTY event will fire.

Returns

  • Configured transmit FIFO threshold value.

This function configures the threshold for the transmit FIFO. When the number of bytes in the transmit FIFO falls below the configured threshold, sl_rail_config_t::events_callback() will fire with SL_RAIL_EVENT_TX_FIFO_ALMOST_EMPTY set. The tx_threshold_bytes value should be smaller than or equal to the transmit FIFO size; higher values will be pegged to the FIFO size. A value of 0 or SL_RAIL_FIFO_THRESHOLD_DISABLED will disable the threshold, returning SL_RAIL_FIFO_THRESHOLD_DISABLED.


sl_rail_set_rx_fifo_threshold#

uint16_t sl_rail_set_rx_fifo_threshold (sl_rail_handle_t rail_handle, uint16_t rx_threshold_bytes)

Configure the RAIL receive FIFO almost full threshold.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

uint16_t[in]rx_threshold_bytes

The threshold above which the SL_RAIL_EVENT_RX_FIFO_ALMOST_FULL event will fire.

Returns

  • Configured receive FIFO threshold value.

This function configures the threshold for the receive FIFO. When the number of bytes of packet data in the receive FIFO exceeds the configured threshold, sl_rail_config_t::events_callback() will keep firing with SL_RAIL_EVENT_RX_FIFO_ALMOST_FULL set as long as the number of bytes in the receive FIFO exceeds the configured threshold value. The rx_threshold_bytes value should be smaller than the receive FIFO size; anything else, including a value of SL_RAIL_FIFO_THRESHOLD_DISABLED, will disable the threshold, returning SL_RAIL_FIFO_THRESHOLD_DISABLED.

Note


sl_rail_get_tx_fifo_threshold#

uint16_t sl_rail_get_tx_fifo_threshold (sl_rail_handle_t rail_handle)

Get the RAIL transmit FIFO almost empty threshold value.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

  • Configured TX Threshold value in bytes.

Retrieves the configured TX threshold value.


sl_rail_get_rx_fifo_threshold#

uint16_t sl_rail_get_rx_fifo_threshold (sl_rail_handle_t rail_handle)

Get the RAIL receive FIFO almost full threshold value.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

  • Configured RX Threshold value in bytes.

Retrieves the configured RX threshold value.


sl_rail_reset_fifo#

sl_rail_status_t sl_rail_reset_fifo (sl_rail_handle_t rail_handle, bool tx_fifo, bool rx_fifo)

Reset the RAIL transmit and/or receive FIFOs.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

bool[in]tx_fifo

If true, reset the transmit FIFO.

bool[in]rx_fifo

If true, reset the receive FIFO and its associated receive Packet Queue.

Returns

  • Status code indicating success of the function call.

This function can reset each FIFO independently. The application should not reset the receive FIFO while receiving a frame, nor should it reset the transmit FIFO while transmitting a frame.


sl_rail_get_rx_fifo_bytes_available#

uint16_t sl_rail_get_rx_fifo_bytes_available (sl_rail_handle_t rail_handle)

Get the number of bytes used in the receive FIFO.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Only use this function in RX sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE. Apps should use sl_rail_get_rx_packet_info() instead.

Returns

  • Number of bytes used in the receive FIFO.

This function indicates how much packet-related data exists in the receive FIFO that could be read.

Note

  • The number of bytes returned may not just reflect the current packet's data but could also include raw appended info bytes added after successful packet reception and bytes from subsequently received packets. It is up to the app to never try to consume more than the packet's actual data when using the value returned here in a subsequent call to sl_rail_read_rx_fifo(), otherwise the receive FIFO will be corrupted.


sl_rail_get_tx_fifo_space_available#

uint16_t sl_rail_get_tx_fifo_space_available (sl_rail_handle_t rail_handle)

Get the number of bytes unused in the transmit FIFO.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

  • Number of bytes unused in the transmit FIFO.

This function indicates how much space is available in the transmit FIFO for writing additional packet data.


Macro Definition Documentation#

RAIL_FIFO_ALIGNMENT_TYPE#

#define RAIL_FIFO_ALIGNMENT_TYPE
Value:
uint32_t

Fixed-width type indicating the needed alignment for RX and TX FIFOs.

DeprecatedRAIL 2.x synonym of sl_rail_fifo_buffer_align_t.


RAIL_FIFO_ALIGNMENT#

#define RAIL_FIFO_ALIGNMENT
Value:
(sizeof(RAIL_FIFO_ALIGNMENT_TYPE))

Alignment that is needed for the RX and TX FIFOs.

DeprecatedThis RAIL 2.x define has been eliminated in RAIL 3; use SL_RAIL_DECLARE_FIFO_BUFFER().


RAIL_FIFO_THRESHOLD_DISABLED#

#define RAIL_FIFO_THRESHOLD_DISABLED
Value:
0xFFFFU

A FIFO threshold value that disables the threshold.

DeprecatedRAIL 2.x synonym of SL_RAIL_FIFO_THRESHOLD_DISABLED.


SL_RAIL_BUILTIN_RX_FIFO_BYTES#

#define SL_RAIL_BUILTIN_RX_FIFO_BYTES
Value:
512

Compile-time size in bytes of the built-in receive FIFO buffer to which sl_rail_builtin_rx_fifo_ptr points.


SL_RAIL_BUILTIN_RX_PACKET_QUEUE_ENTRIES#

#define SL_RAIL_BUILTIN_RX_PACKET_QUEUE_ENTRIES
Value:
16

Compile-time number of entries in the built-in receive Packet Queue to which sl_rail_builtin_rx_packet_queue_ptr points.


SL_RAIL_DECLARE_FIFO_BUFFER#

#define SL_RAIL_DECLARE_FIFO_BUFFER
Value:
(buffer_name, bytes)

Convenience macro for declaring RAIL FIFO buffers of desired size.

For example:

#define MY_RX_FIFO_BUFFER_BYTES 512
union my_rx_fifo_buffer_u {
  SL_RAIL_DECLARE_FIFO_BUFFER(aligned, MY_RX_FIFO_BUFFER_BYTES);
  uint8_t bytes[MY_RX_FIFO_BUFFER_BYTES]; // For byte accessing
} my_rx_fifo_buffer;

sl_rail_config_t my_rail_config = {
  .rx_fifo_bytes = sizeof(my_rx_fifo_buffer),
  .rx_fifo_buffer = my_rx_fifo_buffer.aligned,
  ...
};

SL_RAIL_MINIMUM_FIFO_BYTES#

#define SL_RAIL_MINIMUM_FIFO_BYTES
Value:
(64U)

The minimum size in bytes of a receive / transmit / Auto-Ack FIFO.


SL_RAIL_MAXIMUM_FIFO_BYTES#

#define SL_RAIL_MAXIMUM_FIFO_BYTES
Value:
(4096U)

The maximum size in bytes of a receive / transmit / Auto-Ack FIFO.


SL_RAIL_FIFO_THRESHOLD_DISABLED#

#define SL_RAIL_FIFO_THRESHOLD_DISABLED
Value:
0xFFFFU

A FIFO threshold value that disables the threshold.