Front End Module Voltage Detection#
APIs for configuring and detecting a voltage from a Front End Module (VDET).
The rail_util_vdet plugin lets customers measure an output voltage from their attached Front End Module at a specific time in a Tx packet. This information allows optimizations to power configuration, and monitoring FEM performance.
Note
VDET is only supported with EFR32xG25 devices.
Modules#
Enumerations#
VDET Modes.
VDET Resolution for the Aux ADC.
VDET Status.
Functions#
Configure the VDET plugin.
Get the VDET plugin configuration.
Enable the VDET plugin.
Check if the VDET plugin is enabled.
Get VDET measurement.
Macros#
A macro that is string versions of the calibration enums.
A macro that is string versions of the resolution enums.
A macro that is string versions of the status enums.
Enumeration Documentation#
RAIL_Vdet_Mode_t#
RAIL_Vdet_Mode_t
VDET Modes.
The VDET Mode is passed to RAIL_ConfigVdet() via RAIL_VdetConfig_t. The Front End Module Voltage Detection (VDET) Utility component allows customers to measure their Front End Module performance at specified points in the Transmit packet.
| Enumerator | |
|---|---|
| RAIL_VDET_MODE_DISABLED | VDET is completely disabled. |
| RAIL_VDET_MODE_AUTOMATIC | AUTOMATIC causes VDET measurements to be taken every Tx packet at the specified time. |
| RAIL_VDET_MODE_IMMEDIATE | IMMEDIATE causes an immediate VDET measurement. |
| RAIL_VDET_MODE_COUNT | A count of the choices in this enumeration. |
RAIL_Vdet_Resolution_t#
RAIL_Vdet_Resolution_t
VDET Resolution for the Aux ADC.
The VDET Resolution is passed to RAIL_ConfigVdet() via RAIL_VdetConfig_t. Shows available resolution options.
| Enumerator | |
|---|---|
| RAIL_VDET_RESOLUTION_10_BIT | ~10 bit resolution. |
| RAIL_VDET_RESOLUTION_11_BIT | ~11 bit resolution. |
| RAIL_VDET_RESOLUTION_12_BIT | ~12 bit resolution. |
| RAIL_VDET_RESOLUTION_COUNT | A count of the choices in this enumeration. |
RAIL_Vdet_Status_t#
RAIL_Vdet_Status_t
VDET Status.
The VDET Status for internal debug. Shows states.
| Enumerator | |
|---|---|
| RAIL_VDET_STATUS_IDLE | IDLE - Waiting for next command/measurement. |
| RAIL_VDET_STATUS_START | START of the VDET measurement activity. |
| RAIL_VDET_STATUS_10_BIT_DONE | Completion of a 10 bit measurement. |
| RAIL_VDET_STATUS_11_BIT_DONE | Completion of a 11 bit measurement. |
| RAIL_VDET_STATUS_12_BIT_DONE | Completion of a 12 bit measurement. |
| RAIL_VDET_STATUS_BLOCKED | Conflict with another AuxADC user. |
| RAIL_VDET_STATUS_ERROR | An error has occurred. |
| RAIL_VDET_STATUS_COUNT | A count of the choices in this enumeration. |
Function Documentation#
RAIL_ConfigVdet#
RAIL_Status_t RAIL_ConfigVdet (RAIL_Handle_t genericRailHandle, const RAIL_VdetConfig_t * config)
Configure the VDET plugin.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | genericRailHandle | A radio-generic RAIL handle. |
| const RAIL_VdetConfig_t * | [in] | config | A pointer to a RAIL_VdetConfig_t struct that contains configuration data for the VDET. |
Returns
Return values
RAIL_STATUS_NO_ERROR: - All went well
RAIL_STATUS_INVALID_STATE: - VDET is enabled. Must be disabled first.
RAIL_STATUS_INVALID_PARAMETER: - mode/resolution/delayUs out-of-bounds.
Warnings
As this function relies on GPIO access and RAIL is meant to run in TrustZone non-secure world, it is not supported if GPIO is configured as secure peripheral and it will return RAIL_STATUS_INVALID_CALL.
RAIL_GetVdetConfig#
RAIL_Status_t RAIL_GetVdetConfig (RAIL_Handle_t genericRailHandle, RAIL_VdetConfig_t * config)
Get the VDET plugin configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | genericRailHandle | A radio-generic RAIL handle. |
| RAIL_VdetConfig_t * | [out] | config | A pointer to a RAIL_VdetConfig_t struct that will return configuration data for the VDET. |
Returns
Return values
RAIL_STATUS_NO_ERROR: - All went well.
RAIL_EnableVdet#
RAIL_Status_t RAIL_EnableVdet (RAIL_Handle_t genericRailHandle, bool enable)
Enable the VDET plugin.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | genericRailHandle | A RAIL instance handle. |
| bool | [in] | enable | Enable or disable RAIL_VDET_MODE_AUTOMATIC mode captures. Begins measurement if in RAIL_VDET_MODE_IMMEDIATE. |
Returns
Return values
RAIL_STATUS_NO_ERROR: - All went well, VDET is enabled or disabled.
RAIL_STATUS_INVALID_STATE: - VDET has not been configured or VDET was not idle. VDET is disabled.
Warnings
As this function relies on HFXO access and RAIL is meant to run in TrustZone non-secure world, it is not supported if HFXO is configured as secure peripheral and it will return RAIL_STATUS_INVALID_CALL.
RAIL_IsVdetEnabled#
bool RAIL_IsVdetEnabled (RAIL_Handle_t genericRailHandle)
Check if the VDET plugin is enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | genericRailHandle | A RAIL instance handle. |
Returns
bool
RAIL_GetVdet#
RAIL_Status_t RAIL_GetVdet (RAIL_Handle_t genericRailHandle, uint32_t * pVdetMv)
Get VDET measurement.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | genericRailHandle | A RAIL instance handle. |
| uint32_t * | [out] | pVdetMv | A pointer to a uint32_t for returning the measurement. |
A processed measurement in millivolts.
Returns
Return values
RAIL_STATUS_NO_ERROR: - All went well, value in *pVdetMv is valid.
RAIL_STATUS_INVALID_CALL: - VDET is in progress, wait until VDET capture is complete and try again.
RAIL_STATUS_INVALID_STATE: - VDET is not enabled or valid. Wait until next packet and try reading again.
RAIL_STATUS_INVALID_PARAMETER: - In
RAIL_STATUS_SUSPENDED: - Blocked by AuxADC contention. Wait until next packet and try reading again.
Warnings
As this function relies on HFXO access and RAIL is meant to run in TrustZone non-secure world, it is not supported if HFXO is configured as secure peripheral and it will return RAIL_STATUS_INVALID_CALL.