TX Channel Hopping#

Modules#

RAIL_TxChannelHoppingConfigEntry_t

RAIL_TxChannelHoppingConfig_t

sl_rail_tx_channel_hopping_config_entry_t

sl_rail_tx_channel_hopping_config_t

Macros#

#define

The worst-case platform-agnostic static amount of memory needed per channel for channel hopping, measured in 32 bit words, regardless of the size of radio configuration structures.

#define

The worst-case platform-agnostic static amount of memory needed per channel for channel hopping, measured in 32 bit words, regardless of the size of radio configuration structures.

Macro Definition Documentation#

RAIL_CHANNEL_HOPPING_BUFFER_SIZE_PER_CHANNEL_WORST_CASE#

#define RAIL_CHANNEL_HOPPING_BUFFER_SIZE_PER_CHANNEL_WORST_CASE
Value:
(65U)

The worst-case platform-agnostic static amount of memory needed per channel for channel hopping, measured in 32 bit words, regardless of the size of radio configuration structures.

DeprecatedRAIL 2.x synonym of SL_RAIL_CHANNEL_HOPPING_BUFFER_WORDS_PER_CHANNEL_WORST_CASE.


SL_RAIL_CHANNEL_HOPPING_BUFFER_WORDS_PER_CHANNEL_WORST_CASE#

#define SL_RAIL_CHANNEL_HOPPING_BUFFER_WORDS_PER_CHANNEL_WORST_CASE
Value:
(65U)

The worst-case platform-agnostic static amount of memory needed per channel for channel hopping, measured in 32 bit words, regardless of the size of radio configuration structures.