Structure that represents one of the channels that is part of a RAIL_TxChannelHoppingConfig_t sequence of channels used in channel hopping.
Public Attributes#
uint16_t
The channel number to be used for this entry in the channel hopping sequence.
uint8_t
Pad bytes reserved for future use and currently ignored.
uint32_t
Idle time in microseconds to wait before transmitting on the channel indicated by this entry.
Public Attribute Documentation#
channel#
uint16_t RAIL_TxChannelHoppingConfigEntry_t::channel
The channel number to be used for this entry in the channel hopping sequence.
If this is an invalid channel for the current PHY, the call to RAIL_SetNextTxRepeat() will fail.
Definition at line
2934
of file common/rail_types.h
reserved#
uint8_t RAIL_TxChannelHoppingConfigEntry_t::reserved[2]
Pad bytes reserved for future use and currently ignored.
Definition at line
2938
of file common/rail_types.h
delay#
uint32_t RAIL_TxChannelHoppingConfigEntry_t::delay
Idle time in microseconds to wait before transmitting on the channel indicated by this entry.
Definition at line
2943
of file common/rail_types.h