Wrapper struct that will contain the sequence of sl_rail_tx_channel_hopping_config_entry_t that represents the channel sequence to use during TX Channel Hopping.

Public Attributes#

uint32_t *

Pointer to contiguous global read-write memory that will be used by RAIL to store channel hopping information throughout its operation.

uint16_t

This parameter must be set to the length of the buffer array, in 32 bit words.

uint8_t

The number of channels in the channel hopping sequence, which is the number of elements in the array that entries points to.

uint8_t

Pad byte reserved for future use and currently ignored.

A pointer to the first element of an array of sl_rail_tx_channel_hopping_config_entry_t that represents the channels used during channel hopping.

Public Attribute Documentation#

p_buffer#

uint32_t* sl_rail_tx_channel_hopping_config_t::p_buffer

Pointer to contiguous global read-write memory that will be used by RAIL to store channel hopping information throughout its operation.

It need not be initialized and applications should never write data anywhere in this buffer.

Note

  • The size of this buffer must be at least as large as 3 + SL_RAIL_CHANNEL_HOPPING_BUFFER_WORDS_PER_CHANNEL * number_of_channels, plus the sum of the sizes of the radio_config_delta_add's of the required channels, plus the size of the radio_config_delta_subtract. In the case that one channel appears two or more times in your channel sequence (e.g., 1, 2, 3, 2), you must account for the radio configuration size that number of times (i.e., need to count channel 2's radio configuration size twice for the given example). The buffer is for internal use to the library.


buffer_words#

uint16_t sl_rail_tx_channel_hopping_config_t::buffer_words

This parameter must be set to the length of the buffer array, in 32 bit words.

This way, during configuration, the software can confirm it's writing within the bounds of the buffer. The configuration API will return an error or trigger SL_RAIL_ASSERT_CHANNEL_HOPPING_BUFFER_TOO_SHORT if buffer_words is insufficient.


number_of_channels#

uint8_t sl_rail_tx_channel_hopping_config_t::number_of_channels

The number of channels in the channel hopping sequence, which is the number of elements in the array that entries points to.


reserved#

uint8_t sl_rail_tx_channel_hopping_config_t::reserved

Pad byte reserved for future use and currently ignored.


p_entries#

sl_rail_tx_channel_hopping_config_entry_t* sl_rail_tx_channel_hopping_config_t::p_entries

A pointer to the first element of an array of sl_rail_tx_channel_hopping_config_entry_t that represents the channels used during channel hopping.

The length of this array must be number_of_channels.