TrustZone#
APIs to use RAIL with TrustZone enabled and peripherals configured as secure.
RAIL internally accesses CMU, EMU, GPIO, LDMA, HFXO, PRS and SYSRTC. If some of them are configured as secure peripherals, some RAIL code must be executed as secure code. To do so, callbacks gathered in RAIL_TZ_Config_t must be implemented and passed to RAIL through RAIL_TZ_InitNonSecure(). Each callback must do the non-secure/secure transition, call RAIL_TZ_CheckPeripheralsSecureStates() and then call the corresponding RAIL API from secure world:
RAIL internally calls platform functions that access CMU, EMU, GPIO, LDMA HFXO and PRS. If some of them are configured as secure peripherals, some functions must be executed as secure code. To do so, those functions are prepended with weak symbols and must be overwritten to do the non-secure/secure transition and call the corresponding platform function from secure world:
Secure peripheral | Platform functions to overwrite |
|---|---|
CMU | CMU_ClockEnable, EMU_DCDCSetPFMXTimeoutMaxCtrl (DCDC access: SL_TRUSTZONE_PERIPHERAL_DCDC_S) |
HFXO | CMU_HFXOCTuneSet, CMU_HFXOCTuneGet, CMU_HFXOCoreBiasCurrentCalibrate |
PRS | PRS_SourceAsyncSignalSet, PRS_GetFreeChannel, PRS_ConnectConsumer, PRS_PinOutput, PRS_Combine |
When there is a combination of secure and non-secure peripherals, defines must be added in secure application slcp file so non-secure peripherals can properly accessed by secure code. Example with only CMU non-secure:
define:
- name: SL_TRUSTZONE_PERIPHERAL_CMU_S
value: 0
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_EMU_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_GPIO_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_LDMA_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_HFXO0_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_PRS_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_SYSRTC_S
value: 1
condition: [trustzone_secure]
Some RAIL API are not suppoted with EMU, GPIO, LDMA, HFXO, PRS or SYSRTC configured secure:
RAIL internally accesses CMU, EMU, GPIO, LDMA, HFXO, PRS and SYSRTC. If some of them are configured as secure peripherals, some RAIL code must be executed as secure code. To do so, callbacks gathered in sl_rail_tz_config_t must be implemented and passed to RAIL through sl_rail_tz_init_non_secure(). Each callback must do the non-secure/secure transition, call sl_rail_tz_check_peripherals_secure_states() and then call the corresponding RAIL API from secure world:
RAIL internally calls platform functions that access CMU, EMU, GPIO, LDMA HFXO and PRS. If some of them are configured as secure peripherals, some functions must be executed as secure code. To do so, those functions are prepended with weak symbols and must be overwritten to do the non-secure/secure transition and call the corresponding platform function from secure world:
Secure peripheral | Platform functions to overwrite |
|---|---|
CMU | CMU_ClockEnable, EMU_DCDCSetPFMXTimeoutMaxCtrl (DCDC access: SL_TRUSTZONE_PERIPHERAL_DCDC_S) |
HFXO | CMU_HFXOCTuneSet, CMU_HFXOCTuneGet, CMU_HFXOCoreBiasCurrentCalibrate |
PRS | PRS_SourceAsyncSignalSet, PRS_GetFreeChannel, PRS_ConnectConsumer, PRS_PinOutput, PRS_Combine |
When there is a combination of secure and non-secure peripherals, defines must be added in secure application slcp file so non-secure peripherals can properly accessed by secure code. Example with only CMU non-secure:
define:
- name: SL_TRUSTZONE_PERIPHERAL_CMU_S
value: 0
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_EMU_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_GPIO_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_LDMA_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_HFXO0_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_PRS_S
value: 1
condition: [trustzone_secure]
- name: SL_TRUSTZONE_PERIPHERAL_SYSRTC_S
value: 1
condition: [trustzone_secure]
Some RAIL API are not suppoted with EMU, GPIO LDMA, HFXO, PRS or SYSRTC configured secure:
Modules#
Typedefs#
A pointer to the callback used to switch to secure world and run RAIL_ChangedDcdc().
A pointer to the callback used to switch to secure world and run RAIL_TZ_ConfigAntennaGpio().
A pointer to the callback used to switch to secure world and run RAIL_TZ_RadioClockEnable().
A pointer to the callback used to switch to secure world and run RAIL_GetRadioClockFreqHz().
A pointer to the callback used to switch to secure world and run RAIL_TZ_RfecaClockEnable().
A pointer to the callback used to switch to secure world and run RAIL_TZ_RfecaIsClockEnabled().
A pointer to the callback used to switch to secure world and run RAIL_TZ_ReadInternalTemperature().
A pointer to the callback used to switch to secure world and run RAIL_TZ_EnableSecureRadioIrqs().
A pointer to the callback used to switch to secure world and run RAIL_TZ_DisableSecureRadioIrqs().
A pointer to the callback used to switch to secure world and run RAIL_TZ_RadioPerformM2mLdma().
A pointer to the callback used to switch to secure world and run RAIL_TZ_ConfigureHfxo().
A pointer to the callback used to switch to secure world and run sl_rail_changed_dcdc().
A pointer to the callback used to switch to secure world and run sl_rail_tz_config_antenna_gpio().
A pointer to the callback used to switch to secure world and run sl_rail_tz_radio_clock_enable().
A pointer to the callback used to switch to secure world and run sl_rail_get_radio_clock_freq_hz().
A pointer to the callback used to switch to secure world and run sl_rail_tz_rfeca_clock_enable().
A pointer to the callback used to switch to secure world and run sl_rail_tz_rfeca_is_clock_enabled().
A pointer to the callback used to switch to secure world and run sl_rail_tz_read_internal_temperature().
A pointer to the callback used to switch to secure world and run sl_rail_tz_enable_secure_radio_irqs().
A pointer to the callback used to switch to secure world and run sl_rail_tz_disable_secure_radio_irqs().
A pointer to the callback used to switch to secure world and run sl_rail_tz_radio_perform_m2m_ldma().
A pointer to the callback used to switch to secure world and run sl_rail_tz_configure_hfxo().
Functions#
Init RAIL TrustZone feature for non-secure world.
Init RAIL TrustZone feature for secure world.
Check the secure state of peripherals used by RAIL.
Enable radio clocks.
Enable RFECA clocks.
Indicate whether RFECA clocks are enabled.
Read the internal temperature.
Enable secure peripheral interrupts needed by the radio.
Disable secure peripheral interrupts needed by the radio.
Perform ldma transfer for the radio.
Configure HFXO.
Set GPIO for antenna config.
Init RAIL TrustZone feature for non-secure world.
Init RAIL TrustZone feature for secure world.
Check the secure state of peripherals used by RAIL.
Enable radio clocks.
Enable RFECA clocks.
Indicate whether RFECA clocks are enabled.
Read the internal temperature.
Enable secure peripheral interrupts needed by the radio.
Disable secure peripheral interrupts needed by the radio.
Perform ldma transfer for the radio.
Configure HFXO.
Set GPIO for antenna config.
Typedef Documentation#
RAIL_TZ_ChangedDcdcCallbackPtr_t#
RAIL_TZ_ChangedDcdcCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_ChangedDcdc().
Returns
Status code indicating success of the function call.
DeprecatedRAIL 2.x synonym of sl_rail_tz_changed_dcdc_callback_t().
RAIL_TZ_ConfigAntennaGpioCallbackPtr_t#
RAIL_TZ_ConfigAntennaGpioCallbackPtr_t )(const RAIL_AntennaConfig_t *config)
A pointer to the callback used to switch to secure world and run RAIL_TZ_ConfigAntennaGpio().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | config | A pointer to a configuration structure applied to the relevant Antenna Configuration registers. A NULL configuration will produce undefined behavior. |
Returns
Status code indicating success of the function call.
DeprecatedRAIL 2.x synonym of sl_rail_tz_config_antenna_gpio_callback_t().
RAIL_TZ_RadioClockEnableCallbackPtr_t#
RAIL_TZ_RadioClockEnableCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_RadioClockEnable().
DeprecatedRAIL 2.x synonym of sl_rail_tz_radio_clock_enable_callback_t().
RAIL_TZ_GetRadioClockFreqHzCallbackPtr_t#
RAIL_TZ_GetRadioClockFreqHzCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_GetRadioClockFreqHz().
Returns
Radio subsystem clock frequency in Hz.
DeprecatedRAIL 2.x synonym of sl_rail_tz_get_radio_clock_freq_hz_callback_t().
RAIL_TZ_RfecaClockEnableCallbackPtr_t#
RAIL_TZ_RfecaClockEnableCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_RfecaClockEnable().
DeprecatedRAIL 2.x synonym of sl_rail_tz_rfeca_clock_enable_callback_t().
RAIL_TZ_RfecaIsClockEnabledCallbackPtr_t#
RAIL_TZ_RfecaIsClockEnabledCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_RfecaIsClockEnabled().
Returns
true if RFECA clocks are enabled; false otherwise
DeprecatedRAIL 2.x synonym of sl_rail_tz_rfeca_is_clock_enabled_callback_t().
RAIL_TZ_ReadInternalTemperatureCallbackPtr_t#
RAIL_TZ_ReadInternalTemperatureCallbackPtr_t )(uint16_t *internalTemperatureKelvin, bool enableTemperatureInterrupts)
A pointer to the callback used to switch to secure world and run RAIL_TZ_ReadInternalTemperature().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [out] | internalTemperatureKelvin | A pointer to the internal temperature in Kelvin. | |
| [in] | enableTemperatureInterrupts | Indicate whether temperature interrupts are enabled. |
Returns
Status code indicating success of the function call.
DeprecatedRAIL 2.x synonym of sl_rail_tz_read_internal_temperature_callback_t().
RAIL_TZ_EnableSecureRadioIrqsCallbackPtr_t#
RAIL_TZ_EnableSecureRadioIrqsCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_EnableSecureRadioIrqs().
DeprecatedRAIL 2.x synonym of sl_rail_tz_enable_secure_radio_irqs_callback_t().
RAIL_TZ_DisableSecureRadioIrqsCallbackPtr_t#
RAIL_TZ_DisableSecureRadioIrqsCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_DisableSecureRadioIrqs().
DeprecatedRAIL 2.x synonym of sl_rail_tz_disable_secure_radio_irqs_callback_t().
RAIL_TZ_RadioPerformM2mLdmaCallbackPtr_t#
RAIL_TZ_RadioPerformM2mLdmaCallbackPtr_t )(uint32_t *pDest, const uint32_t *pSrc, uint32_t numWords)
A pointer to the callback used to switch to secure world and run RAIL_TZ_RadioPerformM2mLdma().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | pDest | A pointer to the destination data. | |
| [in] | pSrc | A pointer to the source data. | |
| [in] | numWords | Number of words to transfer. |
Returns
Status code indicating success of the function call.
DeprecatedRAIL 2.x synonym of sl_rail_tz_radio_perform_m2m_ldma_callback_t().
RAIL_TZ_ConfigureHfxoCallbackPtr_t#
RAIL_TZ_ConfigureHfxoCallbackPtr_t )(void)
A pointer to the callback used to switch to secure world and run RAIL_TZ_ConfigureHfxo().
DeprecatedRAIL 2.x synonym of sl_rail_tz_configure_hfxo_callback_t().
sl_rail_tz_changed_dcdc_callback_t#
sl_rail_tz_changed_dcdc_callback_t )(void)
A pointer to the callback used to switch to secure world and run sl_rail_changed_dcdc().
Returns
Status code indicating success of the function call.
sl_rail_tz_config_antenna_gpio_callback_t#
sl_rail_tz_config_antenna_gpio_callback_t )(const sl_rail_antenna_config_t *p_config)
A pointer to the callback used to switch to secure world and run sl_rail_tz_config_antenna_gpio().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | p_config | A pointer to a configuration structure applied to the relevant Antenna Configuration registers. A NULL configuration will produce undefined behavior. |
Returns
Status code indicating success of the function call.
sl_rail_tz_radio_clock_enable_callback_t#
sl_rail_tz_radio_clock_enable_callback_t )(void)
A pointer to the callback used to switch to secure world and run sl_rail_tz_radio_clock_enable().
sl_rail_tz_get_radio_clock_freq_hz_callback_t#
sl_rail_tz_get_radio_clock_freq_hz_callback_t )(void)
A pointer to the callback used to switch to secure world and run sl_rail_get_radio_clock_freq_hz().
Returns
Radio subsystem clock frequency in Hz.
sl_rail_tz_rfeca_clock_enable_callback_t#
sl_rail_tz_rfeca_clock_enable_callback_t )(void)
A pointer to the callback used to switch to secure world and run sl_rail_tz_rfeca_clock_enable().
sl_rail_tz_rfeca_is_clock_enabled_callback_t#
sl_rail_tz_rfeca_is_clock_enabled_callback_t )(void)
A pointer to the callback used to switch to secure world and run sl_rail_tz_rfeca_is_clock_enabled().
Returns
true if RFECA clocks are enabled; false otherwise
sl_rail_tz_read_internal_temperature_callback_t#
sl_rail_tz_read_internal_temperature_callback_t )(uint16_t *p_internal_temperature_kelvin, bool enable_temperature_interrupts)
A pointer to the callback used to switch to secure world and run sl_rail_tz_read_internal_temperature().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [out] | p_internal_temperature_kelvin | A pointer to the internal temperature in Kelvin. | |
| [in] | enable_temperature_interrupts | Indicate whether temperature interrupts are enabled. |
Returns
Status code indicating success of the function call.
sl_rail_tz_enable_secure_radio_irqs_callback_t#
sl_rail_tz_enable_secure_radio_irqs_callback_t )(void)
A pointer to the callback used to switch to secure world and run sl_rail_tz_enable_secure_radio_irqs().
sl_rail_tz_disable_secure_radio_irqs_callback_t#
sl_rail_tz_disable_secure_radio_irqs_callback_t )(void)
A pointer to the callback used to switch to secure world and run sl_rail_tz_disable_secure_radio_irqs().
sl_rail_tz_radio_perform_m2m_ldma_callback_t#
sl_rail_tz_radio_perform_m2m_ldma_callback_t )(uint32_t *p_dest, const uint32_t *p_src, uint32_t num_words)
A pointer to the callback used to switch to secure world and run sl_rail_tz_radio_perform_m2m_ldma().
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | p_dest | A pointer to the destination data. | |
| [in] | p_src | A pointer to the source data. | |
| [in] | num_words | Number of words to transfer. |
Returns
Status code indicating success of the function call.
sl_rail_tz_configure_hfxo_callback_t#
sl_rail_tz_configure_hfxo_callback_t )(void)
A pointer to the callback used to switch to secure world and run sl_rail_tz_configure_hfxo().
Function Documentation#
RAIL_TZ_InitNonSecure#
RAIL_Status_t RAIL_TZ_InitNonSecure (const RAIL_TZ_Config_t * pTzConfig)
Init RAIL TrustZone feature for non-secure world.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const RAIL_TZ_Config_t * | [in] | pTzConfig | A non-NULL pointer to a RAIL_TZ_Config_t structure. |
Returns
Status code indicating success of the function call.
Note
This function must only be called from non-secure world (only if TrustZone is activated) on platforms having RAIL_SUPPORTS_TRUSTZONE_SECURE_PERIPHERALS. It must be called before RAIL_Init() and it must be called again with updated RAIL_TZ_Config_t if peripherals secure configuration has changed.
DeprecatedRAIL 2.x synonym of sl_rail_tz_init_non_secure().
RAIL_TZ_InitSecure#
RAIL_Status_t RAIL_TZ_InitSecure (void )
Init RAIL TrustZone feature for secure world.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world (only if TrustZone is activated) on platforms having RAIL_SUPPORTS_TRUSTZONE_SECURE_PERIPHERALS. It must be called before starting the non-secure application.
DeprecatedRAIL 2.x synonym of sl_rail_tz_init_secure().
RAIL_TZ_CheckPeripheralsSecureStates#
RAIL_Status_t RAIL_TZ_CheckPeripheralsSecureStates (void )
Check the secure state of peripherals used by RAIL.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world and it must be called at the beginning of each RAIL TrustZone callbacks (RAIL_TZ_Config_t) secure code to avoid secure fault.
DeprecatedRAIL 2.x synonym of sl_rail_tz_check_peripherals_secure_states().
RAIL_TZ_RadioClockEnable#
RAIL_Status_t RAIL_TZ_RadioClockEnable (void )
Enable radio clocks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when CMU is configured as secure TrustZone peripheral.
DeprecatedRAIL 2.x synonym of sl_rail_tz_radio_clock_enable().
RAIL_TZ_RfecaClockEnable#
RAIL_Status_t RAIL_TZ_RfecaClockEnable (void )
Enable RFECA clocks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when CMU is configured as secure TrustZone peripheral.
DeprecatedRAIL 2.x synonym of sl_rail_tz_rfeca_clock_enable().
RAIL_TZ_RfecaIsClockEnabled#
bool RAIL_TZ_RfecaIsClockEnabled (void )
Indicate whether RFECA clocks are enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
true if RFECA clocks are enabled; false otherwise
Note
This function must only be called from secure world when CMU is configured as secure TrustZone peripheral.
DeprecatedRAIL 2.x synonym of sl_rail_tz_rfeca_is_clock_enabled().
RAIL_TZ_ReadInternalTemperature#
RAIL_Status_t RAIL_TZ_ReadInternalTemperature (uint16_t * internalTemperatureKelvin, bool enableTemperatureInterrupts)
Read the internal temperature.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t * | [out] | internalTemperatureKelvin | A pointer to the internal temperature in Kelvin. |
| bool | [in] | enableTemperatureInterrupts | Indicate whether temperature interrupts are enabled. |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when EMU is configured as secure TrustZone peripheral.
DeprecatedRAIL 2.x synonym of sl_rail_tz_read_internal_temperature().
RAIL_TZ_EnableSecureRadioIrqs#
RAIL_Status_t RAIL_TZ_EnableSecureRadioIrqs (void )
Enable secure peripheral interrupts needed by the radio.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when EMU is configured as secure TrustZone peripheral.
DeprecatedRAIL 2.x synonym of sl_rail_tz_enable_secure_radio_irqs().
RAIL_TZ_DisableSecureRadioIrqs#
RAIL_Status_t RAIL_TZ_DisableSecureRadioIrqs (void )
Disable secure peripheral interrupts needed by the radio.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when EMU is configured as secure TrustZone peripheral.
DeprecatedRAIL 2.x synonym of sl_rail_tz_disable_secure_radio_irqs().
RAIL_TZ_RadioPerformM2mLdma#
RAIL_Status_t RAIL_TZ_RadioPerformM2mLdma (uint32_t * pDest, const uint32_t * pSrc, uint32_t numWords)
Perform ldma transfer for the radio.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | [in] | pDest | A pointer to the destination data. |
| const uint32_t * | [in] | pSrc | A pointer to the source data. |
| uint32_t | [in] | numWords | Number of words to transfer. |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when LDMA is configured as secure TrustZone peripheral.
DeprecatedRAIL 2.x synonym of sl_rail_tz_radio_perform_m2m_ldma().
RAIL_TZ_ConfigureHfxo#
RAIL_Status_t RAIL_TZ_ConfigureHfxo (void )
Configure HFXO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when HFXO is configured as secure TrustZone peripheral.
DeprecatedRAIL 2.x synonym of sl_rail_tz_configure_hfxo().
RAIL_TZ_ConfigAntennaGpio#
RAIL_Status_t RAIL_TZ_ConfigAntennaGpio (const RAIL_AntennaConfig_t * config)
Set GPIO for antenna config.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const RAIL_AntennaConfig_t * | [in] | config | A pointer to a configuration structure applied to the relevant Antenna Configuration registers. A NULL configuration will produce undefined behavior. |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when CMU or GPIO are configured as secure TrustZone peripheral.
DeprecatedRAIL 2.x synonym of sl_rail_tz_config_antenna_gpio().
sl_rail_tz_init_non_secure#
sl_rail_status_t sl_rail_tz_init_non_secure (const sl_rail_tz_config_t * p_tz_config)
Init RAIL TrustZone feature for non-secure world.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_rail_tz_config_t * | [in] | p_tz_config | A non-NULL pointer to a sl_rail_tz_config_t structure. |
Returns
Status code indicating success of the function call.
Note
This function must only be called from non-secure world (only if TrustZone is activated) on platforms having SL_RAIL_SUPPORTS_TRUSTZONE_SECURE_PERIPHERALS. It must be called before sl_rail_init() and it must be called again with updated sl_rail_tz_config_t if peripherals secure configuration has changed.
sl_rail_tz_init_secure#
sl_rail_status_t sl_rail_tz_init_secure (void )
Init RAIL TrustZone feature for secure world.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world (only if TrustZone is activated) on platforms having SL_RAIL_SUPPORTS_TRUSTZONE_SECURE_PERIPHERALS. It must be called before starting the non-secure application.
sl_rail_tz_check_peripherals_secure_states#
sl_rail_status_t sl_rail_tz_check_peripherals_secure_states (void )
Check the secure state of peripherals used by RAIL.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world and it must be called at the beginning of each RAIL TrustZone callbacks (sl_rail_tz_config_t) secure code to avoid secure fault.
sl_rail_tz_radio_clock_enable#
sl_rail_status_t sl_rail_tz_radio_clock_enable (void )
Enable radio clocks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when CMU is configured as secure TrustZone peripheral.
sl_rail_tz_rfeca_clock_enable#
sl_rail_status_t sl_rail_tz_rfeca_clock_enable (void )
Enable RFECA clocks.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when CMU is configured as secure TrustZone peripheral.
sl_rail_tz_rfeca_is_clock_enabled#
bool sl_rail_tz_rfeca_is_clock_enabled (void )
Indicate whether RFECA clocks are enabled.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
true if RFECA clocks are enabled; false otherwise
Note
This function must only be called from secure world when CMU is configured as secure TrustZone peripheral.
sl_rail_tz_read_internal_temperature#
sl_rail_status_t sl_rail_tz_read_internal_temperature (uint16_t * p_internal_temperature_kelvin, bool enable_temperature_interrupts)
Read the internal temperature.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t * | [out] | p_internal_temperature_kelvin | A pointer to the internal temperature in Kelvin. |
| bool | [in] | enable_temperature_interrupts | Indicate whether temperature interrupts are enabled. |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when EMU is configured as secure TrustZone peripheral.
sl_rail_tz_enable_secure_radio_irqs#
sl_rail_status_t sl_rail_tz_enable_secure_radio_irqs (void )
Enable secure peripheral interrupts needed by the radio.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when EMU is configured as secure TrustZone peripheral.
sl_rail_tz_disable_secure_radio_irqs#
sl_rail_status_t sl_rail_tz_disable_secure_radio_irqs (void )
Disable secure peripheral interrupts needed by the radio.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when EMU is configured as secure TrustZone peripheral.
sl_rail_tz_radio_perform_m2m_ldma#
sl_rail_status_t sl_rail_tz_radio_perform_m2m_ldma (uint32_t * p_dest, const uint32_t * p_src, uint32_t num_words)
Perform ldma transfer for the radio.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint32_t * | [in] | p_dest | A pointer to the destination data. |
| const uint32_t * | [in] | p_src | A pointer to the source data. |
| uint32_t | [in] | num_words | Number of words to transfer. |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when LDMA is configured as secure TrustZone peripheral.
sl_rail_tz_configure_hfxo#
sl_rail_status_t sl_rail_tz_configure_hfxo (void )
Configure HFXO.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when HFXO is configured as secure TrustZone peripheral.
sl_rail_tz_config_antenna_gpio#
sl_rail_status_t sl_rail_tz_config_antenna_gpio (const sl_rail_antenna_config_t * p_config)
Set GPIO for antenna config.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| const sl_rail_antenna_config_t * | [in] | p_config | A pointer to a configuration structure applied to the relevant Antenna Configuration registers. A NULL configuration will produce undefined behavior. |
Returns
Status code indicating success of the function call.
Note
This function must only be called from secure world when CMU or GPIO are configured as secure TrustZone peripherals.