Retiming#
EFR32-specific retiming capability.
The EFR product families have many digital and analog modules that can run in parallel with a radio. These combinations can cause interference and degradation on the radio RX sensitivity. Retiming can modify the clocking of the digital modules to reduce the interference.
Enumerations#
Retiming options bit shifts.
Retiming options bit shifts.
Functions#
Configure retiming options.
Get the currently configured retiming option.
Indicate that the DCDC peripheral bus clock enable has changed allowing RAIL to react accordingly.
Configure retiming options.
Get the currently configured retiming option.
Indicate that the DCDC peripheral bus clock enable has changed allowing RAIL to react accordingly.
Macros#
An option to configure HFXO retiming.
An option to configure HFRCO retiming.
An option to configure DCDC retiming.
An option to configure LCD retiming.
A value representing no retiming options.
A value representing all retiming options.
An option to configure HFXO retiming.
An option to configure HFRCO retiming.
An option to configure DCDC retiming.
An option to configure LCD retiming.
A value representing no retiming options.
A value representing all retiming options.
Enumeration Documentation#
RAIL_RetimeOptions_t#
RAIL_RetimeOptions_t
Retiming options bit shifts.
DeprecatedRAIL 2.x synonym of sl_rail_retime_options_t.
| Enumerator | |
|---|---|
| RAIL_RETIME_OPTION_HFXO_SHIFT | Shift position of RAIL_RETIME_OPTION_HFXO bit. |
| RAIL_RETIME_OPTION_HFRCO_SHIFT | Shift position of RAIL_RETIME_OPTION_HFRCO bit. |
| RAIL_RETIME_OPTION_DCDC_SHIFT | Shift position of RAIL_RETIME_OPTION_DCDC bit. |
| RAIL_RETIME_OPTION_LCD_SHIFT | Shift position of RAIL_RETIME_OPTION_LCD bit. |
sl_rail_retime_options_t#
sl_rail_retime_options_t
Retiming options bit shifts.
| Enumerator | |
|---|---|
| SL_RAIL_RETIME_OPTION_HFXO_SHIFT | Shift position of SL_RAIL_RETIME_OPTION_HFXO bit. |
| SL_RAIL_RETIME_OPTION_HFRCO_SHIFT | Shift position of SL_RAIL_RETIME_OPTION_HFRCO bit. |
| SL_RAIL_RETIME_OPTION_DCDC_SHIFT | Shift position of SL_RAIL_RETIME_OPTION_DCDC bit. |
| SL_RAIL_RETIME_OPTION_LCD_SHIFT | Shift position of SL_RAIL_RETIME_OPTION_LCD bit. |
Function Documentation#
RAIL_ConfigRetimeOptions#
RAIL_Status_t RAIL_ConfigRetimeOptions (RAIL_Handle_t railHandle, RAIL_RetimeOptions_t mask, RAIL_RetimeOptions_t options)
Configure retiming options.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A handle of RAIL instance. |
| RAIL_RetimeOptions_t | [in] | mask | A bitmask containing which options should be modified. |
| RAIL_RetimeOptions_t | [in] | options | A bitmask containing desired configuration settings. Bit positions for each option are found in the RAIL_RetimeOptions_t. |
Returns
Status code indicating success of the function call.
DeprecatedRAIL 2.x synonym of sl_rail_config_retime_options().
RAIL_GetRetimeOptions#
RAIL_Status_t RAIL_GetRetimeOptions (RAIL_Handle_t railHandle, RAIL_RetimeOptions_t * pOptions)
Get the currently configured retiming option.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A handle of RAIL instance. |
| RAIL_RetimeOptions_t * | [out] | pOptions | A pointer to configured retiming options bitmask indicating which are enabled. |
Returns
Status code indicating success of the function call.
DeprecatedRAIL 2.x synonym of sl_rail_get_retime_options().
RAIL_ChangedDcdc#
RAIL_Status_t RAIL_ChangedDcdc (void )
Indicate that the DCDC peripheral bus clock enable has changed allowing RAIL to react accordingly.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This should be called after DCDC has been enabled or disabled.
DeprecatedRAIL 2.x synonym of sl_rail_changed_dcdc().
sl_rail_config_retime_options#
sl_rail_status_t sl_rail_config_retime_options (sl_rail_handle_t rail_handle, sl_rail_retime_options_t mask, sl_rail_retime_options_t options)
Configure retiming options.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A handle of RAIL instance. |
| sl_rail_retime_options_t | [in] | mask | A bitmask containing which options should be modified. |
| sl_rail_retime_options_t | [in] | options | A bitmask containing desired configuration settings. Bit positions for each option are found in the sl_rail_retime_options_t. |
Returns
Status code indicating success of the function call.
sl_rail_get_retime_options#
sl_rail_status_t sl_rail_get_retime_options (sl_rail_handle_t rail_handle, sl_rail_retime_options_t * p_options)
Get the currently configured retiming option.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A handle of RAIL instance. |
| sl_rail_retime_options_t * | [out] | p_options | A pointer to configured retiming options bitmask indicating which are enabled. |
Returns
Status code indicating success of the function call.
sl_rail_changed_dcdc#
sl_rail_status_t sl_rail_changed_dcdc (void )
Indicate that the DCDC peripheral bus clock enable has changed allowing RAIL to react accordingly.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
Status code indicating success of the function call.
Note
This should be called after DCDC has been enabled or disabled.
Macro Definition Documentation#
RAIL_RETIME_OPTION_HFXO#
#define RAIL_RETIME_OPTION_HFXOValue:
(1U << RAIL_RETIME_OPTION_HFXO_SHIFT)
An option to configure HFXO retiming.
DeprecatedRAIL 2.x synonym of SL_RAIL_RETIME_OPTION_HFXO.
RAIL_RETIME_OPTION_HFRCO#
#define RAIL_RETIME_OPTION_HFRCOValue:
(1U << RAIL_RETIME_OPTION_HFRCO_SHIFT)
An option to configure HFRCO retiming.
DeprecatedRAIL 2.x synonym of SL_RAIL_RETIME_OPTION_HFRCO.
RAIL_RETIME_OPTION_DCDC#
#define RAIL_RETIME_OPTION_DCDCValue:
(1U << RAIL_RETIME_OPTION_DCDC_SHIFT)
An option to configure DCDC retiming.
Ignored on platforms that lack DCDC.
DeprecatedRAIL 2.x synonym of SL_RAIL_RETIME_OPTION_DCDC.
RAIL_RETIME_OPTION_LCD#
#define RAIL_RETIME_OPTION_LCDValue:
(1U << RAIL_RETIME_OPTION_LCD_SHIFT)
An option to configure LCD retiming.
Ignored on platforms that lack LCD.
DeprecatedRAIL 2.x synonym of SL_RAIL_RETIME_OPTION_LCD.
RAIL_RETIME_OPTIONS_NONE#
#define RAIL_RETIME_OPTIONS_NONEValue:
0x0U
A value representing no retiming options.
DeprecatedRAIL 2.x synonym of SL_RAIL_RETIME_OPTIONS_NONE.
RAIL_RETIME_OPTIONS_ALL#
#define RAIL_RETIME_OPTIONS_ALLValue:
0xFFU
A value representing all retiming options.
DeprecatedRAIL 2.x synonym of SL_RAIL_RETIME_OPTIONS_ALL.
SL_RAIL_RETIME_OPTION_HFXO#
#define SL_RAIL_RETIME_OPTION_HFXOValue:
(1U << SL_RAIL_RETIME_OPTION_HFXO_SHIFT)
An option to configure HFXO retiming.
SL_RAIL_RETIME_OPTION_HFRCO#
#define SL_RAIL_RETIME_OPTION_HFRCOValue:
(1U << SL_RAIL_RETIME_OPTION_HFRCO_SHIFT)
An option to configure HFRCO retiming.
SL_RAIL_RETIME_OPTION_DCDC#
#define SL_RAIL_RETIME_OPTION_DCDCValue:
(1U << SL_RAIL_RETIME_OPTION_DCDC_SHIFT)
An option to configure DCDC retiming.
Ignored on platforms that lack DCDC.
SL_RAIL_RETIME_OPTION_LCD#
#define SL_RAIL_RETIME_OPTION_LCDValue:
(1U << SL_RAIL_RETIME_OPTION_LCD_SHIFT)
An option to configure LCD retiming.
Ignored on platforms that lack LCD.
SL_RAIL_RETIME_OPTIONS_NONE#
#define SL_RAIL_RETIME_OPTIONS_NONEValue:
0x0U
A value representing no retiming options.
SL_RAIL_RETIME_OPTIONS_ALL#
#define SL_RAIL_RETIME_OPTIONS_ALLValue:
0xFFU
A value representing all retiming options.