General Settings#
Use General Settings to configure the following options:
Wireless Network Name (SSID)
Region Code
Channel
Bandwidth
Wi-Fi Band
Transmission Mode
Wireless Network Name (SSID)#
Service Set Identifier (SSID) is a unique identifier applied to the access point and the wireless client, which allows them to associate. The Password can be set in the Security subpage.
Region Code#
The following region codes are available:
Factory Default Region
World Wide Domain
European Union
Japan
Korea
China
United States
Channel#
The supported channel range is 0-13.
Auto mode is also supported.
Bandwidth#
The only supported bandwidth is 20 MHz.
Wi-Fi Band#
The only supported Wi-Fi band is 2.4 GHz.
Transmission Mode#
The following transmission modes are supported:
802.11b only
802.11g only
802.11n only
802.11ax only
Auto mode is also supported.