Network Settings#
Use Network Settings to configure the following options:
IP Management
Internet Protocol
IP Address
Gateway
Mask
IP Management#
The following IP management modes are supported:
Static IP
Link Local
DHCP
Internet Protocol#
The following Internet Protocol modes are supported:
IPv4
IPv6
IP Address#
An Internet Protocol (IP) address is a unique numerical identifier assigned to a device on a network.
Gateway#
The gateway IP address used to route traffic to networks outside the local network.
Mask#
A mask, commonly called a subnet mask or netmask, is a 32-bit value that divides an IP address into network and host portions.