Driver change log
Release 2.0.1
(release date 2019-04-18)
- Fix an issue with the softAP interface
- Limit the input buffers to avoid running into issues when transmitting data and sending regular FMAC commands
- Update the Doxygen documentation
- Aligned on firmware 2.2.1
Release 2.0.0
(release date 2019-04-12)
- File name prefixes changed from wf200_ to sl_wfx_
- Function name prefixes changed from wf200_ to sl_wfx_
- Structure name prefixes changed from wf200_ to sl_wfx_
- Add following APIs:
- sl_wfx_join_ibss_command()
- sl_wfx_leave_ibss_command()
- sl_wfx_remove_multicast_address()
- sl_wfx_set_arp_ip_address()
- sl_wfx_set_ns_ip_address()
- sl_wfx_set_broadcast_filter()
- sl_wfx_set_unicast_filter()
- sl_wfx_add_whitelist_address()
- sl_wfx_add_blacklist_address()
- sl_wfx_set_max_ap_client_inactivity()
- sl_wfx_set_scan_parameters()
- sl_wfx_set_roam_parameters()
- sl_wfx_set_tx_rate_parameters()
- sl_wfx_set_max_tx_power()
- sl_wfx_get_max_tx_power()
- sl_wfx_control_gpio()
- sl_wfx_prevent_rollback()
- Remove wf200_pds.h from the driver
- Add sl_wfx_host_get_pds_data() and sl_wfx_host_get_pds_size() APIs
- Modify sl_wfx_host_post_event() declaration
- Modify sl_wfx_host_spi_transfer_no_cs_assert() declaration
- wf200_frame_t structure replaced by sl_wfx_send_frame_req_t
- wf200_ethernet_frame_t structure replaced by sl_wfx_received_ind_t
- wf200_buffer_t structure replaced by sl_wfx_generic_message_t
- wf200_scan_result_t structure replaced by sl_wfx_scan_result_ind_t
- Align existing driver APIs to firmware APIs
- Aligned on firmware 2.2.1
Release 1.0.1
(release date 2019-03-04)
- Modification in wf200_bus_sdio.c to improve SDIO support
- Removed Doxygen HTML output
- Aligned on firmware 2.0.0
Release 1.0.0
(release date 2019-01-08)
- Initial release
- Aligned on firmware 2.0.0