API messages in IBSS modeFULL_MAC_API > API messages by mode

WFM API messages applicable for an interface in IBSS mode.

Data Structures

struct sl_wfx_send_frame_req_t
Request message for sending a packet to the network.
struct sl_wfx_send_frame_cnf_t
Confirmation message for sl_wfx_send_frame_req_t .
struct sl_wfx_received_ind_t
Indication message used to signal a received packet.
struct sl_wfx_leave_ibss_cnf_t
Confirmation message for sl_wfx_leave_ibss_req_t .
struct sl_wfx_set_max_tx_power_req_t
Request message for setting a maximum transmit power.
struct sl_wfx_set_max_tx_power_cnf_t
Confirmation message for sl_wfx_set_max_tx_power_req_t .
struct sl_wfx_get_max_tx_power_cnf_t
Confirmation message for sl_wfx_get_max_tx_power_req_t .
struct sl_wfx_leave_ibss_req_t
Request message for disconnecting from an IBSS network.
struct sl_wfx_leave_ibss_ind_t
Indication message used to signal the completion of a disconnect operation.
struct sl_wfx_get_max_tx_power_req_t
Request message for getting the maximum transmit power.

Detailed Description

WFM API messages applicable for an interface in IBSS mode.


Data Structure Documentation

◆ sl_wfx_send_frame_req_t

struct sl_wfx_send_frame_req_t

Request message for sending a packet to the network.

The host can use this request to send a packet to the network.

Interface mode Request allowed
idle No
station Yes
AP Yes
IBSS Yes


Definition at line 1547 of file wfm_cmd_api.h .

Data Fields
sl_wfx_send_frame_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_send_frame_cnf_t

struct sl_wfx_send_frame_cnf_t

Confirmation message for sl_wfx_send_frame_req_t .

Definition at line 1581 of file wfm_cmd_api.h .

Data Fields
sl_wfx_send_frame_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_received_ind_t

struct sl_wfx_received_ind_t

Indication message used to signal a received packet.

The device will send this indication to signal a packet has been received.

Definition at line 1622 of file wfm_cmd_api.h .

Data Fields
sl_wfx_received_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_leave_ibss_cnf_t

struct sl_wfx_leave_ibss_cnf_t

Confirmation message for sl_wfx_leave_ibss_req_t .

Definition at line 1992 of file wfm_cmd_api.h .

Data Fields
sl_wfx_leave_ibss_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_max_tx_power_req_t

struct sl_wfx_set_max_tx_power_req_t

Request message for setting a maximum transmit power.

The host can use this request to set a maximum transmit power. The device can still use a lower transmit power depending on regulatory rules or internal limitations.

Interface mode Request allowed
idle Yes
station Yes
AP Yes
IBSS Yes


Definition at line 2897 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_max_tx_power_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_max_tx_power_cnf_t

struct sl_wfx_set_max_tx_power_cnf_t

Confirmation message for sl_wfx_set_max_tx_power_req_t .

Definition at line 2924 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_max_tx_power_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_get_max_tx_power_cnf_t

struct sl_wfx_get_max_tx_power_cnf_t

Confirmation message for sl_wfx_get_max_tx_power_req_t .

Definition at line 2978 of file wfm_cmd_api.h .

Data Fields
sl_wfx_get_max_tx_power_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_leave_ibss_req_t

struct sl_wfx_leave_ibss_req_t

Request message for disconnecting from an IBSS network.

The host can use this request to disconnect from an IBSS network.

Interface mode Request allowed
idle No
station No
AP No
IBSS Yes

◆ sl_wfx_leave_ibss_ind_t

struct sl_wfx_leave_ibss_ind_t

Indication message used to signal the completion of a disconnect operation.

The device will send this indication to signal the disconnect request initiated with sl_wfx_leave_ibss_req_t has been completed. The indication is also sent when the network has encountered a fatal error.

◆ sl_wfx_get_max_tx_power_req_t

struct sl_wfx_get_max_tx_power_req_t

Request message for getting the maximum transmit power.

The host can use this request to get the current value of maximum transmit power.

Interface mode Request allowed
idle Yes
station Yes
AP Yes
IBSS Yes