API messages in AP modeFULL_MAC_API > API messages by mode

WFM API messages applicable for an interface in AP mode.

Data Structures

struct sl_wfx_update_ap_req_t
Request message for updating parameters of the started Wi-Fi network.
struct sl_wfx_update_ap_cnf_t
Confirmation message for sl_wfx_update_ap_req_t .
struct sl_wfx_stop_ap_cnf_t
Confirmation message for sl_wfx_stop_ap_req_t .
struct sl_wfx_ap_client_connected_ind_t
Indication message used to signal a connected station.
struct sl_wfx_ap_client_rejected_ind_t
Indication message used to signal a rejected connection attempt from a station.
struct sl_wfx_disconnect_ap_client_req_t
Request message for disconnecting a client from the started Wi-Fi network.
struct sl_wfx_disconnect_ap_client_cnf_t
Confirmation message for sl_wfx_disconnect_ap_client_req_t .
struct sl_wfx_ap_client_disconnected_ind_t
Indication message used to signal a disconnected station.
struct sl_wfx_send_frame_req_t
Request message for sending a packet to the network.
struct sl_wfx_send_frame_cnf_t
Confirmation message for sl_wfx_send_frame_req_t .
struct sl_wfx_received_ind_t
Indication message used to signal a received packet.
struct sl_wfx_add_multicast_addr_req_t
Request message for adding a multicast address to the multicast filter whitelist.
struct sl_wfx_add_multicast_addr_cnf_t
Confirmation message for sl_wfx_add_multicast_addr_req_t .
struct sl_wfx_remove_multicast_addr_req_t
Request message for removing a multicast address from the multicast filter whitelist.
struct sl_wfx_remove_multicast_addr_cnf_t
Confirmation message for sl_wfx_remove_multicast_addr_req_t .
struct sl_wfx_set_max_ap_client_count_req_t
Request message for setting the maximum number of connected clients.
struct sl_wfx_set_max_ap_client_count_cnf_t
Confirmation message for sl_wfx_set_max_ap_client_count_req_t .
struct sl_wfx_set_max_ap_client_inactivity_req_t
Request message for setting the maximum number of connected clients.
struct sl_wfx_set_max_ap_client_inactivity_cnf_t
Confirmation message for sl_wfx_set_max_ap_client_inactivity_req_t .
struct sl_wfx_set_unicast_filter_req_t
Request message for setting unicast filter state.
struct sl_wfx_set_unicast_filter_cnf_t
Confirmation message for sl_wfx_set_unicast_filter_req_t .
struct sl_wfx_add_whitelist_addr_req_t
Request message for adding a MAC address to the device whitelist.
struct sl_wfx_add_whitelist_addr_cnf_t
Confirmation message for sl_wfx_add_whitelist_addr_req_t .
struct sl_wfx_add_blacklist_addr_req_t
Request message for adding a MAC address to the device blacklist.
struct sl_wfx_add_blacklist_addr_cnf_t
Confirmation message for sl_wfx_add_blacklist_addr_req_t .
struct sl_wfx_set_max_tx_power_req_t
Request message for setting a maximum transmit power.
struct sl_wfx_set_max_tx_power_cnf_t
Confirmation message for sl_wfx_set_max_tx_power_req_t .
struct sl_wfx_get_max_tx_power_cnf_t
Confirmation message for sl_wfx_get_max_tx_power_req_t .
struct sl_wfx_get_pmk_cnf_t
Confirmation message for sl_wfx_get_pmk_req_t .
struct sl_wfx_stop_ap_req_t
Request message for stopping the started Wi-Fi network.
struct sl_wfx_stop_ap_ind_t
Indication message used to signal the completion of a stop operation.
struct sl_wfx_get_max_tx_power_req_t
Request message for getting the maximum transmit power.
struct sl_wfx_get_pmk_req_t
Request message for getting the Pairwise Master Key (PMK).

Detailed Description

WFM API messages applicable for an interface in AP mode.


Data Structure Documentation

◆ sl_wfx_update_ap_req_t

struct sl_wfx_update_ap_req_t

Request message for updating parameters of the started Wi-Fi network.

The host can use this request to update parameters of the started Wi-Fi network.

Interface mode Request allowed
idle No
station No
AP Yes
IBSS No


Definition at line 1286 of file wfm_cmd_api.h .

Data Fields
sl_wfx_update_ap_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_update_ap_cnf_t

struct sl_wfx_update_ap_cnf_t

Confirmation message for sl_wfx_update_ap_req_t .

Definition at line 1310 of file wfm_cmd_api.h .

Data Fields
sl_wfx_update_ap_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_stop_ap_cnf_t

struct sl_wfx_stop_ap_cnf_t

Confirmation message for sl_wfx_stop_ap_req_t .

Definition at line 1348 of file wfm_cmd_api.h .

Data Fields
sl_wfx_stop_ap_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_ap_client_connected_ind_t

struct sl_wfx_ap_client_connected_ind_t

Indication message used to signal a connected station.

The device will send this indication to signal a station has connected to the started network.

Definition at line 1381 of file wfm_cmd_api.h .

Data Fields
sl_wfx_ap_client_connected_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_ap_client_rejected_ind_t

struct sl_wfx_ap_client_rejected_ind_t

Indication message used to signal a rejected connection attempt from a station.

The device will send this indication to signal a station has attempted connection to the started network and was rejected by the device.

Definition at line 1412 of file wfm_cmd_api.h .

Data Fields
sl_wfx_ap_client_rejected_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_disconnect_ap_client_req_t

struct sl_wfx_disconnect_ap_client_req_t

Request message for disconnecting a client from the started Wi-Fi network.

The host can use this request to disconnect a client from the started Wi-Fi network.

Interface mode Request allowed
idle No
station No
AP Yes
IBSS No


Definition at line 1441 of file wfm_cmd_api.h .

Data Fields
sl_wfx_disconnect_ap_client_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_disconnect_ap_client_cnf_t

struct sl_wfx_disconnect_ap_client_cnf_t

Confirmation message for sl_wfx_disconnect_ap_client_req_t .

Definition at line 1465 of file wfm_cmd_api.h .

Data Fields
sl_wfx_disconnect_ap_client_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_ap_client_disconnected_ind_t

struct sl_wfx_ap_client_disconnected_ind_t

Indication message used to signal a disconnected station.

The device will send this indication to signal a station has left the started network.

Definition at line 1494 of file wfm_cmd_api.h .

Data Fields
sl_wfx_ap_client_disconnected_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_send_frame_req_t

struct sl_wfx_send_frame_req_t

Request message for sending a packet to the network.

The host can use this request to send a packet to the network.

Interface mode Request allowed
idle No
station Yes
AP Yes
IBSS Yes


Definition at line 1547 of file wfm_cmd_api.h .

Data Fields
sl_wfx_send_frame_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_send_frame_cnf_t

struct sl_wfx_send_frame_cnf_t

Confirmation message for sl_wfx_send_frame_req_t .

Definition at line 1581 of file wfm_cmd_api.h .

Data Fields
sl_wfx_send_frame_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_received_ind_t

struct sl_wfx_received_ind_t

Indication message used to signal a received packet.

The device will send this indication to signal a packet has been received.

Definition at line 1622 of file wfm_cmd_api.h .

Data Fields
sl_wfx_received_ind_body_t body Indication message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_add_multicast_addr_req_t

struct sl_wfx_add_multicast_addr_req_t

Request message for adding a multicast address to the multicast filter whitelist.

The host can use this request to add a multicast address to the multicast filter whitelist. When the first address is added the whitelist, the device will discard all multicast frames whose destination address does not match any of the addresses on the list. The default state is to allow all multicast addresses. The whitelist is reset to the default state when the interface is reset. Up to 8 multicast addresses may be added.
See Filtering for further details.

Interface mode Request allowed
idle No
station Yes
AP Yes
IBSS No


Definition at line 2042 of file wfm_cmd_api.h .

Data Fields
sl_wfx_add_multicast_addr_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_add_multicast_addr_cnf_t

struct sl_wfx_add_multicast_addr_cnf_t

Confirmation message for sl_wfx_add_multicast_addr_req_t .

Definition at line 2067 of file wfm_cmd_api.h .

Data Fields
sl_wfx_add_multicast_addr_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_remove_multicast_addr_req_t

struct sl_wfx_remove_multicast_addr_req_t

Request message for removing a multicast address from the multicast filter whitelist.

The host can use this request to remove a multicast address from the multicast filter whitelist.

Interface mode Request allowed
idle No
station Yes
AP Yes
IBSS No


Definition at line 2100 of file wfm_cmd_api.h .

Data Fields
sl_wfx_remove_multicast_addr_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_remove_multicast_addr_cnf_t

struct sl_wfx_remove_multicast_addr_cnf_t

Confirmation message for sl_wfx_remove_multicast_addr_req_t .

Definition at line 2125 of file wfm_cmd_api.h .

Data Fields
sl_wfx_remove_multicast_addr_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_max_ap_client_count_req_t

struct sl_wfx_set_max_ap_client_count_req_t

Request message for setting the maximum number of connected clients.

The host can use this request to limit the number of stations that can connect the started Wi-Fi network.

Interface mode Request allowed
idle No
station No
AP Yes
IBSS No


Definition at line 2162 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_max_ap_client_count_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_max_ap_client_count_cnf_t

struct sl_wfx_set_max_ap_client_count_cnf_t

Confirmation message for sl_wfx_set_max_ap_client_count_req_t .

Definition at line 2186 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_max_ap_client_count_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_max_ap_client_inactivity_req_t

struct sl_wfx_set_max_ap_client_inactivity_req_t

Request message for setting the maximum number of connected clients.

The host can use this request to limit the number of stations that can connect the started Wi-Fi network.

Interface mode Request allowed
idle No
station No
AP Yes
IBSS No


Definition at line 2223 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_max_ap_client_inactivity_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_max_ap_client_inactivity_cnf_t

struct sl_wfx_set_max_ap_client_inactivity_cnf_t

Confirmation message for sl_wfx_set_max_ap_client_inactivity_req_t .

Definition at line 2247 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_max_ap_client_inactivity_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_unicast_filter_req_t

struct sl_wfx_set_unicast_filter_req_t

Request message for setting unicast filter state.

The host can use this request to configure the state of the unicast filter. When enabled, the device will only forward certain unicast frames to the host and automatically discard the rest.
See Filtering for further details.

Interface mode Request allowed
idle No
station No
AP Yes
IBSS No


Definition at line 2711 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_unicast_filter_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_unicast_filter_cnf_t

struct sl_wfx_set_unicast_filter_cnf_t

Confirmation message for sl_wfx_set_unicast_filter_req_t .

Definition at line 2735 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_unicast_filter_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_add_whitelist_addr_req_t

struct sl_wfx_add_whitelist_addr_req_t

Request message for adding a MAC address to the device whitelist.

The host can use this request to add a MAC address to the list of allowed MAC addresses. When the first address is added the whitelist, the device will prevent communication with any devices whose MAC address does not match any of the addresses on the list. Setting a whitelist will clear all entries from the device blacklist. The default state is to allow all MAC addresses. The whitelist is reset to the default state when the interface is reset. Up to 8 MAC addresses may be added.
See Filtering for further details.

Interface mode Request allowed
idle No
station No
AP Yes
IBSS No


Definition at line 2772 of file wfm_cmd_api.h .

Data Fields
sl_wfx_add_whitelist_addr_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_add_whitelist_addr_cnf_t

struct sl_wfx_add_whitelist_addr_cnf_t

Confirmation message for sl_wfx_add_whitelist_addr_req_t .

Definition at line 2796 of file wfm_cmd_api.h .

Data Fields
sl_wfx_add_whitelist_addr_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_add_blacklist_addr_req_t

struct sl_wfx_add_blacklist_addr_req_t

Request message for adding a MAC address to the device blacklist.

The host can use this request to add a MAC address to the list of denied MAC addresses. When the first address is added the blacklist, the device will prevent communication with any device whose MAC address matches any of the addresses on the list. Setting a blacklist will clear all entries from the device whitelist. The default state is to allow all MAC addresses. The blacklist is reset to the default state when the interface is reset. Up to 8 MAC addresses may be added.
See Filtering for further details.

Interface mode Request allowed
idle No
station No
AP Yes
IBSS No


Definition at line 2833 of file wfm_cmd_api.h .

Data Fields
sl_wfx_add_blacklist_addr_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_add_blacklist_addr_cnf_t

struct sl_wfx_add_blacklist_addr_cnf_t

Confirmation message for sl_wfx_add_blacklist_addr_req_t .

Definition at line 2857 of file wfm_cmd_api.h .

Data Fields
sl_wfx_add_blacklist_addr_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_max_tx_power_req_t

struct sl_wfx_set_max_tx_power_req_t

Request message for setting a maximum transmit power.

The host can use this request to set a maximum transmit power. The device can still use a lower transmit power depending on regulatory rules or internal limitations.

Interface mode Request allowed
idle Yes
station Yes
AP Yes
IBSS Yes


Definition at line 2897 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_max_tx_power_req_body_t body Request message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_set_max_tx_power_cnf_t

struct sl_wfx_set_max_tx_power_cnf_t

Confirmation message for sl_wfx_set_max_tx_power_req_t .

Definition at line 2924 of file wfm_cmd_api.h .

Data Fields
sl_wfx_set_max_tx_power_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_get_max_tx_power_cnf_t

struct sl_wfx_get_max_tx_power_cnf_t

Confirmation message for sl_wfx_get_max_tx_power_req_t .

Definition at line 2978 of file wfm_cmd_api.h .

Data Fields
sl_wfx_get_max_tx_power_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_get_pmk_cnf_t

struct sl_wfx_get_pmk_cnf_t

Confirmation message for sl_wfx_get_pmk_req_t .

Definition at line 3032 of file wfm_cmd_api.h .

Data Fields
sl_wfx_get_pmk_cnf_body_t body Confirmation message body.
sl_wfx_header_t header Common message header.

◆ sl_wfx_stop_ap_req_t

struct sl_wfx_stop_ap_req_t

Request message for stopping the started Wi-Fi network.

The host can use this request to stop the started Wi-Fi network.

Interface mode Request allowed
idle No
station No
AP Yes
IBSS No

◆ sl_wfx_stop_ap_ind_t

struct sl_wfx_stop_ap_ind_t

Indication message used to signal the completion of a stop operation.

The device will send this indication to signal the stop request initiated with sl_wfx_stop_ap_req_t has been completed. The indication is also sent when the started network has encountered a fatal error.

◆ sl_wfx_get_max_tx_power_req_t

struct sl_wfx_get_max_tx_power_req_t

Request message for getting the maximum transmit power.

The host can use this request to get the current value of maximum transmit power.

Interface mode Request allowed
idle Yes
station Yes
AP Yes
IBSS Yes

◆ sl_wfx_get_pmk_req_t

struct sl_wfx_get_pmk_req_t

Request message for getting the Pairwise Master Key (PMK).

The host can use this request to retrieve the Pairwise Master Key (PMK) used to connect to the current secure network. PMK can be given in the next sl_wfx_connect_req_t message to speed up connection process. See Passwords and passphrases for further details.

Interface mode Request allowed
idle No
station Yes
AP Yes
IBSS No