Structure to hold the clock configuration parameters.

Public Attributes#

uint16_t

Division factor (0 to 1023).

uint32_t

SoC PLL clock frequency.

uint32_t

SoC PLL reference clock frequency.

Public Attribute Documentation#

division_factor#

uint16_t sl_adc_clock_config_t::division_factor

Division factor (0 to 1023).


Definition at line 163 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h

soc_pll_clock#

uint32_t sl_adc_clock_config_t::soc_pll_clock

SoC PLL clock frequency.


Definition at line 164 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h

soc_pll_reference_clock#

uint32_t sl_adc_clock_config_t::soc_pll_reference_clock

SoC PLL reference clock frequency.


Definition at line 165 of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h