Structure to hold the FIFO threshold configuration parameters.
Public Attributes#
uint8_t
Number of channels enabled.
uint8_t
AEMPTY (almost empty) threshold.
uint8_t
AFULL (almost full) threshold.
uint8_t
Internal (0) or external (1) DMA type.
Public Attribute Documentation#
num_of_channel_en#
uint8_t sl_adc_fifo_thrld_config_t::num_of_channel_en
Number of channels enabled.
Definition at line
153
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
a_empty_threshold#
uint8_t sl_adc_fifo_thrld_config_t::a_empty_threshold
AEMPTY (almost empty) threshold.
Definition at line
154
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
a_full_threshold#
uint8_t sl_adc_fifo_thrld_config_t::a_full_threshold
AFULL (almost full) threshold.
Definition at line
155
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h
dma_type#
uint8_t sl_adc_fifo_thrld_config_t::dma_type
Internal (0) or external (1) DMA type.
Definition at line
156
of file components/device/silabs/si91x/mcu/drivers/unified_api/inc/sl_si91x_adc.h